Tool/software: Linux
Hi,
Image capture and memory dump are ok in DCC, and DCC file which is included in program image is also ok.
Sensor id in DCC was set up correctly. But "Update Current DCC" is not working.
Please find the following err log.
<DCC side>
Request to Update active DCC data in Target : 10.159.171.31
Loaded communication DLL:itCommun.dll
Error in Updating current DCC bin data
<TDA2Px EVB side>
[HOST] [HOST ] 1262.919203 s: NETWORK_CTRL: Received command [iss_send_dcc_file], with 173 bytes of parameters
[HOST] [HOST ] 1262.919538 s: NETWORK_CTRL: Network_read() failed to read parameters (port=5000) !!!
[HOST] [HOST ] 1262.919538 s: NETWORK_CTRL: iss_send_dcc_file:
[HOST] [HOST ] 1262.919843 s: NETWORK_CTRL: Sent response for command [iss_send_dcc_file], with 0 bytes of parameters
Regards,
HJ Kim