Part Number: AM3352
Hi Champs,
We connected AM3352 (master) and FPGA (slave) via GPMC.
We confirmed OE, CS,GPMC_CLK , data line output control using WAIT signal at single access setting (READMULTIPLE =0).
However, TRM mentioned as bellow.
So, Can we continue to use this setting ?
--------------------------------------------------------------------------------------
「AM3352_Technical Reference Manual.pdf」P.614
7.1.2.3.8.3.4 Wait Monitoring During a Synchronous Read Access
• WAIT monitored as inactive unfreezes the CYCLETIME counter. For an access within a burst (when
the CYCLETIME counter is by definition in lock state), WAIT monitored as inactive completes the
current access time and starts the next access phase in the burst. The data bus is considered valid,
and data are captured during this clock cycle. In a single access or if this was the last access in a
multiple-access cycle, all signals are controlled according to their relative control timing value and the
CYCLETIME counter status.
--------------------------------------------------------------------------------------
Regards,
Kz777