Part Number: 66AK2H14
Hi,
We are using 66AK2H14DAAWA24 part in our design where the device is getting booted and all the DDR and SERDES(SRIO & ETHERNET Switch) interface are functioning properly, except HYPERLINK INTERFACE.
Issue with this interface is that the PLL is not getting locked for this interface
We have checked all the power as well as the clock(312.5Mhz) corresponding to hyperlink interface and all are as expected.
We have mounted 3K_Ohm from HYP0REFRES pin to GND as specified but the resistance but the observed resistance value across this was 1.2OHM, so we removed this resistor and checked the impedance at the resistor pads and observed same 1.2E(after removing 3K resistor). The same observation is see across HYP1REFRES and GND as well.
Is this the expected impedance value at this pin please suggest or is there any issue with, whether these pins are damaged internally,Should we replace the chipset or is there any alternate solution?
Request you to provide your valuable feedback ASAP.
Regards,
Karthik