This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5718: EMIF configuration in U-boot

Part Number: AM5718

We are using -

Processor : AM571x Sitara processor
SDK : ti-processor-sdk-linux-am57xx-evm-05.03.00.07

We have modified the EMIF_RegisterConfiguration.xlsm worksheet with the new values according to our custom design board with DDR3L RAM memory and generated the code required to be copied to U-boot source code.

Please can you suggest exactly which is/are the files to be modified in the U-boot source code.