Part Number: PROCESSOR-SDK-AM437X
Other Parts Discussed in Thread: AM4379
Tool/software: TI-RTOS
HI,
We have purchased MYD-C437X-PRU development board from MYIR tech. currently we are in a process of building the RTOS example projects, we have successfully installed code composer studio 6.2.0 and "processor_sdk_rtos_am437x_3_01 _00_06" . Now we are trying to build the "pdk_am437x_1_0_4" example files and i am getting the following errors on the command promt. I am able to set up environment successfully. Kindly suggest us how to resolve the below issue (highlighted with red color font).
C:\ti\processor_sdk_rtos_am437x_3_01_00_06>setupenv.bat
Optional parameter not configured : CG_XML_BIN_INSTALL_PATH
REQUIRED for xdc release build
Example: set CG_XML_BIN_INSTALL_PATH=C:/ti/cg_xml/bin
Optional parameter not configured : DOXYGEN_INSTALL_PATH
REQUIRED for xdc release build
Example: set DOXYGEN_INSTALL_PATH=C:/ti/Doxygen/doxygen/1.5.1-p1/bin
**************************************************************************
Environment Configuration:
LIMIT_SOCS : am437x
LIMIT_BOARDS : evmAM437x idkAM437x skAM437x
PDK_INSTALL_PATH : /ti/PDK_AM~1/packages/
C6X_GEN_INSTALL_PATH : C:/ti/ccsv6/tools/compiler/ti-cgt-c6000_8.1.0
TOOLCHAIN_PATH_A15 : C:/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-4_9-2015q3
TOOLCHAIN_PATH_A8 : C:/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-4_9-2015q3
TOOLCHAIN_PATH_A9 : C:/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-4_9-2015q3
TOOLCHAIN_PATH_M4 : C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS
FPULIB_PATH : C:/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-4_9-2015q3/lib/gcc/arm-none-eabi/4.9.3/fpu
CROSS_TOOL_PRFX : arm-none-eabi-
XDC_INSTALL_PATH : C:/ti/xdctools_3_32_00_06_core
BIOS_INSTALL_PATH : C:/ti/bios_6_45_01_29
IPC_INSTALL_PATH : C:/ti/ipc_3_43_02_04
EDMA3LLD_BIOS6_INSTALLDIR : C:/ti/edma3_lld_2_12_01_25
NDK_INSTALL_PATH : C:/ti/ndk_2_24_03_35
IMGLIB_INSTALL_PATH : C:/ti/imglib_c66x_3_1_1_0
UIA_INSTALL_PATH : C:/ti/uia_2_00_03_43
IPC_PLATFORM: UNKNOWN
IPC_ALT_PLATFORM:
PROC_SDK_INSTALL_PATH : C:/ti/processor_sdk_rtos_am437x_3_01_00_06
**************************************************************************
Changing to short name to support directory names containing spaces
current directory: C:/ti/processor_sdk_rtos_am437x_3_01_00_06
PROCESSOR SDK BUILD ENVIRONMENT CONFIGURED
**************************************************************************
C:\ti\processor_sdk_rtos_am437x_3_01_00_06>cd ../
C:\ti>cd pdk_am437x_1_0_4
C:\ti\pdk_am437x_1_0_4>cd packages
C:\ti\pdk_am437x_1_0_4\packages>pdkProjectCreate.bat AM437x EVMAM437x
=========================================================================
Configuration:
SOC : AM437x
BOARD : EVMAM437x
ENDIAN : little
MODULE : all
PROCESSOR : arm
PDK_SHORT_NAME : C:\ti\PDK_AM~1\packages\
=========================================================================
Checking Configuration...
Complete
=========================================================================
PDK_PARTNO : AM437
PDK_ECLIPSE_ID : com.ti.pdk.am437x
RTSC_PLATFORM_NAME : ti.platforms.evmAM437X
RTSC_TARGET : gnu.targets.arm.A9F
CCS_DEVICE : "Cortex A.AM4379.IDK_AM437X"
*****************************************************************************
Detecting all projects in PDK and importing them in the workspace C:\ti\PDK_AM~1\packages\\MyExampleProjects
Detected Test Project: EMAC_BasicExample_evmAM437x_armBiosExampleProject
--------------------------------------------------------------------------------
Creating project 'EMAC_BasicExample_evmAM437x_armBiosExampleProject'...
!ERROR: Unknown product-type ID 'com.ti.sdo.edma3'!
NOTE: Refer to the following list of available product-type IDs (the display-names in square brackets are for reference only):
Copying macro.ini
The system cannot find the path specified.
0 file(s) copied.
Detected Test Project: GPIO_LedBlink_evmAM437x_armExampleProject
Regards
Nagaraj G