Part Number: AM5728
Tool/software: Linux
My program use ipc and the host is linux. When I use ccs to build the project which creats a .out file. Then I change the .out to .xe66 and bind it to dsp. But, the dsp can't work and the log is following:
root@am57xx-evm:~/ipc/bigdata# ./dspchs.sh [ 6936.941778] remoteproc remoteproc2: releasing 40800000.dsp [ 6936.953946] omap-rproc 40800000.dsp: assigned reserved memory node dsp1-memo0 [ 6936.962145] remoteproc remoteproc2: 40800000.dsp is available [ 6936.978117] remoteproc remoteproc2: powering up 40800000.dsp [ 6936.983814] remoteproc remoteproc2: Booting fw image dra7-dsp1-fw.xe66, size8 [ 6936.998594] omap_hwmod: mmu0_dsp1: _wait_target_disable failed [ 6937.004486] omap-iommu 40d01000.mmu: 40d01000.mmu: version 3.0 root@am57xx-evm:~/ipc/bigdata# [ 6937.010444] omap-iommu 40d02000.mmu: 40d020000 [ 6937.020407] remoteproc remoteproc2: Failed to find resource table [ 6937.033163] omap_hwmod: mmu0_dsp1: _wait_target_disable failed