This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA2EXEVM
Tool/software: Linux
hi all,
i want to run virtual drm on J6Entry EVM board, kernel version is 4.14.
now i can port virtual drm from kernel 4.4 to kernel 4.14, and i also modify DTS add vdrm device.
and when kernel boot i can see the /dev/dri/card0 and /dev/vdrm-controller-0 devices.
but when i try to use virtual drm, it goes wrong:
int fd = open("/dev/dri/card0", O_RDWR);
struct gbm_device *display = gbm_create_device(fd);
if (NULL == display)
{
OS_TRACE(("fail to create GBM display\n"));
}
PVR:(Error): [ 71-> 71] < gbm_pvr_create_device():592|ERROR> Failed to create DBM device: No such device [0, ]
it can open success, but when call gbm_create_device() to create device, it goes wrong.
does the libgbm.so need to modify too? does PVR need modify? or else need modify too?
best regards!
Hi fanok,
Which filesystem is used here. Is it from PSDKLA5.03 or from VISIONSDK3.x? If you don't have a /etc/powervr.ini you can create this with these as contents.
[default]
#WindowSystem=libpvrws_WAYLAND.so
[appName]
DbmDriverName=vdrm
Here , appName is the name of the application you are launching? If you are not using wayland/weston, you can first try with kmscube.
We have tested kmscube on vDRM with this patch applied.
http://git.ti.com/glsdk/kmscube/commit/456cabc661caac5c60729751d45efd668faa8e97
Thanks
Ramprasad
hi Ramprasad,
the file system is from PSDK.
if i add /etc/powervr.ini config file, should i execute pvrsrvinit in rcS?
now my rcS as following:
#! /bin/sh
..
insmod lib/modules/4.14.24-01358-g403020b/extra/pvrsrvkm.ko
pvrsrvctl --start --no-module&
....
but not execute pvrsrvinit.
best regards!
Hi fanok,
Are you not using vision-sdk at all here and only PSDKLA? In that case vDRM is not going to work.
vDRM is currently supported with vision-sdk's firmware running on M4 and display is controlled by M4.
In PSDKLA case, display is controlled by A15 and vDRM feature is not available here.
Ramprasad
hi Ramprasad ,
The purpose of porting vitual drm into kernel 4.14 is using visionSDK, but now vitual drm work on A15 is not correct, so the buffer can not transfer to M4 side to display by DSS.
i disable omapdrm, enable vdrm, then i write an app that is similar with Kmscube app.
when call gbm_create_device() API, it occurred error that the previous mention.
best regards!
Hi fanok,
I still didn't understand if you have ported vision-sdk-linux to 4.14 and taken care of all patches. Please confirm.
Can you also let me know if the sgx-um binaries now is from PSDKLA5.03 or from the vision-sdk?
Please share the details of commit-ID of omap5-sgx-ddk-um-linux
Thanks
Ramprasrad
hi Ramprasrad,
thanks for your reply, kernel 4.14 is not support virtual drm, and kernel 4.4 is support it , so we
get the virtual drm patchs from kernel 4.4, then port it into kernel 4.14. fix some compile error,
then running visionsdk IPU2 firmware by remoteproc module.
omap5-sgx-ddk-um-linux is from PSDK,
branch is: ti-img-sgx/1.14.3699939/k4.1
commit ID is :
best regards!
Hi fanok,
There are some changes required in omap5-sgx-ddk-um-linux to support vDRM.
If you take sgx-um binaries from PSDKLA5.x, it won't support vDRM. Can you try with the sgx-um binaries provided in vision-SDK. Refer the userGuide of vision-sdk on the link
TI has not tried 4.14 kernel for vDRM.
Thanks
Ramprasad
Latest available vision-sdk is v3.07
http://software-dl.ti.com/processor-sdk-vision/esd/TDAx/vision-sdk/latest/index_FDS.html
If you have not vision-sdk earlier , you can not use vDRM with Linux SDK alsone.
Thanks
Ramprasad
which version of vision-sdk firmwares you are using now?
Take sgx-um binaries from same vision-SDK.
sgx-um binaries are available in the filesystem provided here.
tisdk-rootfs-image-dra7xx-evm_vsdk_3_4.tar.xz
http://software-dl.ti.com/processor-sdk-vision/esd/TDAx/vision-sdk/03_04_00_00/index_FDS.html
Did you try using this filesystem but migrating only linux kernel to 4.14. and replacing kernel modules and zImage ?
hi Ramprasad,
i get pvrsrvkm.ko from tisdk-rootfs-image-dra7xx-evm_vsdk_3_4.tar.xz and replace the current ko file.
but insmod fail. log as following:
[ 2.470543] pvrsrvkm: disagrees about version of symbol module_layout
insmod: can't insert 'lib/modules/4.14.24-01358-g403020b/extra/pvrsrvkm.ko': invalid module format
i think this ko is not match to current kernel. i guess i need recompile PVR using kernel 4.14.
how can i know the git branch and commit id of sgx-um binaries in tisdk-rootfs-image-dra7xx-evm_vsdk_3_4.tar.xz,
if i know the commit id, i can recompile it and then it can insmod successful.
best regards!
Hi Fanok,
You should update your filesystem with 4.14 kernel image and kernel modules