This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TDA2PXEVM: Cannot Select TIDL Usecases..

Part Number: TDA2PXEVM

Tool/software: TI-RTOS

Previously I ran successfully TIDL usecases on the TDA2xx. However, this time, I am trying to run the same usecase in the TDA2px. I have altered my semseg usecase for 2 EVE's as per the requirement of TDA2px and also configured in the configuration file available at the following directory "vision_sdk/apps/configs/tda2px_evm_bios_all.cfg.mk". Is there any important step I am missing to run my usecase?

2. When I run main interface and select 'f', it does not show the other three usecases: Here is my log:

Vision SDK Usecases,
[IPU1-0]  --------------------
[IPU1-0]  1: Single Camera Usecases
[IPU1-0]  2: Multi-Camera LVDS Usecases
[IPU1-0]  3: AVB RX Usecases, (TDA2x & TDA2Ex ONLY)
[IPU1-0]  4: Dual Display Usecases, (TDA2x EVM ONLY)
[IPU1-0]  5: ISS Usecases, (TDA3x ONLY)
[IPU1-0]  6: TDA2x Stereo Usecases
[IPU1-0]  7: Network RX/TX Usecases
[IPU1-0]  9: RADAR Usecases
[IPU1-0]  a: Miscellaneous test's
[IPU1-0]  c: OPENVX Usecases
[IPU1-0]  f: TIDL Usecase
[IPU1-0]  g: Camera Radar Combo Usecases
[IPU1-0]  
[IPU1-0]  s: System Settings
[IPU1-0]  
[IPU1-0]  x: Exit
[IPU1-0]  
[IPU1-0]  Enter Choice:
[IPU1-0]  
[IPU1-1]     11.151711 s:  NETWORK_CTRL: Starting Server (port=5000) !!!
[IPU1-1]     11.151985 s:  NETWORK_CTRL: Starting Server ... DONE (port=5000) !!!
[IPU1-0]     17.837522 s:  
[IPU1-0]     17.837674 s:
[IPU1-0]  
[IPU1-0]  TIDL Usecases
[IPU1-0]  ---------------
[IPU1-0]  
[IPU1-0]  x: Exit
[IPU1-0]  
[IPU1-0]  Enter Choice:
[IPU1-0]  
[IPU1-0]     20.805801 s:  
[IPU1-0]     20.805862 s:  Unsupported option '1'. Please try again
[IPU1-0]     20.806045 s:
[IPU1-0]  
[IPU1-0]  TIDL Usecases

Kindly respond me asap. Thank you.

With best regards,

H.M.Owais