Part Number: TMS320DM8168
Other Parts Discussed in Thread: PCM3168
Hi,
I am connecting the I2C0 line (SCL,SDA) of DM8168 to 3 PCM3168 Audio codec to configure them..Can i connect them directly or should i use a 1:3 I2C BUFFER?
Regards,
Shyama
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320DM8168
Other Parts Discussed in Thread: PCM3168
Hi,
I am connecting the I2C0 line (SCL,SDA) of DM8168 to 3 PCM3168 Audio codec to configure them..Can i connect them directly or should i use a 1:3 I2C BUFFER?
Regards,
Shyama
Hi Shyama,
Adding 3 PCM3168 Audio codecs to I2C0 line should not be an issue, thus no need of buffer, you can add 3 codec directly. Refer to the DM816x TI EVM (link below), where 8 external devices are attached to I2C0, one audio codec (U2 AIC3106) and 7 other devices (U13, U38, U12, U62, U61, U20, JP1). And no I2C buffer is used for I2C0 lines. We also have 6 external devices attached to I2C1 module directly, no buffer is used for I2C1.

Regards,
Pavel