Part Number: PROCESSOR-SDK-AM65X
Tool/software: Linux
Dear TI support team,
we've seen in the release notes for the processor SDK 06.00 that U-Boot now supports use of the PRU ethernet ports.
We've tested this following the instructions from the documentation (http://software-dl.ti.com/processor-sdk-linux/esd/docs/06_00_00_07/linux/Foundational_Components_U-Boot.html#booting-linux-from-the-network) and it works with the bottom ethernet port on the base board itself.
We didn't manage to get this running with one of the ports on the IDK board, nor did we manage to get this to work on our own custom hardware. We modified the setenv lines from the documentation to use rprocs 0 and 1 and also changed ethact to pruss0_eth, but so far haven't been able to get this to work. On our custom hardware only ICSSG0 and ICSSG1 are connected to PHYs.
The documentation states that "Only PRU-ICSSG port of the base board (ICSSG2) is supported for net boot.". Is there a reason for this limitation?
Regards,
Dominic