This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TDA2EVM5777: Self converted JDetNet model doesn't show same FPS with pre-installed JDetNet model

Part Number: TDA2EVM5777

Tool/software: Linux

Hi,

I downloaded JDetNet model from github and converted that model.

In TIDL OD usecase, the installed JDetNet model that is contained in Vision SDK showed about 20 FPS.

However, the converted JDetNet model shows about 10 FPS and file size was different. 

Moreover, the detected box of vehicle was pink color. The color of vehicle was green when is tested with original model.

I also changed objectDraw link as related post says.

The path of downloaded deploy.prototxt is 'ti_dl\test\testvecs\config\caffe-jacinto-models\trained\object_detection\voc0712\JDetNet\ssd768x320_ds_PSP_dsFac_32_hdDS8_0\test_quantize'  and the name of pretrained model is voc0712_ssdJacintoNetV2_iter_120000.caffemodel.

Is it normal situation?

Regards,

Yoo