This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/PROCESSOR-SDK-AM65X: Task blocked on huge sleep values

Part Number: PROCESSOR-SDK-AM65X

Tool/software: TI-RTOS

Hi,

I see that the task are getting blocked on huge sleep values(like 4294921836), i don't have these sleeps values in the code. 

below is the ROV view of task getting blocked.

When i check in the clock section, i see clocks having timeout of 2ms have tRemaining 4294921836ms, how is this possible?

  • Since the issue related to Profinet switch application on AM65xx, I will loop in our industrial team to comment on this issue. Please indicate why your application requires the task to sleep for that large value ?

    In the meantime, it could be useful if you can share the .cfg file or steps to help us set this issue up on the AM65x  Task sleeps use clock/system ticks, so please indicate how the system timer  is setup.

    Regards,

    Rahul