This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux: Processor SDK Linux V6 AM57xx: linux-devkit

Tool/software: Linux

Hello,

I have installed Processor SDK Linux RT am57xx from software-dl.ti.com/processor-sdk-linux-rt/esd/AM57X/latest/exports/ti-processor-sdk-linux-rt-am57xx-evm-06.00.00.07-Linux-x86-Install.bin on Ubuntu LTS without errors. Right after the installation, the subdirectory linux-devkit/sysroots looks quite different from previous versions - the x86_64-arago-linux directory is missing completely, which means that the cross compiler is not there at all; and the other dir is named armv7at2hf... in contrast to armv7ahf... earlierdays. Am I supposed to install the cross toolchain separate, although the SW download page explicitly says " (all of the below compoonents are bundled within the Linux SDK Essentials package)" ? 

Thanks for some insight & best regards,

Stefan