Hello everyone.
I have a tough question to ask. I use dm355 to capture and encode a mpeg4 bitstream. In the same network section, there's a server takes charge of decoding the bitstream which is sent by dm355 with RTP. Now the problem is that the decoder of the server is a XVID decoder, it seems that it cannot decode the bitsream which is encoded by dm355. In the beginning, I doubt wheather RTP have transported every frame to the server end or not. So I write a test program which receive every frame and write them to a .mpeg4 file. The truth is that I can play the .mpeg4 file with MPlayer but not VLC. So I can reasonably conclude that it is not because of RTP transportation error but the XVID decoder. I really want to know can XVID decoder decode a bitstream which encoded by dm355 ? Thanks.
Best Regards,
Bresso