Part Number: TMS320C5517
Hi Champs,
Based on previous answer,
We have additional question from customer
1: EOT bit timing method.
They understand clock skip is able to detect EOT function.
However, we don't know this detail setting.
So, do you have any interrupt that synchronize to EOT bit changing ?
Or we would like to know such a information
"When xxx interrupt happen, EOT bit will be "1" (complete transmit) in xxx sec "
Or Could you please tell us any recommend to use EOT bit (error detection method) ?
2. How to reset bit count on the McSPI CS Active
Currently, customer is using the most simple slave setting that is not using a FIFO and DMA
At this environment , we have never seen bit count reset phenomenon that is commented by TI comment.
So, Could you please tell us bit coun reset method in case of not using FIFO and DMA at slave ?
Regards,
Kz777