Part Number: AM4379
Other Parts Discussed in Thread: PROFIBUS
Tool/software: Code Composer Studio
Hi all,
what will be - from your point of view - the best approach to combine these two technologies regarding the demos?
With EtherCAT, there is a complete project where IO-Link could be "added" as a kind of library.
Another possibility could be to create an IO-Link project first and then to "merge" both.
(But with respect to the existing demo setup of IO-Link, this seems to be much more effort...).
Or is it possible to think about adding IO-Link only in a file based manner?
But therefore its necessary to have detailed knowledge about the build setup.
Any help welcome,
Thomas