This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3358: DCAN loopback questions

Part Number: AM3358

There are two types of loopback supported in AM335x. (1) Loopback(Internal) and (2) External Loopback.

This question pertains to both loopback types: Does DCAN module set RXOK bit in ES register when any of the loopback modes are enabled ?

It was observed on AM3358 and J6 processors that RXOK bit works as expected when DCAN is operating in normal mode but the DCAN module does not set(or reset) RXOK when internal loopback mode is enabled. AM335x TRM document does not talk anything about this. 

Does TI have any documentation(other than TRM) on what all things that DCAN module do and don't do when loopback mode is enabled/disabled.