Part Number: AM5728
Tool/software: TI C/C++ Compiler
hello
I want to build linux processor SDK 06.00.00.07 for AM5728.
I have done all steps mentioned in Processor SDK Linux Documentation. (http://software-dl.ti.com/processor-sdk-linux/esd/docs/latest/linux/index.html).
in last step (MACHINE=am57xx-evm bitbake arago-base-tisdk-image), following warnings and Errors appear:
sitara@myTI:~/tisdk/build$ MACHINE=am57xx-evm bitbake arago-base-tisdk-image
WARNING: Layer meta-processor-sdk should set LAYERSERIES_COMPAT_meta-processor-sdk in its conf/layer.conf file to list the core layer names it is compatible with.
WARNING: Layer browser-layer should set LAYERSERIES_COMPAT_browser-layer in its conf/layer.conf file to list the core layer names it is compatible with.
WARNING: Layer meta-processor-sdk should set LAYERSERIES_COMPAT_meta-processor-sdk in its conf/layer.conf file to list the core layer names it is compatible with.
WARNING: Layer browser-layer should set LAYERSERIES_COMPAT_browser-layer in its conf/layer.conf file to list the core layer names it is compatible with.
WARNING: You have included the meta-virtualization layer, but 'virtualization' has not been enabled in your DISTRO_FEATURES. Some bbappend files may not take effect. See the meta-virtualization README for details on enabling virtualization support.
Loading cache: 100% |############################################| Time: 0:00:01
Loaded 4697 entries from dependency cache.
WARNING: No recipes available for:
/home/sitara/tisdk/sources/meta-processor-sdk/recipes-graphics/wayland/weston_2.0.0.bbappend
/home/sitara/tisdk/sources/meta-processor-sdk/recipes-ros/navigation/move-base_1.12.14.bbappend
/home/sitara/tisdk/sources/meta-processor-sdk/recipes-ros/navigation/rotate-recovery_1.12.14.bbappend
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "1.40.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-16.04"
TARGET_SYS = "arm-linux-gnueabi"
MACHINE = "am57xx-evm"
DISTRO = "arago"
DISTRO_VERSION = "2019.05"
TUNE_FEATURES = "arm armv7a vfp thumb neon callconvention-hard"
TARGET_FPU = "hard"
meta-processor-sdk = "HEAD:e5b633c0aa6d924ab6bea15906e3790c01c86633"
meta-ros = "HEAD:72068b17e4192b51e09c8dc633805a35edac8701"
meta-arago-distro
meta-arago-extras = "HEAD:9373674c699c8ad98f8b6b3eac45473448f55e94"
meta-browser = "HEAD:26d50665e2f7223c5f4ad7481a8d2431e7cb55fb"
meta-qt5 = "HEAD:1520d5b2b2beec5e1c3209d3178219e93ef08bca"
meta-virtualization = "HEAD:bbc38dc9d6d02e73c08df289bb22a292c2264e9b"
meta-networking
meta-python
meta-oe
meta-gnome
meta-multimedia
meta-filesystems = "HEAD:9b3b907f30b0d5b92d58c7e68289184fda733d3e"
meta-ti = "HEAD:28a2f128fbadd37463060eb5ee40c7c9a47cc530"
meta-linaro-toolchain
meta-optee = "HEAD:b30036d4ef7ce9fe746833fc54de6ac7b0e00638"
meta = "HEAD:f162d5bfe6eaeca24f441c83c87252c8d05744fc"
Initialising tasks: 100% |#######################################| Time: 0:00:05
Sstate summary: Wanted 1371 Found 0 Missed 1371 Current 89 (0% match, 6% complete)
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
WARNING: external-arm-toolchain-2019.03-r0 do_fetch: Failed to fetch URL git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git;protocol=git;branch=ti-linux-4.19.y, attempting MIRRORS if available
WARNING: linux-ti-staging-4.19.38+gitAUTOINC+4dae378bbe-r7a.arago5.tisdk0.3 do_fetch: Failed to fetch URL git://git.ti.com/processor-sdk/processor-sdk-linux.git;protocol=git;branch=processor-sdk-linux-4.19.y, attempting MIRRORS if available
ERROR: external-arm-toolchain-2019.03-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export DBUS_SESSION_BUS_ADDRESS="unix:abstract=/tmp/dbus-kz5lQ5yvPk"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/home/sitara/tisdk/sources/oe-core/scripts:/home/sitara/tisdk/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/external-arm-toolchain/2019.03-r0/recipe-sysroot-native/usr/bin/arm-linux-gnueabi:/home/sitara/tisdk/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/external-arm-toolchain/2019.03-r0/recipe-sysroot/usr/bin/crossscripts:/home/sitara/tisdk/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/external-arm-toolchain/2019.03-r0/recipe-sysroot-native/usr/sbin:/home/sitara/tisdk/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/external-arm-toolchain/2019.03-r0/recipe-sysroot-native/usr/bin:/home/sitara/tisdk/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/external-arm-toolchain/2019.03-r0/recipe-sysroot-native/sbin:/home/sitara/tisdk/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/external-arm-toolchain/2019.03-r0/recipe-sysroot-native/bin:/home/sitara/gcc-arm-8.3-2019.03-x86_64-arm-linux-gnueabihf/bin:/home/sitara/tisdk/sources/bitbake/bin:/home/sitara/tisdk/build/arago-tmp-external-arm-toolchain/hosttools"; export HOME="/home/sitara"; LANG=C git -c core.fsyncobjectfiles=0 clone --bare --mirror git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git /home/sitara/tisdk/downloads/git2/git.ti.com.ti-linux-kernel.ti-linux-kernel.git --progress failed with exit code 128, output:
Cloning into bare repository '/home/sitara/tisdk/downloads/git2/git.ti.com.ti-linux-kernel.ti-linux-kernel.git'...
fatal: unable to connect to git.ti.com:
git.ti.com[0: 198.47.28.208]: errno=Connection refused
ERROR: external-arm-toolchain-2019.03-r0 do_fetch: Fetcher failure for URL: 'git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git;protocol=git;branch=ti-linux-4.19.y'. Unable to fetch URL from any source.
ERROR: external-arm-toolchain-2019.03-r0 do_fetch: Function failed: base_do_fetch
ERROR: Logfile of failure stored in: /home/sitara/tisdk/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/external-arm-toolchain/2019.03-r0/temp/log.do_fetch.14858
ERROR: Task (/home/sitara/tisdk/sources/meta-linaro/meta-linaro-toolchain/recipes-devtools/external-arm-toolchain/external-arm-toolchain.bb:do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 668 tasks of which 655 didn't need to be rerun and 2 failed.
Summary: 2 tasks failed:
/home/sitara/tisdk/sources/meta-linaro/meta-linaro-toolchain/recipes-devtools/external-arm-toolchain/external-arm-toolchain.bb:do_fetch
/home/sitara/tisdk/sources/meta-ti/recipes-kernel/linux/linux-ti-staging_4.19.bb:do_fetch
Summary: There were 8 WARNING messages shown.
Summary: There were 6 ERROR messages shown, returning a non-zero exit code.
now, I do not know what to do.
any help may be appreciated
Ali