Part Number: AM3358
Other Parts Discussed in Thread: SYSBIOS,
What step should I follow? I use XDCscript Editor to add it to cfg file. Task_create return NULL! Here is my cfg file
var Defaults = xdc.useModule('xdc.runtime.Defaults');
var Diags = xdc.useModule('xdc.runtime.Diags');
var Error = xdc.useModule('xdc.runtime.Error');
var Log = xdc.useModule('xdc.runtime.Log');
var LoggerBuf = xdc.useModule('xdc.runtime.LoggerBuf');
var Main = xdc.useModule('xdc.runtime.Main');
var Memory = xdc.useModule('xdc.runtime.Memory')
var SysMin = xdc.useModule('xdc.runtime.SysMin');
var System = xdc.useModule('xdc.runtime.System');
var Text = xdc.useModule('xdc.runtime.Text');
var Clock = xdc.useModule('ti.sysbios.knl.Clock');
var Swi = xdc.useModule('ti.sysbios.knl.Swi');
var Task = xdc.useModule('ti.sysbios.knl.Task');
var Semaphore = xdc.useModule('ti.sysbios.knl.Semaphore');
var Mailbox = xdc.useModule('ti.sysbios.knl.Mailbox');
var Hwi = xdc.useModule('ti.sysbios.hal.Hwi');
var Timer = xdc.useModule('ti.sysbios.hal.Timer');
var HeapMem = xdc.useModule('ti.sysbios.heaps.HeapMem');
var Edma = xdc.loadPackage ("ti.sdo.edma3.drv.sample");
var drv = xdc.loadPackage ("ti.sdo.edma3.drv");
var rm = xdc.loadPackage ("ti.sdo.edma3.rm");
/* ================ BIOS configuration ================ */
var BIOS = xdc.useModule('ti.sysbios.BIOS');
/*
* Build a custom SYS/BIOS library from sources.
*/
BIOS.libType = BIOS.LibType_Custom;
BIOS.customCCOpts = BIOS.customCCOpts.replace(" -g ","");
BIOS.assertsEnabled = false;
BIOS.logsEnabled = false;
BIOS.swiEnabled = false;
/*
* The BIOS module will create the default heap for the system.
* Specify the size of this default heap.
*/
BIOS.heapSize = 0x8000;
Swi.common$.namedInstance = true;
Program.sectionsExclude = ".*";
Clock.tickPeriod = 1000;
Hwi.dispatcherSwiSupport = true;
Hwi.dispatcherTaskSupport = true;
Hwi.dispatcherAutoNestingSupport = true;
Task.enableIdleTask = false;
Task.initStackFlag = false;
Task.checkStackFlag = false;
/* ================ Driver configuration ================ */
/* Load the Osal package */
var osType = "tirtos";
var Osal = xdc.loadPackage('ti.osal');
Osal.Settings.osType = osType;
/*use CSL package*/
var socType = "am335x";
var Csl = xdc.loadPackage('ti.csl');
Csl.Settings.deviceType = socType;
/* Load the driver packages, starting with mcasp */
var McASP = xdc.loadPackage('ti.drv.mcasp');
McASP.Settings.socType = socType;
/* Load the spi package */
var Spi = xdc.loadPackage('ti.drv.spi');
Spi.Settings.socType = socType;
/* Load the I2C package */
var I2C = xdc.loadPackage('ti.drv.i2c');
I2C.Settings.socType = socType;
/* Load the uart package */
var Uart = xdc.loadPackage('ti.drv.uart');
Uart.Settings.socType = socType;
/* Load the board package */
var Board = xdc.loadPackage('ti.board');
Board.Settings.boardName = "bbbAM335x";
/* Load Profiling package */
var Utils = xdc.loadPackage('ti.utils.profiling');
/* Load the gpio package */
var Gpio = xdc.loadPackage('ti.drv.gpio');
Gpio.Settings.socType = socType;
Gpio.Settings.enableProfiling = true;
/* ================ Cache and MMU configuration ================ */
var Cache = xdc.useModule('ti.sysbios.family.arm.a8.Cache');
Cache.enableCache = true;
var Mmu = xdc.useModule('ti.sysbios.family.arm.a8.Mmu');
Mmu.enableMMU = true;
/* Force peripheral section to be NON cacheable strongly-ordered memory */
var peripheralAttrs = {
type : Mmu.FirstLevelDesc_SECTION, // SECTION descriptor
tex: 0,
bufferable : false, // bufferable
cacheable : false, // cacheable
shareable : false, // shareable
noexecute : true, // not executable
};
/* Define the base address of the 1 Meg page the peripheral resides in. */
var peripheralBaseAddr = 0x44e00400;;
/* Configure the corresponding MMU page descriptor accordingly */
Mmu.setFirstLevelDescMeta(peripheralBaseAddr,
peripheralBaseAddr,
peripheralAttrs);
/* Define the base address of the 1 Meg page the peripheral resides in. */
var peripheralBaseAddr = 0x481a6000;
/* Configure the corresponding MMU page descriptor accordingly */
Mmu.setFirstLevelDescMeta(peripheralBaseAddr,
peripheralBaseAddr,
peripheralAttrs);
/*
* Uncomment this line to globally disable Asserts.
* All modules inherit the default from the 'Defaults' module. You
* can override these defaults on a per-module basis using Module.common$.
* Disabling Asserts will save code space and improve runtime performance.
*/
/*Defaults.common$.diags_ASSERT = Diags.ALWAYS_OFF; */
/*
* Uncomment this line to keep module names from being loaded on the target.
* The module name strings are placed in the .const section. Setting this
* parameter to false will save space in the .const section. Error and
* Assert messages will contain an "unknown module" prefix instead
* of the actual module name.
Defaults.common$.namedModule = false;
*/
/*
* Minimize exit handler array in System. The System module includes
* an array of functions that are registered with System_atexit() to be
* called by System_exit().
*/
System.maxAtexitHandlers = 4;
/*
* Uncomment this line to disable the Error print function.
* We lose error information when this is disabled since the errors are
* not printed. Disabling the raiseHook will save some code space if
* your app is not using System_printf() since the Error_print() function
* calls System_printf().
Error.raiseHook = null;
*/
/*
* Uncomment this line to keep Error, Assert, and Log strings from being
* loaded on the target. These strings are placed in the .const section.
* Setting this parameter to false will save space in the .const section.
* Error, Assert and Log message will print raw ids and args instead of
* a formatted message.
Text.isLoaded = false;
*/
/*
* Uncomment this line to disable the output of characters by SysMin
* when the program exits. SysMin writes characters to a circular buffer.
* This buffer can be viewed using the SysMin Output view in ROV.
SysMin.flushAtExit = false;
*/
/* System stack size (used by ISRs and Swis) */
Program.stack = 0x4000;
/* Circular buffer size for System_printf() */
SysMin.bufSize = 0x200;
/*
* Create and install logger for the whole system
*/
var loggerBufParams = new LoggerBuf.Params();
loggerBufParams.numEntries = 16;
var logger0 = LoggerBuf.create(loggerBufParams);
Defaults.common$.logger = logger0;
Main.common$.diags_INFO = Diags.ALWAYS_ON;
System.SupportProxy = SysMin;
var timer0Params = new Timer.Params();
timer0Params.instance.name = "timer0";
Program.global.timer0 = Timer.create(null, null, timer0Params);
I have no clue what is going wrong? What should I do to fix it? My project use driver UART, SPI, maybe McASP, GPIO and I2C. Thanks