This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI。
I set board boot from emmc.
but when I want to dvr in the sd card, then i plug the sd card ,the board can not boot from emmc,because it think the sd card is boot deviece.how can i slove it.(sd card is empty,so that has no boot file in the sd card).
my boot mode is : support boot from sd ,emmc .
Hi,
can you share which SYSBOOT settings you use for emmc boot?
Regards,
Yordan
Hi,
can you try to set sysboot [5:0] to 000111.
Your value sets the boot order to USB -> SD card -> eMMC, you can look at "Table 29-9. Booting Devices Order" in device's TRM:
Regards,
Yordan