This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3359: U-boot issue on custom board

Part Number: AM3359

Hello,

We are trying to bring-up a custom board based on AM3359.

SD card is on MMC0 and the strap option is set for boot from MMC0 priority.

Issue is console message stops after the first line and does not move forward.  See below:

U-Boot SPL 2013.07 (Nov 01 2019 - 10:22:33)

>>spl:board_init_r()

boot device - 8


After this message stops.

I probed the hardware lines on the board and there is activity on CLK, CMD and all the DAT lines.

Any help will be appreciated.

Thanks

Vijay