Part Number: PROCESSOR-SDK-DRA7X
Tool/software: TI C/C++ Compiler
Hello,
I need to solve this issue which I have got at the moment on J6. It was successful that I boot linux kernel from SD card and it can mount root file system .
The issue I am facing is that unabashed to mount the root file system when the boot mode was emmc boot mode. And this work refer to this http://processors.wiki.ti.com/index.php/Processor_SDK_Linux_Automotive_Software_Developers_Guide#Using_eMMC_Boot .
I see this fragment in the log:
[ 2.304766] ALSA device list:
[ 2.307743] #0: DRA7xx-EVM
[ 2.310645] #1: HDMI 58040000.encoder
[ 2.314491] #2: DRA7xx-JAMR3
[ 2.318230] VFS: PARTUUID= is invalid.
[ 2.318230] Expected PARTUUID=<valid-uuid-id>[/PARTNROFF=%d]
[ 2.327708] Disabling rootwait; root= is invalid.
[ 2.332711] VFS: Cannot open root device "PARTUUID=" or unknown-block(0,0): error -6
[ 2.340532] Please append a correct "root=" boot option; here are the available partitions:
[ 2.348944] 1f00 256 mtdblock0 (driver?)
[ 2.354077] 1f01 1024 mtdblock1 (driver?)
[ 2.359188] 1f02 512 mtdblock2 (driver?)
[ 2.364382] 1f03 64 mtdblock3 (driver?)
[ 2.369465] 1f04 64 mtdblock4 (driver?)
[ 2.374566] 1f05 8192 mtdblock5 (driver?)
[ 2.379646] 1f06 22656 mtdblock6 (driver?)
[ 2.384742] b300 7602176 mmcblk0 driver: mmcblk
[ 2.390086] b301 65536 mmcblk0p1 5181ef41-01
[ 2.395444] b302 7527176 mmcblk0p2 5181ef41-02
[ 2.400800] b320 8192 mmcblk0boot1 (driver?)
[ 2.406142] b310 8192 mmcblk0boot0 (driver?)
[ 2.411492] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
But,if the SD card is plugged in the board ,the board can boot linux kernel from emmc and mount root file system.