(This is a breakout thread from http://e2e.ti.com/support/embedded/f/356/p/86363/298144.aspx#298144)
I need to get the DM6467T EVM (and eventually my own custom DM6467T board) booting from NAND with a small file system also in NAND.
Should I "develop" new small file system on hard disk first, then migrate file system to NAND? Or is there no advantage there (but disadvantage of possible need to restore hard drive)?
Note that it's my understanding that the DM64676T EVM (aka Spectrum Digital HD1080P) comes booting from NAND, but uses a file system on the hard drive. My own custom DM6467T in prototype assembly right now, does not have a hard disk, so the small file system needs to be elsewhere. Note I do have both NAND and I2C EEPROM. I assume the I2C EEPROM is too tiny.
Thanks,
Helmut