This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The customer wants to switch two kinds of sysboot below, it depends on their some products.
Sysboot[5:0] = 0b00 0101
Sysboot[5:0] = 0b11 0101
In order to change the above sysboots without layout change, they’re considering to add another pull-down register on sysboot[4] or [5] to change from pull-up to pull-down as follows.
In the case of 0b11 0101, both 3.6k ohm pull-up register and 10k ohm pull-down register are connected on each sysboot[5] and [4] pin as pull-up.
For the case of 0b00 0101, 1.2k ohm pull-down register is added in parallel to ensure 1.07k ohm pull-down register (10k + 1.2k in parallel) on each sysboot[5] and [4] pin.
Is this no problem ?
Regards,
Hideaki
Hi,
The SYSBOOT pins have Dual Voltage LVCMOS I/O buffers. You must ensure that the resistive dividers meet the required input level thresholds listed in Table 5-17 from the AM572x Datasheet SR2.0 Rev. F. Note that there are different input level thresholds depending on the supply voltage for the I/O cells.