If I set MAR as below,I can use IPC to communicate with Linux A72.
But if I set MAR as following, Linux will not find char device "rpmsg_chrdev", so that I can not communicate with Linux A72
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If I set MAR as below,I can use IPC to communicate with Linux A72.
But if I set MAR as following, Linux will not find char device "rpmsg_chrdev", so that I can not communicate with Linux A72
See vision_apps/apps/basic_demos/app_tirtos/tirtos_linux/c66x_1/main.c, appCacheMarInit
/* enable cache for cached sections */
Cache_setMar((Ptr)DDR_C66x_1_DTS_ADDR, DDR_C66x_1_DTS_SIZE, Cache_Mar_ENABLE);
Cache_setMar((Ptr)DDR_SHARED_MEM_ADDR, DDR_SHARED_MEM_SIZE, Cache_Mar_ENABLE);
/* disable cache for non-cached sections */
Cache_setMar((Ptr)DDR_C66x_1_IPC_ADDR, DDR_C66x_1_IPC_SIZE, Cache_Mar_DISABLE);
Cache_setMar((Ptr)APP_LOG_MEM_ADDR, APP_LOG_MEM_SIZE, Cache_Mar_DISABLE);
Cache_setMar((Ptr)TIOVX_OBJ_DESC_MEM_ADDR, TIOVX_OBJ_DESC_MEM_SIZE, Cache_Mar_DISABLE);
Cache_setMar((Ptr)IPC_VRING_MEM_ADDR, IPC_VRING_MEM_SIZE, Cache_Mar_DISABLE);
Mar_ENABLE enables cache for these regions.
Mar_DISABLE disables cache for these regions.
Note, the below contraints though,
- region start address MUST be 16MB aligned
- region size MUST be 16MB aligned.
i.e you can enable or disable cache in units of 16MB
regards
Kedar