Referring to the thread title, i have here a bunch of buffer models for one of the pins of the TDA3LX.
SR000_DRV48_1P8_M#100
SR011_DRV40_1P8_M#101
SR010_DRV40_1P8_M#102 and etc....
I have a few questions regarding these buffer models:
1) If i would like to run a signal integrity simulation, for a DDR3L SRAM I/O type of trace, which models do i choose? (I have other buffer names that don't start with SRXXXX, but are DDR3L_ODT_60_1P5_M#118, DDR3_ODT_120_1P5_M#120 etc, so am looking for something like a general guideline to choosing buffer models.)
2) If the standard termination value is recommended to be 50ohms, should a 40 ohm or 60 ohm, or even higher, be chosen? (The list i have doesn't show any buffers with a 50 ohm termination, be it on die or without on-die termination?
3) What is the standard procedure in selecting the MOST appropriate buffer model for a selected trace such as the the mentioned DDR3 trace?
Thanks.