Part Number: AM3352
Hi,
I am using U-Boot 2019.01 from ti-processor-sdk-linux-am335x-evm-06.00.00.07 on our custom board.
We are not using RTC. Hence I commented out all the RTC access related code from board.c file. I am getting following data abort error:
I am not using FDT booting. Anyway I have removed RTC node from am33xx.dtsi.
U-Boot SPL 2019.01-g8b90adfb16 (Mar 06 2020 - 14:13:42 +0530)
Trying to boot from MMC1
U-Boot 2019.01-g8b90adfb16 (Mar 06 2020 - 14:13:42 +0530)
CPU : AM335X-GP rev 2.1
Model: TI AM335x EVM
DRAM: 1 GiB
NAND: 256 MiB
MMC: OMAP SD/MMC: 0
Loading Environment from FAT... *** Warning - bad CRC, using default environment
<ethaddr> not set. Validating first E-fuse MAC
Returning from board_late_init *********
Net: Returning from eth_post_probe() ****
eth0: ethernet@4a100000
Warning: usb_ether MAC addresses don't match:
Address in ROM is de:ad:be:ef:00:01
Address in environment is f4:84:4c:2f:a5:f8
Returning from eth_post_probe() ****
, eth1: usb_ether
data abort
pc : [<bff85134>] lr : [<bff77753>]
reloc pc : [<8081c134>] lr : [<8080e753>]
sp : bdf3a948 ip : bdf3a8a0 fp : 80800020
r10: 00000017 r9 : bdf48eb8 r8 : 81fffee0
r7 : bffcbd54 r6 : bffcbcbc r5 : bffcbd58 r4 : 3f769000
r3 : 44e3e000 r2 : b0010000 r1 : bffcbd84 r0 : 00000000
Flags: nZcv IRQs off FIQs on Mode SVC_32
Code: 44e3e000 83e70b13 95a4f1e0 4a064b05 (ba006e98)
Resetting CPU ...
resetting ...
I am able to boot successfully using U-Boot 2013 from ti sdk 7.0
What could be causing data abort error ?
Regards,
Pranay