Other Parts Discussed in Thread: SYSBIOS
Hi TI members:
I study the thread https://e2e.ti.com/support/processors/f/791/p/862675/3190807?tisearch=e2e-sitesearch&keymatch=mcu_mcan0#3190807
there are two things I have questions form Karan Saxena's reply
1. >> There is no driver for CAN on TDA4VM/J721EX as of now.
I grep the mcu_mcan related word in Linux / Uboot dts table in 06_02_sdk, but still no-thing find.
so it mean we still only can control can bus through R5F in main domain/mcu domain not A72, right?
2. >> Both the mcu1_0 and mcu2_1 can control all CAN instances - the SDK has example running on mcu1_0 where you can control the MCU_MCAN0 and MCU_MCAN1.
Can you give more information abou "the SDK has example", like path in SDK...
right now, I only find below adaptor in Processor SDK Linux Automotive
4.1.1. CAN-Ethernet Gateway demo
but it use mcan4 & mcan9 in main-domain. not mcu_mcan0 & mcu_mcan1.
Is it the same thing of "the SDK has example"?
3. >> mcan_evm_loopback_app_main_k3.c
does ti have related documents to explain how to use this loopback tool?
Can it use to test MCU_MCAN0 & MCU_MCAN1?
BR
Sentinen Chen