This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear experts,
We ran into a issue that rtos decoder graph verify failed.
Reproduce steps are:
(PSDKRA 6.2 version on TDA4VMXEVM)
1. run "VX_TEST_DATA_PATH=/opt/vision_apps/test_data ./vx_app_conformance.out --filter=tivxHwaVideoDecoder.MultiStreamProcessing" for at least 3~5 times.
2. you will see "[ FAILED ] 1 test(s)"
Here is my log: from TIOVX
118.037524 s: VX_ZONE_INFO:[ownGraphScheduleGraph:763] Scheduling Graph (graph=13, pipe=0) 118.037578 s: VX_ZONE_INFO:[ownNodeKernelSchedule:570] Scheduling Node (node=8, pipe=0) 118.037607 s: VX_ZONE_INFO:[ownNodeKernelSchedule:570] Scheduling Node (node=7, pipe=0) 118.072115 s: VX_ZONE_INFO:[ownCheckGraphCompleted:676] Graph Completed (graph=13, pipe=0) 118.072144 s: VX_ZONE_INFO:[ownCheckGraphCompleted:701] All Graphs Completed 118.717528 s: VX_ZONE_INFO:[ownGraphScheduleGraph:763] Scheduling Graph (graph=13, pipe=0) 118.717550 s: VX_ZONE_INFO:[ownNodeKernelSchedule:570] Scheduling Node (node=8, pipe=0) 118.717595 s: VX_ZONE_INFO:[ownNodeKernelSchedule:570] Scheduling Node (node=7, pipe=0) 118.752087 s: VX_ZONE_INFO:[ownCheckGraphCompleted:676] Graph Completed (graph=13, pipe=0) 118.752116 s: VX_ZONE_INFO:[ownCheckGraphCompleted:701] All Graphs Completed 119.485541 s: VX_ZONE_INFO:[ownGraphScheduleGraph:763] Scheduling Graph (graph=13, pipe=0) 119.485561 s: VX_ZONE_INFO:[ownNodeKernelSchedule:570] Scheduling Node (node=8, pipe=0) 119.485608 s: VX_ZONE_INFO:[ownNodeKernelSchedule:570] Scheduling Node (node=7, pipe=0) 119.520099 s: VX_ZONE_INFO:[ownCheckGraphCompleted:676] Graph Completed (graph=13, pipe=0) 119.520127 s: VX_ZONE_INFO:[ownCheckGraphCompleted:701] All Graphs Completed 120.309507 s: VX_ZONE_INFO:[ownGraphScheduleGraph:763] Scheduling Graph (graph=13, pipe=0) 120.309529 s: VX_ZONE_INFO:[ownNodeKernelSchedule:570] Scheduling Node (node=8, pipe=0) 120.309574 s: VX_ZONE_INFO:[ownNodeKernelSchedule:570] Scheduling Node (node=7, pipe=0) 120.343900 s: VX_ZONE_INFO:[ownCheckGraphCompleted:676] Graph Completed (graph=13, pipe=0) 120.343928 s: VX_ZONE_INFO:[ownCheckGraphCompleted:701] All Graphs Completed 121.125495 s: VX_ZONE_INFO:[ownGraphScheduleGraph:763] Scheduling Graph (graph=13, pipe=0) 121.125516 s: VX_ZONE_INFO:[ownNodeKernelSchedule:570] Scheduling Node (node=8, pipe=0) 121.125559 s: VX_ZONE_INFO:[ownNodeKernelSchedule:570] Scheduling Node (node=7, pipe=0) 121.160043 s: VX_ZONE_INFO:[ownCheckGraphCompleted:676] Graph Completed (graph=13, pipe=0) 121.160072 s: VX_ZONE_INFO:[ownCheckGraphCompleted:701] All Graphs Completed 122.094723 s: VX_ZONE_INFO:[tivxQueueDelete:182] tivxQueueDelete: if this hangs, please ensure all application threads have been destroyed 122.095337 s: VX_ZONE_INFO:[tivxQueueDelete:182] tivxQueueDelete: if this hangs, please ensure all application threads have been destroyed 122.095371 s: VX_ZONE_INFO:[tivxQueueDelete:182] tivxQueueDelete: if this hangs, please ensure all application threads have been destroyed [ DONE ] tivxHwaVideoDecoder.MultiStreamProcessing [ -------- ] 1 tests from test case tivxHwaVideoDecoder [ ======== ] [ ALL DONE ] 1 test(s) from 1 test case(s) ran [ PASSED ] 1 test(s) [ FAILED ] 0 test(s) [ DISABLED ] 0 test(s) ================================= OpenVX Conformance report summary ================================= To be conformant to the OpenVX baseline, 1 required test(s) must pass. 1 tests passed, 0 tests failed. PASSED. To be conformant to the User Data Object extension, 0 required test(s) must pass. 0 tests passed, 0 tests failed. PASSED. Note: The 0 disabled tests are optional and are not considered for conformance. #REPORT: YYYYMMDDHHMMSS FILTERED 21932 0 1 1 1 0 (version 1.1-20170301) 122.105486 s: VX_ZONE_INIT:[tivxHostDeInit:49] De-Initialization Done for HOST !!! 122.106599 s: VX_ZONE_INFO:[tivxQueueDelete:182] tivxQueueDelete: if this hangs, please ensure all application threads have been destroyed 122.107671 s: VX_ZONE_INFO:[tivxQueueDelete:182] tivxQueueDelete: if this hangs, please ensure all application threads have been destroyed 122.108738 s: VX_ZONE_INFO:[tivxQueueDelete:182] tivxQueueDelete: if this hangs, please ensure all application threads have been destroyed 122.109804 s: VX_ZONE_INFO:[tivxQueueDelete:182] tivxQueueDelete: if this hangs, please ensure all application threads have been destroyed 122.109849 s: VX_ZONE_INIT:[tivxDeInit:100] De-Initialization Done !!! APP: Deinit ... !!! REMOTE_SERVICE: Deinit ... !!! REMOTE_SERVICE: Deinit ... Done !!! IPC: Deinit ... !!! IPC: DeInit ... Done !!! MEM: Deinit ION ... !!! MEM: Alloc's: 11 alloc's of 8986376 bytes MEM: Free's : 11 free's of 8986376 bytes MEM: Open's : 0 allocs of 0 bytes MEM: Deinit ION ... Done !!! APP: Deinit ... Done !!! root@j7-evm:/opt/vision_apps# VX_TEST_DATA_PATH=/opt/vision_apps/test_data ./vx_app_conformance.out --filter=tivxHwaVideoDecoder.MultiStreamProcessing APP: Init ... !!! APP_LOG: Mapping 0xac000000 ... APP_LOG: Mapped 0xac000000 -> 0xffff8b0f0000 of size 262144 bytes MEM: Init ION ... !!! MEM: Initialized ION (fd=4) !!! MEM: Init ION ... Done !!! IPC: Init ... !!! APP_LOG: Mapping 0xac040000 ... APP_LOG: Mapped 0xac040000 -> 0xffff89150000 of size 33161216 bytes APP_LOG: Mapping 0x30e00000 ... APP_LOG: Mapped 0x30e00000 -> 0xffff8b5e0000 of size 3072 bytes IPC: Init ... Done !!! REMOTE_SERVICE: Init ... !!! REMOTE_SERVICE: Init ... Done !!! APP: Init ... Done !!! 0.000913 s: VX_ZONE_INIT:Enabled 0.000921 s: VX_ZONE_ERROR:Enabled 0.000925 s: VX_ZONE_WARNING:Enabled 0.000929 s: VX_ZONE_INFO:Disabled 0.001806 s: VX_ZONE_INIT:[tivxInit:64] Initialization Done !!! 0.002183 s: VX_ZONE_INIT:[tivxHostInit:44] Initialization Done for HOST !!! VxTests version: 1.1-20170301 VCS version: unknown Build config: Release [ ======== ] Total 21932 tests from 144 test cases Use test filter: tivxHwaVideoDecoder.MultiStreamProcessing Use global OpenVX context: FALSE [ -------- ] tests from tivxHwaVideoDecoder [ RUN 0001 ] tivxHwaVideoDecoder.MultiStreamProcessing ... 0.015868 s: VX_ZONE_PARAMETER:[vxSetParameterByIndex:203] Attempting to set parameter[0] on com.ti.hwa.video_decoder (enum:-2097101) to 0xb075c0 0.015891 s: VX_ZONE_PARAMETER:[vxSetParameterByIndex:236] Query returned type 00000816 for ref 0xb075c0 0.015899 s: VX_ZONE_PARAMETER:[vxSetParameterByIndex:302] Assigned Node[0] 0xadafc0 type:00000816 ref=0xb075c0 0.015904 s: VX_ZONE_PARAMETER:[vxSetParameterByIndex:203] Attempting to set parameter[1] on com.ti.hwa.video_decoder (enum:-2097101) to 0xb07a00 0.015910 s: VX_ZONE_PARAMETER:[vxSetParameterByIndex:236] Query returned type 00000816 for ref 0xb07a00 0.016055 s: VX_ZONE_PARAMETER:[vxSetParameterByIndex:302] Assigned Node[1] 0xadafc0 type:00000816 ref=0xb07a00 0.016066 s: VX_ZONE_PARAMETER:[vxSetParameterByIndex:203] Attempting to set parameter[2] on com.ti.hwa.video_decoder (enum:-2097101) to 0xb396c0 0.016072 s: VX_ZONE_PARAMETER:[vxSetParameterByIndex:236] Query returned type 0000080f for ref 0xb396c0 0.016077 s: VX_ZONE_PARAMETER:[vxSetParameterByIndex:302] Assigned Node[2] 0xadafc0 type:0000080f ref=0xb396c0 0.016112 s: VX_ZONE_PARAMETER:[vxSetParameterByIndex:203] Attempting to set parameter[0] on com.ti.hwa.video_decoder (enum:-2097101) to 0xb077e0 0.016118 s: VX_ZONE_PARAMETER:[vxSetParameterByIndex:236] Query returned type 00000816 for ref 0xb077e0 0.016123 s: VX_ZONE_PARAMETER:[vxSetParameterByIndex:302] Assigned Node[0] 0xadb290 type:00000816 ref=0xb077e0 0.016128 s: VX_ZONE_PARAMETER:[vxSetParameterByIndex:203] Attempting to set parameter[1] on com.ti.hwa.video_decoder (enum:-2097101) to 0xb07c20 0.016133 s: VX_ZONE_PARAMETER:[vxSetParameterByIndex:236] Query returned type 00000816 for ref 0xb07c20 0.016139 s: VX_ZONE_PARAMETER:[vxSetParameterByIndex:302] Assigned Node[1] 0xadb290 type:00000816 ref=0xb07c20 0.016144 s: VX_ZONE_PARAMETER:[vxSetParameterByIndex:203] Attempting to set parameter[2] on com.ti.hwa.video_decoder (enum:-2097101) to 0xb39978 0.016149 s: VX_ZONE_PARAMETER:[vxSetParameterByIndex:236] Query returned type 0000080f for ref 0xb39978 0.016154 s: VX_ZONE_PARAMETER:[vxSetParameterByIndex:302] Assigned Node[2] 0xadb290 type:0000080f ref=0xb39978 0.086957 s: VX_ZONE_INFO:[ownGraphNodeKernelInit:578] kernel init for node 0, kernel com.ti.hwa.video_decoder ... 0.086975 s: VX_ZONE_INFO:[ownGraphNodeKernelInit:589] kernel init for node 0, kernel com.ti.hwa.video_decoder ... done !!! 0.146141 s: VX_ZONE_ERROR:[ownContextSendCmd:553] Command ack message returned failure cmd_status: -1 0.146148 s: VX_ZONE_ERROR:[ownNodeKernelInit:486] Target kernel, TIVX_CMD_NODE_CREATE failed 0.146153 s: VX_ZONE_INFO:[ownGraphNodeKernelInit:578] kernel init for node 1, kernel com.ti.hwa.video_decoder ... 0.146158 s: VX_ZONE_ERROR:[ownGraphNodeKernelInit:583] kernel init for node 1, kernel com.ti.hwa.video_decoder ... failed !!! 0.146164 s: VX_ZONE_ERROR:[vxVerifyGraph:2010] Node kernel init failed 0.146169 s: VX_ZONE_ERROR:[vxVerifyGraph:2064] Graph verify failed FAILED at /work/j7/6.2/psdk_rtos_auto_j7_06_02_00_21/tiovx/kernels_j7/hwa/test/test_video_decoder.c:549 Expected: VX_SUCCESS == vxVerifyGraph(graph) Actual: VX_SUCCESS != VX_FAILURE 0.183689 s: VX_ZONE_WARNING:[vxReleaseContext:743] Stale reference 0xb075c0 of type 00000816 at external count 1, internal count 1 0.183697 s: VX_ZONE_WARNING:[vxReleaseContext:746] Unreleased reference name = user_data_object_84 0.183702 s: VX_ZONE_WARNING:[vxReleaseContext:743] Stale reference 0xb077e0 of type 00000816 at external count 1, internal count 1 0.183707 s: VX_ZONE_WARNING:[vxReleaseContext:746] Unreleased reference name = user_data_object_85 0.183712 s: VX_ZONE_WARNING:[vxReleaseContext:743] Stale reference 0xb07a00 of type 00000816 at external count 1, internal count 1 0.183716 s: VX_ZONE_WARNING:[vxReleaseContext:746] Unreleased reference name = user_data_object_86 0.183721 s: VX_ZONE_WARNING:[vxReleaseContext:743] Stale reference 0xb07c20 of type 00000816 at external count 1, internal count 1 0.183725 s: VX_ZONE_WARNING:[vxReleaseContext:746] Unreleased reference name = user_data_object_87 0.183730 s: VX_ZONE_WARNING:[vxReleaseContext:743] Stale reference 0xb396c0 of type 0000080f at external count 1, internal count 1 0.183735 s: VX_ZONE_WARNING:[vxReleaseContext:746] Unreleased reference name = image_88 0.183740 s: VX_ZONE_WARNING:[vxReleaseContext:743] Stale reference 0xb39978 of type 0000080f at external count 1, internal count 1 0.183744 s: VX_ZONE_WARNING:[vxReleaseContext:746] Unreleased reference name = image_89 0.183749 s: VX_ZONE_WARNING:[vxReleaseContext:743] Stale reference 0xa9af20 of type 00000802 at external count 1, internal count 0 0.183753 s: VX_ZONE_WARNING:[vxReleaseContext:746] Unreleased reference name = graph_90 0.183995 s: VX_ZONE_INFO:[tivxQueueDelete:182] tivxQueueDelete: if this hangs, please ensure all application threads have been destroyed 0.184038 s: VX_ZONE_INFO:[tivxQueueDelete:182] tivxQueueDelete: if this hangs, please ensure all application threads have been destroyed 0.184048 s: VX_ZONE_INFO:[tivxQueueDelete:182] tivxQueueDelete: if this hangs, please ensure all application threads have been destroyed [ !FAILED! ] tivxHwaVideoDecoder.MultiStreamProcessing [ -------- ] 1 tests from test case tivxHwaVideoDecoder [ ======== ] [ ALL DONE ] 1 test(s) from 1 test case(s) ran [ PASSED ] 0 test(s) [ FAILED ] 1 test(s), listed below: [ FAILED ] tivxHwaVideoDecoder.MultiStreamProcessing [ DISABLED ] 0 test(s) ================================= OpenVX Conformance report summary ================================= To be conformant to the OpenVX baseline, 1 required test(s) must pass. 0 tests passed, 1 tests failed. FAILED. To be conformant to the User Data Object extension, 0 required test(s) must pass. 0 tests passed, 0 tests failed. PASSED. Note: The 0 disabled tests are optional and are not considered for conformance. #REPORT: YYYYMMDDHHMMSS FILTERED 21932 0 1 1 0 1 (version 1.1-20170301) 0.193843 s: VX_ZONE_INIT:[tivxHostDeInit:49] De-Initialization Done for HOST !!! 0.194946 s: VX_ZONE_INFO:[tivxQueueDelete:182] tivxQueueDelete: if this hangs, please ensure all application threads have been destroyed 0.196018 s: VX_ZONE_INFO:[tivxQueueDelete:182] tivxQueueDelete: if this hangs, please ensure all application threads have been destroyed 0.197085 s: VX_ZONE_INFO:[tivxQueueDelete:182] tivxQueueDelete: if this hangs, please ensure all application threads have been destroyed 0.198151 s: VX_ZONE_INFO:[tivxQueueDelete:182] tivxQueueDelete: if this hangs, please ensure all application threads have been destroyed 0.198194 s: VX_ZONE_INIT:[tivxDeInit:100] De-Initialization Done !!! APP: Deinit ... !!! REMOTE_SERVICE: Deinit ... !!! REMOTE_SERVICE: Deinit ... Done !!! IPC: Deinit ... !!! IPC: DeInit ... Done !!! MEM: Deinit ION ... !!! MEM: Alloc's: 12 alloc's of 8986632 bytes MEM: Free's : 12 free's of 8986632 bytes MEM: Open's : 0 allocs of 0 bytes MEM: Deinit ION ... Done !!! APP: Deinit ... Done !!! root@j7-evm:/opt/vision_apps#
Another log from my own app, FYI:
202004142219-multi-decode-error.log
Thanks & Best Regards!
ZM
Hi ZM,
Can you provide a full log from boot to the end of the test? Also, this issue starts occurring only after a few runs, is that correct?
Thanks,
David
Hi David,
I am attaching the logs.
I am able to reproduce the issue. 4th time i ran the command:
VX_TEST_DATA_PATH=/opt/vision_apps/test_data ./vx_app_conformance.out --filter=tivxHwaVidDecoder.MultiStreamProcessing
Regards,
Keerthy
root@j7-evm:/opt/vision_apps# VX_TEST_DATA_PATH=/opt/vision_apps/test_data ./vx_app_conformance.out --filter=tivxHwaVideoDecoder.MultiStreamProcessing APP: Init ... !!! APP_LOG: Mapping 0xac000000 ... APP_LOG: Mped 0xac000000 -> 0xffffa4440000 of size 262144 bytes MEM: Iit ION ... !!! MEM: Initialized ION (fd=4) !!! MEM: Init ION.. Done !!! IPC: Init ... !!! APP_LOG: Mapping 0xac040000 .. APP_LOG: Mapped 0xac040000 -> 0xffffa24a0000 of size 33161216 bytes APP_LOG: Mapping 0x30e00000 ... APP_LOG: Mappe0x30e00000 -> 0xffffa4930000 of size 3072 bytes IPC: Init ..Done !!! REMOTE_SERVICE: Init ... !!! REMOTE_SERVICE: Init ... Done !!! APP: Init ... Done !!! 0.015201 s: VZONE_INIT:Enabled 0.015214 s: VX_ZONE_ERROR:Enabled 0.015218 s: VX_ZONE_WARNING:Enabled 0.017453 s: VX_ZONE_INIT:[tivxInit:64] Initialization Done !!! 0.0179 s: VX_ZONE_INIT:[tivxHostInit:44] Initialization Done for HT !!! VxTests version: 1.1-20170301 VCS version: unknown Build config: Release [ ======== ] Total 21932 tests from 144 test cases Use test filter: tivxHwaVideoDecoder.MtiStreamProcessing Use global OpenVX context: FALSE [ -------- ] tests from tivxHwaVideoDecoder [ RUN 0001 ] tivxaVideoDecoder.MultiStreamProcessing ... [ 133.333456] ion_buffer_destroy: buffer still mapped in the rnel [ DONE ] tivxHwaVideoDecoder.MultiStreamProcessing -------- ] 1 tests from test case tivxHwaVideoDecoder [ ======== ] [ ALL DE ] 1 test(s) from 1 test case(s) ran [ PASSED ] 1 test(s) [ ILED ] 0 test(s) [ DISABLED ] 0 test(s) =============================== OpenVX Conformance report summary ================================= To be conformant to the OpenVbaseline, 1 required test(s) must pass. 1 tests passed, 0 testfailed. PASSED. To be conformant to the User Data Object extension, 0 required test(s) must pass. 0 tests passed, 0 tts failed. PASSED. Note: The 0 disabled tests are optional anare not considered for conformance. #REPORT: YYYYMMDDHHMMSS FILTERED 21932 0 1 1 1 0 (version 1.1-20170301) 48.5891 s: VX_ZONE_INIT:[tivxHostDeInit:49] De-Initialization Do for HOST !!! 48.190236 s: VX_ZONE_INIT:[tivxDeInit:100] De-Initialization Done !!! APP: Deinit ... !!! REMOTEERVICE: Deinit ... !!! REMOTE_SERVICE: Deinit ... Done !!! I: Deinit ... !!! IPC: DeInit ... Done !!! MEM: Deinit ION ... !!! MEM: Alloc's: 11 alloc's of 8986376 bytes MEM: Fe's : 11 free's of 8986376 bytes MEM: Open's : 0 allocs of bytes MEM: Deinit ION ... Done !!! APP: Deinit ... Done !!! root@j7-evm:/opt/vision_apps# root@j7-evm:/opt/vision_apps# root@j7-evm:/opt/vision_apps# VX_TEST_DATA_PATH=/opt/vision_apps/test_data ./vx_app_conformae.out --filter=tivxHwaVideoDecoder.MultiStreamProcessing APP: Init ... !!! APP_LOG: Mapping 0xac000000 ... APP_LOG: Mped 0xac000000 -> 0xffff848b0000 of size 262144 bytes MEM: Init ION ... !!! MEM: InitializeION (fd=4) !!! MEM: Init ION ... Done !!! PP_LOG: Mapping 0xac040000 ... APP_LOG: Mapped 0xac040000 -> 0xffff82910000 of size 33161216 bytes APP_LOG: Mappingx30e00000 ... APP_LOG: Mapped 0x30e00000 -> 0xffff84da0000 ofize 3072 bytes IPC: Init ... Done !!! REMOTE_SERVICE: Init ... !!! REMOTE_SERVICE: Init ... Done !!! APP: Init ..Done !!! 0.000638 s: VX_ZONE_INIT:Enabled 0.00064s: VX_ZONE_ERROR:Enabled 0.000652 s: VX_ZONE_WARNING:Enabled 0.001203 s: VX_ZONE_INIT:[tivxInit:64] Initlization Done !!! 0.001456 s: VX_ZONE_INIT:[tivxHostIni44] Initialization Done for HOST !!! VxTests version: 1.1-20170301 VCS version: unknown Build config: Release [ ====== ] Total 21932 tests from 144 test cases Use test filte tivxHwaVideoDecoder.MultiStreamProcessing Use global OpenVX context: FALSE [ -------- ] tests from tivxHwaVideecoder [ RUN 0001 ] tivxHwaVideoDecoder.MultiStreamProcessing.. [ DONE ] tivxHwaVideoDecoder.MultiStreamProcessing [ ------ ] 1 tests from test case tivxHwaVideoDecoder [ ======== ] [ ALL DONE 1 test(s) from 1 test case(s) ran [ PASSED ] 1 test(s) [ FLED ] 0 test(s) [ DISABLED ] 0 test(s) ================================= OpenVX Conformance report summary =============================== To be conformant to the OpenVX seline, 1 required test(s) must pass. 1 tests passed, 0 tests failed. PASSED. To be conformant to the User Data Objecextension, 0 required test(s) must pass. 0 tests passed, 0 tes failed. PASSED. Note: The 0 disabled tests are optional and are not considered for conformance. #REPORT: YYYYMMDDMMSS FILTERED 21932 0 1 1 1 0 (version 1.1-20170301) 13.6064 s: VX_ZONE_INIT:[tivxHostDeInit:49] De-Initialization Done for HOST !!! 13.656385 s: VX_ZONE_INIT:[tivxDeIni100] De-Initialization Done !!! APP: Deinit ... !!! REMOTE_SVICE: Deinit ... !!! REMOTE_SERVICE: Deinit ... Done !!! IPC: Deinit ... !!! IPC: DeInit ... Done !!! MEM: Deinit N ... !!! MEM: Alloc's: 11 alloc's of 8986376 bytes MEM: Fr's : 11 free's of 8986376 bytes MEM: Open's : 0 allocs of 0 bytes MEM: Deinit ION ... Done !!! APP: Deinit ... De !!! root@j7-evm:/opt/vision_apps# VX_TEST_DATA_PATH=/opt/vision_apps/test_data ./vx_app_conformae.out --filter=tivxHwaVideoDecoder.MultiStreamProcessing APP: Init ... !!! APP_LOG: Mapping 0xac000000 ... APP_LOG: Mped 0xac000000 -> 0xffff905a0000 of size 262144 bytes MEM: It ION ... !!! MEM: Initialized ION (fd=4) !!! MEM: Init ION ... Done !!! IPC: Init ... !!! APP_LOG: Mappi 0xac040000 ... APP_LOG: Mapped 0xac040000 -> 0xffff8e600000 size 33161216 bytes APP_LOG: Mapping 0x30e00000 ... APP_LOG: Mapped 0x30e00000 -> 0xffff90a90000 of size 3072 byte IPC: Init ... Done !!! REMOTE_SERVICE: Init ... !!! REMOTEERVICE: Init ... Done !!! APP: Init ... Done !!! 0.000330 s: VX_ZONE_INIT:Enabled 0.000345 s: VX_ZONE_EOR:Enabled 0.000349 s: VX_ZONE_WARNING:Enabled 0.0769 s: VX_ZONE_INIT:[tivxInit:64] Initialization Done !!! 0.000978 s: VX_ZONE_INIT:[tivxHostInit:44] Initializion Done for HOST !!! VxTests version: 1.1-20170301 VCS versn: unknown Build config: Release [ ======== ] Total 21932 tests from 144 test cases Use test filter: tivxHwaVideocoder.MultiStreamProcessing Use global OpenVX context: FALS [ -------- ] tests from tivxHwaVideoDecoder [ RUN 0001 ] tivxHwaVideoDecoder.MultiStreamProcessing ... [ DONE ] tivxHwaVideoDecoder.MultiStreamProcessing [ -------- ] 1 tests from test case tiHwaVideoDecoder [ ======== ] [ ALL DONE ] 1 test(s) from 1est case(s) ran [ PASSED ] 1 test(s) [ FAILED ] 0 test(s) [ DISABLED ] 0 test(s) =============================== OpenVX Conformance report summary =============================== To be conformant to the OpenVX baseline, 1 required test(s) must pass. 1 tests passed, 0 tests failed. PAED. To be conformant to the User Data Object extension, 0 reqred test(s) must pass. 0 tests passed, 0 tests failed. PASSED. Note: The 0 disabled tests are optional and are not coidered for conformance. #REPORT: YYYYMMDDHHMMSS FILTERED 212 0 1 1 1 0 (version 1.1-20170301) 45.180468 s: VX_ZONE_INIT:[tivxHostDeInit:49] De-Initialization Done for HOST ! 45.184812 s: VX_ZONE_INIT:[tivxDeInit:100] De-Initialition Done !!! APP: Deinit ... !!! REMOTE_SERVICE: Deinit ... !!! REMOTE_SERVICE: Deinit ... Done !!! IPC: Deinit . !!! IPC: DeInit ... Done !!! MEM: Deinit ION ... !!! MEM: loc's: 11 alloc's of 8986376 bytes MEM: Free's : 11 free's of 8986376 bytes MEM: Open's : 0 allocs of 0 bytes M: Deinit ION ... Done !!! APP: Deinit ... Done !!! root@j7-e:/opt/vision_apps# VX_TEST_DATA_PATH=/opt/vision_apps/test_data ./vx_app_conformance.out --filter=tivxHwaVidDecoder.MultiStreamProcessing APP: Init ... !!! APP_LOG: Mapping 0xac000000 ... APP_LOG: Mapped 0xac000000 -> 0xffff854e0000 of size 262144 bytes MEM:nit ION ... !!! MEM: Initialized ION (fd=4) !!! MEM: Init IO... Done !!! IPC: Init ... !!! APP_LOG: Mapping 0xac040000 ... APP_LOG: Mapped 0xac040000 -> 0xffff83540000 of size3161216 bytes APP_LOG: Mapping 0x30e00000 ... APP_LOG: Mapp 0x30e00000 -> 0xffff859d0000 of size 3072 bytes IPC: Init ... Done !!! REMOTE_SERVICE: Init ... !!! REMOTE_SERVIC Init ... Done !!! APP: Init ... Done !!! 0.000404 s: _ZONE_INIT:Enabled 0.000427 s: VX_ZONE_ERROR:Enabled 0.000432 s: VX_ZONE_WARNING:Enabled 0.001092 s VX_ZONE_INIT:[tivxInit:64] Initialization Done !!! 0.0053 s: VX_ZONE_INIT:[tivxHostInit:44] Initialization Done for HOST !!! VxTests version: 1.1-20170301 VCS version: unown Build config: Release [ ======== ] Total 21932 tests fm 144 test cases Use test filter: tivxHwaVideoDecoder.MultiStreamProcessing Use global OpenVX context: FALSE -------- ] tests from tivxHwaVideoDecoder [ RUN 0001 ] tivxHwideoDecoder.MultiStreamProcessing ... 0.138337 s: VX_ZONE_ERROR:[ownContextSendCmd:553] Command ack message returned failure cmd_status: -1 138357 s: VX_ZONE_ERROR:[ownNodeKernelInit:486] Target kernelTIVX_CMD_NODE_CREATE failed 0.138377 s: VX_ZONE_ERROR:[ownGraphNodeKernelInit:583] kernel init for node 1, kernecom.ti.hwa.video_decoder ... failed !!! 0.138383 s: VX_NE_ERROR:[vxVerifyGraph:2010] Node kernel init failed 0.138388 s: VX_ZONE_ERROR:[vxVerifyGraph:2064] Graph veri failed [MCU2_1] 254.766752 s: REMOTE_SERVICE: Unable to cate tx semaphore [MCU2_1] 254.766841 s: BSPP stream create failed 12 [MCU2_1] 254.767066 s: VX_ZONE_ERROR:[txVideoDecoderCreate:562] tivxVideoDecoderCreate: MM_DEC Createailed FAILED at /ti/j7/releases/06_02_00/06_02_00_21/psdk_rtos_auto_j7_06_02_00_21/tiovx/kernels_j7/hwa/test/test_deo_decoder.c:549 Expected: VX_SUCCESS == vxVerifyGraph(grap Actual: VX_SUCCESS != VX_FAILURE 0.175411 s: VX_ZONE_WARNING:[vxReleaseContext:743] Stale reference 0xb075 of type 00000816 at external count 1, internal count 1 175417 s: VX_ZONE_WARNING:[vxReleaseContext:746] Unreleased reference name = user_data_object_84 0.175423 s: VXONE_WARNING:[vxReleaseContext:743] Stale reference 0xb077e0 ofype 00000816 at external count 1, internal count 1 0.175428 s: VX_ZONE_WARNING:[vxReleaseContext:746] Unreleasereference name = user_data_object_85 0.175434 s: VX_ZONWARNING:[vxReleaseContext:743] Stale reference 0xb07a00 of type 00000816 at external count 1, internal count 1 0.5438 s: VX_ZONE_WARNING:[vxReleaseContext:746] Unreleased refence name = user_data_object_86 0.175444 s: VX_ZONE_WARNING:[vxReleaseContext:743] Stale reference 0xb07c20 of pe 00000816 at external count 1, internal count 1 0.1754 s: VX_ZONE_WARNING:[vxReleaseContext:746] Unreleased reference name = user_data_object_87 0.175453 s: VX_ZONE_RNING:[vxReleaseContext:743] Stale reference 0xb396c0 of type 00080f at external count 1, internal count 1 0.175458 s: VX_ZONE_WARNING:[vxReleaseContext:746] Unreleased refence name = image_88 0.175463 s: VX_ZONE_WARNING:[vxReleeContext:743] Stale reference 0xb39978 of type 0000080f at external count 1, internal count 1 0.175467 s: VX_ZO_WARNING:[vxReleaseContext:746] Unreleased reference name = ime_89 0.175473 s: VX_ZONE_WARNING:[vxReleaseContext:743] Stale reference 0xa9af20 of type 00000802 at external cot 1, internal count 0 0.175477 s: VX_ZONE_WARNING:[vxReaseContext:746] Unreleased reference name = graph_90 [ !FAILED! ] tivxHwaVideoDecoder.MultiStreamProcessing [ ------ ] 1 tests from test case tivxHwaVideoDecoder ALL DONE ] 1 test(s) from 1 test case(s) ran [ PASSED ] 0 test(s) [ FAILED ] 1 test(s), listed below: [ FAILED ] tivxHwaVideoDecoder.MultiStreamProcessing [ DISABLED ] 0 te(s) ================================= OpenVX Conformance report summary ================================= To bconformant to the OpenVX baseline, 1 required test(s) must pas 0 tests passed, 1 tests failed. FAILED. To be conformant to the User Data Object extension, 0 required test(s) must ps. 0 tests passed, 0 tests failed. PASSED. Note: The 0 disabl tests are optional and are not considered for conformance. #REPORT: YYYYMMDDHHMMSS FILTERED 21932 0 1 1 0 1 (versi 1.1-20170301) 0.186380 s: VX_ZONE_INIT:[tivxHostDeInit9] De-Initialization Done for HOST !!! 0.190703 s: VX_ZONE_INIT:[tivxDeInit:100] De-Initialization Done !!! APPDeinit ... !!! REMOTE_SERVICE: Deinit ... !!! REMOTE_SERVICEDeinit ... Done !!! IPC: Deinit ... !!! IPC: DeInit ... Done !!! MEM: Deinit ION ... !!! MEM: Alloc's: 12 alloc's 8986632 bytes MEM: Free's : 12 free's of 8986632 bytes M: Open's : 0 allocs of 0 bytes MEM: Deinit ION ... Done !!!
decoder-robustness.7zHi Zhong Ming,
David has fixed the issue and myself and David tested the test case 100 & 500 times respectively.
2 Things:
1) Patch: 0001-osal-tirtos-osa_queue-Fix-semaphore-cleanup
To fix the actual issue with destroying the acquired semaphores. This needs the following build commands:
video_codec: rm –rf out
video_codec: make codec_apps
vision_apps: make
to install the changes to SD card i am doing:
make linux_fs_install_sd
2) The above will get us running mltiple iterations of decoder. That means by default output gets continuously written to SD
Card and we observed that card gets full by 8-12 iteration depending on the memory size of the card.
So we suggest the following change in the file \psdk_rtos_auto_j7_06_02_00_21\tiovx\kernels_j7\hwa\test\test_video_decoder.c:
Comment out the below line:
#define DUMP_DECODED_VIDEO_TO_FILE.
The above ensures that output is not written to SD or else one will have manually clear the output of decoder every iteration
to avoid SD card memory getting full.
This needs the following build commands:
tiovx directory: make tiovx
vision_apps: make
to install the changes to SD card i am doing:
make linux_fs_install_sd
I am posting this on behalf of David.
Thanks,
Keerthy
Hi Keerthy,
The patch does not work in my environment. And once the patch is used, it causes other stuck problem when decode multi H.264 streams. And if we run multi times, it will end up with decoder's crash just as before.
Leon