Other Parts Discussed in Thread: SYSBIOS
Hi,
I am trying to enable PRP support for my AM335x Linux device (running ti-processor-sdk-linux-am335x-evm-05.01.00.11) using PRU-ICSS-HSR-PRP-DAN_01.00.04.02. After installing the SDK and the Code Composer Studio (CCS8.1.0.00011_linux), creating the project file, as mentioned in the start up guide gives me the following error:
./projectCreate.sh AM335x arm prp_app
**************************************************************************
Environment Configuration Summary:
 CCS Install Directory : /opt/ti-processor-sdk-linux-am335x-evm-05.01.00.11/ccsv8
 CCS Workspace Directory : /tmp/ccs_workspace
 SDK Install Directory : /PRU-ICSS-HSR-PRP-DAN_01.00.04.02
 PDK Install Directory : /opt/ti-processor-sdk-linux-am335x-evm-05.01.00.11/pdk_am335x_1_0_10/packages
 Projects create Directory : /PRU-ICSS-HSR-PRP-DAN_01.00.04.02/protocols/hsr_prp/projects
 Project create args directory : /PRU-ICSS-HSR-PRP-DAN_01.00.04.02/protocols/hsr_prp/projects/ccsproject_args
**************************************************************************
Creating project 'prp_app_AM335x_arm' for 'AM335x' platform in directory '/PRU-ICSS-HSR-PRP-DAN_01.00.04.02/protocols/hsr_prp/projects/prp_app_AM335x_arm' by overwriting the project if it exists already...
--------------------------------------------------------------------------------
Creating project 'prp_app_AM335x_arm'...
NOTE: Compiler version 'GNU_6.3.1:Linaro' is not currently installed! - defaulting to 'GNU_7.2.1:Linaro'.
 !ERROR: No products of type 'com.ti.rtsc.SYSBIOS' are currently installed!
Could you please help me in solving it?
PS: read some forum posts informing to use SDK_4.3 version of TI_RTOS. But we need the feature in Linux SDK 5,01. Can you please detail the steps to be followed to handle the same