Part Number: TDA4VM
Hi Experts:
I'm working on a custom board with TDA4VM,pcie0 is host,when kernel starting ,below messging
[ 2.070987] cdns-pcie-host d000000.pcie: missing "mem"
[ 2.076614] cdns-pcie-host d800000.pcie: missing "mem"
[ 2.082225] cdns-pcie-host e000000.pcie: missing "mem"
i look the k3-j271e-main.dtsi,it have
pcie0_rc: pcie@d000000 {
compatible = "ti,j721e-cdns-pcie-host";
reg = <0x00 0x0d000000 0x00 0x00800000>,
<0x00 0x10000000 0x00 0x00001000>;
reg-names = "reg", "cfg";
i look the /dirver/pci/controller/pcie-candence-host.c,it have this code, but the dts dont have "mem" reg.
res = platform_get_resource_byname(pdev, IORESOURCE_MEM, "mem");
if (!res)
dev_err(dev, "missing \"mem\"\n");
My question is:
1, Which version of SDK can start normally?
2,what does "reg", "cfg" "mem" mean?