This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2EVM5777: TI DeepLearning Assertion error

Part Number: TDA2EVM5777

Hello,

I am trying to get the Vision SDK  TI Deep Learning (TIDL) example running on the TDA2EVM5777 board. I was able to generate an AppImage and MLO with no issues. I copied the MLO and AppImage to the SD card as well as all of the files in the PROCESSOR_SDK_VISION_03_08_00_00\vision_sdk\apps\tools\TIDL_files directory. I booted the board up and was able to follow the instructions from the VisionSDK_UserGuide_TI_DeepLearning.pdf user guide.

The steps I took after I was prompted for Vision SDK usecase, was I selected "f" for TIDL usecase. Then I selected "1" for TIDL File I/O usecase. From there, I am prompted with which core I wanted to use. I selected "2" for EVE. For the Use case Mode, I wanted to dump the output to a file. Once I selected that case I got a few error messages:

[IPU1-0]     40.147379 s:  Assertion @ Line: 103 in /home/user01/PROCESSOR_SDK_VISION_03_08_00_00/vision_sdk/apps/src/rtos/usecases/common/chains_common_tidl.c: readSize == sizeof(sTIDL_Network_t) : failed !!!
[IPU1-0]     40.148295 s:  Assertion @ Line: 103 in /home/user01/PROCESSOR_SDK_VISION_03_08_00_00/vision_sdk/apps/src/rtos/usecases/common/chains_common_tidl.c: readSize == sizeof(sTIDL_Network_t) : failed !!!


What steps can I take to fix this issue?

What can cause this assertion to fail?

I double checked that my files didn't get corrupted when they reached the SD card, so I don't really know how to debug from here.
Thank you very much for your help,

-iFer

  • Hi,

    Can you share the complete logs in a text file? also print the value of "readSize" & "sizeof(sTIDL_Network_t)".

    Thanks

    Gaviraju

  • Hello Gaviraj,

    I can't find a way to print those values.   Can you assist me with the method/syntax to print those values please?  Also I have attached the full log including boot prints.
    Thank you,
    -iFer
     TDA2xx SBL Boot
    
     DPLL Configuration Completed
    
     Clock Domain Configuration Completed
    
     Module Enable Configuration Completed
    
     TI EVM PAD Config Completed
    
     DDR Config Completed
    
     App Image Download Begins
    
     SD Boot - file open completed successfully
    
     MPU CPU0 Image Load Completed
    
     IPU1 CPU0 Image Load Completed
    
     IPU1 CPU1 Image Load Completed
    
     IPU2 CPU0 and CPU1 Image Load Completed
    
     DSP1 Image Load Completed
    
     DSP2 Image Load Completed
    
     EVE1 Image Load Completed
    
     EVE2 Image Load Completed
    
     EVE3 Image Load Completed
    
     EVE4 Image Load Completed
    
     App Image Download Completed
    
     Putting MPU CPU1 in Off mode
    
     EVE MMU configuration completed
    
     EVE MMU configuration completed
    
     EVE MMU configuration completed
    
     EVE MMU configuration completed
    
    *****************************************************************
    
     PMCCNTR counts once every 64 clock cycles, multiple by 64 to get actual CPU cycles
    
     SBL Initial Config Cycles - 143982  (12.28 ms)
     SOC Init Cycles - 170928  (14.58 ms)
     DDR Config Clock Cycles - 43376  (3.70 ms)
     App Image Load Cycles - 44811173  (3823.88 ms)
     Slave Core Bootup Cycles - 208154  (17.76 ms)
     SBL Boot-up Cycles - 45378675  (3872.31 ms)
     Time at which SBL started IPU1_0 - 135962  (4149.23 ms)
    *****************************************************************
    
     Jumping to MPU CPU0 App
    [IPU1-0]      4.152687 s:  ***** IPU1_0 Firmware build time 13:08:49 Jun 29 2020
    [IPU1-0]      4.152900 s:  *** SYSTEM: CPU Frequency <ORG = 212800000 Hz>, <NEW = 212800000 Hz>
    [IPU1-0]      4.953364 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...
    [IPU1-0]      4.953547 s:  SYSTEM: Notify register to [IPU2] line 0, event 15...
    [IPU1-0]      4.953669 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...
    [IPU1-0]      4.953791 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...
    [IPU1-0]      4.953882 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...
    [IPU1-0]      4.954004 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...
    [IPU1-0]      4.954096 s:  SYSTEM: Notify register to [EVE3] line 0, event 15...
    [IPU1-0]      4.954218 s:  SYSTEM: Notify register to [EVE4] line 0, event 15...
    [IPU1-0]      4.954340 s:  SYSTEM: Notify register to [HOST] line 0, event 15...
    [IPU1-0]      4.956139 s:  *** UTILS: CPU MHz = 20 Mhz ***
    [IPU1-0]      4.956292 s:  SYSTEM: System Common Init in progress !!!
    [IPU1-0]      4.970597 s:  UTILS: CIO: Init Done !!!
    [IPU1-0]      4.970719 s:  SYSTEM: IPC init in progress !!!
    [IPU1-0]      4.970780 s:  SYSTEM: Notify init done !!!
    [IPU1-0]      4.972640 s:  SYSTEM: MsgQ init done !!!
    [IPU1-0]      4.972732 s:  SYSTEM: IPC init DONE !!!
    [IPU1-0]      4.976605 s:  SYSTEM: System Common Init Done !!!
    [IPU1-0]      4.976727 s:  SYSTEM: System Init in progress !!!
    [IPU1-0]      4.976788 s:  SYSTEM: BSP Common Init in progress !!!
    [IPU1-0]      4.976880 s:  SYSTEM: BSP Common Init Done !!!
    [IPU1-0]      4.976941 s:  SYSTEM: BSP Platform Init in progress !!!
    [IPU1-0]      4.977093 s:  SYSTEM: BSP Platform Init Done !!!
    [IPU1-0]      4.977154 s:  SYSTEM: FVID2 Init in progress !!!
    [IPU1-0]      4.977307 s:  SYSTEM: FVID2 Init Done !!!
    [IPU1-0]      4.977490 s:  SYSTEM: VPS Init in progress !!!
    [IPU1-0]      4.977612 s:  SYSTEM: VPDMA Descriptor Memory Address translation ENABLED [0xa0000000 -> 0x80000000]
    [IPU1-0]      4.981577 s: *** VPDMA Firmware Loading... ***
    [IPU1-0]      4.981730 s: VPDMA Firmware Address = 0x9fc9c4c0
    [IPU1-0]      4.981821 s: VPDMA Load Address     = 0x4897d004
    [IPU1-0]      4.981943 s: VPDMA Firmware Version = 0x4d0001b8
    [IPU1-0]      4.982065 s: VPDMA List Busy Status = 0x00000000
    [IPU1-0]      4.982187 s: *** VPDMA Firmware Load Success ***
    [IPU1-0]      4.982828 s: *** VPDMA Firmware Loading... ***
    [IPU1-0]      4.982919 s: VPDMA Firmware Address = 0x9fc9c4c0
    [IPU1-0]      4.983011 s: VPDMA Load Address     = 0x4899d004
    [IPU1-0]      4.983133 s: VPDMA Firmware Version = 0x4d0001b8
    [IPU1-0]      4.983194 s: VPDMA List Busy Status = 0x00000000
    [IPU1-0]      4.983285 s: *** VPDMA Firmware Load Success ***
    [IPU1-0]      4.983743 s: *** VPDMA Firmware Loading... ***
    [IPU1-0]      4.983895 s: VPDMA Firmware Address = 0x9fc9c4c0
    [IPU1-0]      4.984017 s: VPDMA Load Address     = 0x489bd004
    [IPU1-0]      4.984109 s: VPDMA Firmware Version = 0x4d0001b8
    [IPU1-0]      4.984200 s: VPDMA List Busy Status = 0x00000000
    [IPU1-0]      4.984292 s: *** VPDMA Firmware Load Success ***
    [IPU1-0]      4.984871 s: *** VPDMA Firmware Loading... ***
    [IPU1-0]      4.984993 s: VPDMA Firmware Address = 0x9fc9c4c0
    [IPU1-0]      4.985054 s: VPDMA Load Address     = 0x489dd004
    [IPU1-0]      4.985176 s: VPDMA Firmware Version = 0x4d0001b8
    [IPU1-0]      4.985268 s: VPDMA List Busy Status = 0x00000000
    [IPU1-0]      4.985329 s: *** VPDMA Firmware Load Success ***
    [IPU1-0]      5.049838 s:  SYSTEM: VPS Init Done !!!
    [IPU1-0]      5.050814 s:  UTILS: DMA: HWI Create for INT34 !!!
    [IPU1-0]      5.050997 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024
    [IPU1-0]      5.051149 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 262144 B (256 KB), Free size = 252328 B (246 KB)
    [IPU1-0]      5.051302 s:  SYSTEM: Heap = SR_OCMC              @ 0x00000000, Total size = 0 B (0 KB), Free size = 0 B (0 KB)
    [IPU1-0]      5.051515 s:  SYSTEM: Heap = SR_DDR_CACHED        @ 0x8a783000, Total size = 355979264 B (339 MB), Free size = 355979264 B (339 MB)
    [IPU1-0]      5.051759 s:  SYSTEM: Heap = SR_DDR_NON_CACHED    @ 0xbfb00000, Total size = 127360 B (0 MB), Free size = 92800 B (0 MB)
    [IPU1-0]      5.051942 s:  SYSTEM: Initializing Links !!!
    [IPU1-0]      5.319160 s:  SYSTEM: Initializing Links ... DONE !!!
    [IPU1-0]      5.414414 s:  BOARD: Board Init in progress !!!
    [IPU1-0]      5.414811 s:  BOARD: Board Init Done !!!
    [IPU1-0]      5.426035 s:
    [IPU1-0]      5.426096 s:  Vision SDK Version    : [REL_VISION_SDK_03_08_00_00]
    [IPU1-0]      5.426157 s:  FVID2 Version         : [FVID_02_01_00_01]
    [IPU1-0]      5.426249 s:  BSP Version           : [PDK_01_10_04__xx]
    [IPU1-0]      5.426310 s:  Platform              : [EVM]
    [IPU1-0]      5.426371 s:  SOC                   : [TDA2XX]
    [IPU1-0]      5.426462 s:  SOC Revision          : [ES1.1]
    [IPU1-0]      5.426523 s:  Board Detected        : [Vision]
    [IPU1-0]      5.432654 s:  EEPROM Base Board Name: [5777xCPU]
    [IPU1-0]      5.432745 s:  Base Board Revision   : [REV E]
    [IPU1-0]      5.434057 s:  Daughter Card Revision: [REV D]
    [IPU1-0]      5.434118 s:
    [IPU1-0]      5.437900 s:  SYSTEM: UART: INTERRUPT Mode is Selected
    [IPU1-1]      4.168883 s:  ***** IPU1_1 Firmware build time 13:07:29 Jun 29 2020
    [IPU1-1]      4.169066 s:  *** SYSTEM: CPU Frequency <ORG = 212800000 Hz>, <NEW = 212800000 Hz>
    [IPU1-1]      4.955865 s:  SYSTEM: Notify register to [IPU1-0] line 0, event 15...
    [IPU1-1]      4.956078 s:  SYSTEM: Notify register to [IPU2] line 0, event 15...
    [IPU1-1]      4.956231 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...
    [IPU1-1]      4.956383 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...
    [IPU1-1]      4.956505 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...
    [IPU1-1]      4.956627 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...
    [IPU1-1]      4.956719 s:  SYSTEM: Notify register to [EVE3] line 0, event 15...
    [IPU1-1]      4.956841 s:  SYSTEM: Notify register to [EVE4] line 0, event 15...
    [IPU1-1]      4.956963 s:  SYSTEM: Notify register to [HOST] line 0, event 15...
    [IPU1-1]      4.959067 s:  SYSTEM: System Common Init in progress !!!
    [IPU1-1]      4.960409 s:  UTILS: CIO: Init Done !!!
    [IPU1-1]      4.960562 s:  SYSTEM: IPC init in progress !!!
    [IPU1-1]      4.960653 s:  SYSTEM: Notify init done !!!
    [IPU1-1]      4.962636 s:  SYSTEM: MsgQ init done !!!
    [IPU1-1]      4.962758 s:  SYSTEM: IPC init DONE !!!
    [IPU1-1]      4.966510 s:  SYSTEM: System Common Init Done !!!
    [IPU1-1]      4.966632 s:  SYSTEM: System IPU1_1 Init in progress !!!
    [IPU1-1]      4.967577 s:  UTILS: DMA: HWI Create for INT25 !!!
    [IPU1-1]      4.967791 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024
    [IPU1-1]      4.967913 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 655360 B (640 KB), Free size = 645688 B (630 KB)
    [IPU1-1]      4.968065 s:  SYSTEM: Initializing Links !!!
    [IPU1-1]      5.083755 s:  UTILS: PRF: ##### Cannot allocate Object for SYNC1 ####
    [IPU1-1]      5.087018 s:  UTILS: PRF: ##### Cannot allocate Object for SYNC2 ####
    [IPU1-1]      5.090099 s:  UTILS: PRF: ##### Cannot allocate Object for SYNC3 ####
    [IPU1-1]      5.093485 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM0 ####
    [IPU1-1]      5.096992 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM1 ####
    [IPU1-1]      5.100378 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM2 ####
    [IPU1-1]      5.103763 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM3 ####
    [IPU1-1]      5.107454 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM4 ####
    [IPU1-1]      5.110687 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM5 ####
    [IPU1-1]      5.114439 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM6 ####
    [IPU1-1]      5.117611 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM7 ####
    [IPU1-1]      5.117733 s:  SYSTEM: Initializing Links ... DONE !!!
    [IPU1-1]      5.117824 s:  SYSTEM: System IPU1_1 Init Done !!!
    [HOST  ]      4.238790 s:  ***** A15_0 Firmware build time 13:07:06 Jun 29 2020
    [HOST  ]      4.238821 s:  *** SYSTEM: CPU Frequency <ORG = 750000000 Hz>, <NEW = 750000000 Hz>
    [HOST  ]      4.954401 s:  SYSTEM: Notify register to [IPU1-0] line 0, event 15...
    [HOST  ]      4.954431 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...
    [HOST  ]      4.954431 s:  SYSTEM: Notify register to [IPU2] line 0, event 15...
    [HOST  ]      4.954462 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...
    [HOST  ]      4.954462 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...
    [HOST  ]      4.954492 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...
    [HOST  ]      4.954492 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...
    [HOST  ]      4.954492 s:  SYSTEM: Notify register to [EVE3] line 0, event 15...
    [HOST  ]      4.954523 s:  SYSTEM: Notify register to [EVE4] line 0, event 15...
    [HOST  ]      4.957176 s:  SYSTEM: System Common Init in progress !!!
    [HOST  ]      4.957237 s:  SYSTEM: IPC init in progress !!!
    [HOST  ]      4.957237 s:  SYSTEM: Notify init done !!!
    [HOST  ]      4.957268 s:  SYSTEM: MsgQ init done !!!
    [HOST  ]      4.957298 s:  SYSTEM: IPC init DONE !!!
    [HOST  ]      4.957847 s:  SYSTEM: System Common Init Done !!!
    [HOST  ]      4.957878 s:  SYSTEM: System A15 Init in progress !!!
    [HOST  ]      4.957908 s:  UTILS: DMA: HWI Create for INT66 !!!
    [HOST  ]      4.957939 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024
    [HOST  ]      4.957939 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 6291456 B (6144 KB), Free size = 6246704 B (6100 KB)
    [HOST  ]      4.957969 s:  SYSTEM: Initializing Links !!!
    [HOST  ]      4.960531 s:  UTILS: PRF: ##### Cannot allocate Object for SYNC1 ####
    [HOST  ]      4.960623 s:  UTILS: PRF: ##### Cannot allocate Object for SYNC2 ####
    [HOST  ]      4.960684 s:  UTILS: PRF: ##### Cannot allocate Object for SYNC3 ####
    [HOST  ]      4.960775 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM0 ####
    [HOST  ]      4.960836 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM1 ####
    [HOST  ]      4.960928 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM2 ####
    [HOST  ]      4.961019 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM3 ####
    [HOST  ]      4.961080 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM4 ####
    [HOST  ]      4.961172 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM5 ####
    [HOST  ]      4.961233 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM6 ####
    [HOST  ]      4.961324 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM7 ####
    [HOST  ]      4.961324 s:  SYSTEM: Initializing Links ... DONE !!!
    [HOST  ]      4.961385 s:  SYSTEM: System A15 Init Done !!!
    [HOST  ]      5.254864 s:  NSP GMAC: PHY 2 Found on MAC Port 0
    [HOST  ]      5.255352 s:  NSP GMAC: PHY 3 Found on MAC Port 1
    [DSP1  ]      4.232873 s:  ***** DSP1 Firmware build time 13:07:55 Jun 29 2020
    [DSP1  ]      4.232965 s:  *** SYSTEM: CPU Frequency <ORG = 600000000 Hz>, <NEW = 600000000 Hz>
    [DSP1  ]      4.958305 s:  SYSTEM: Notify register to [IPU1-0] line 0, event 15...
    [DSP1  ]      4.958366 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...
    [DSP1  ]      4.958396 s:  SYSTEM: Notify register to [IPU2] line 0, event 15...
    [DSP1  ]      4.958457 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...
    [DSP1  ]      4.958488 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...
    [DSP1  ]      4.958518 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...
    [DSP1  ]      4.958549 s:  SYSTEM: Notify register to [EVE3] line 0, event 15...
    [DSP1  ]      4.958610 s:  SYSTEM: Notify register to [EVE4] line 0, event 15...
    [DSP1  ]      4.958640 s:  SYSTEM: Notify register to [HOST] line 0, event 15...
    [DSP1  ]      4.958823 s:  *** UTILS: CPU MHz = 20 Mhz ***
    [DSP1  ]      4.958884 s:  SYSTEM: System Common Init in progress !!!
    [DSP1  ]      4.959128 s:  UTILS: CIO: Init Done !!!
    [DSP1  ]      4.959159 s:  SYSTEM: IPC init in progress !!!
    [DSP1  ]      4.959189 s:  SYSTEM: Notify init done !!!
    [DSP1  ]      4.959342 s:  SYSTEM: MsgQ init done !!!
    [DSP1  ]      4.959403 s:  SYSTEM: IPC init DONE !!!
    [DSP1  ]      4.960135 s:  SYSTEM: System Common Init Done !!!
    [DSP1  ]      4.960165 s:  SYSTEM: System DSP Init in progress !!!
    [DSP1  ]      4.960409 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024
    [DSP1  ]      4.960470 s:  SYSTEM: Heap = LOCAL_L2             @ 0x00800000, Total size = 227264 B (221 KB), Free size = 227264 B (221 KB)
    [DSP1  ]      4.960531 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 524288 B (512 KB), Free size = 514784 B (502 KB)
    [DSP1  ]      4.960562 s:  SYSTEM: Initializing Links !!!
    [DSP1  ]      4.969285 s:  SYSTEM: Initializing Links ... DONE !!!
    [DSP1  ]      4.969346 s: lz4CompDecomp Init
    [DSP1  ]      4.969377 s:  SYSTEM: System DSP Init Done !!!
    [DSP1  ]      5.333312 s:  SYSTEM: CACHE: L1P = 32 KB, L1D = 32 KB, L2 = 32 KB ... after boot !!!
    [DSP1  ]      5.333374 s:  SYSTEM: CACHE: L1P = 32 KB, L1D = 32 KB, L2 = 32 KB ... after update by APP !!!
    [DSP2  ]      4.232812 s: ***** DSP2 Firmware build time 13:07:55 Jun 29 2020
    [DSP2  ]      4.232873 s:  *** SYSTEM: CPU Frequency <ORG = 600000000 Hz>, <NEW = 600000000 Hz>
    [DSP2  ]      4.959769 s:  SYSTEM: Notify register to [IPU1-0] line 0, event 15...
    [DSP2  ]      4.959830 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...
    [DSP2  ]      4.959891 s:  SYSTEM: Notify register to [IPU2] line 0, event 15...
    [DSP2  ]      4.959921 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...
    [DSP2  ]      4.959952 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...
    [DSP2  ]      4.959982 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...
    [DSP2  ]      4.960043 s:  SYSTEM: Notify register to [EVE3] line 0, event 15...
    [DSP2  ]      4.960074 s:  SYSTEM: Notify register to [EVE4] line 0, event 15...
    [DSP2  ]      4.960104 s:  SYSTEM: Notify register to [HOST] line 0, event 15...
    [DSP2  ]      4.960318 s:  *** UTILS: CPU MHz = 20 Mhz ***
    [DSP2  ]      4.960379 s:  SYSTEM: System Common Init in progress !!!
    [DSP2  ]      4.960592 s:  UTILS: CIO: Init Done !!!
    [DSP2  ]      4.960623 s:  SYSTEM: IPC init in progress !!!
    [DSP2  ]      4.960653 s:  SYSTEM: Notify init done !!!
    [DSP2  ]      4.960836 s:  SYSTEM: MsgQ init done !!!
    [DSP2  ]      4.960867 s:  SYSTEM: IPC init DONE !!!
    [DSP2  ]      4.961568 s:  SYSTEM: System Common Init Done !!!
    [DSP2  ]      4.961629 s:  SYSTEM: System DSP Init in progress !!!
    [DSP2  ]      4.961843 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024
    [DSP2  ]      4.961873 s:  SYSTEM: Heap = LOCAL_L2             @ 0x00800000, Total size = 227264 B (221 KB), Free size = 227264 B (221 KB)
    [DSP2  ]      4.961934 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 524288 B (512 KB), Free size = 514784 B (502 KB)
    [DSP2  ]      4.961965 s:  SYSTEM: Initializing Links !!!
    [DSP2  ]      4.970444 s:  SYSTEM: Initializing Links ... DONE !!!
    [DSP2  ]      4.970505 s: lz4CompDecomp Init
    [DSP2  ]      4.970536 s:  SYSTEM: System DSP Init Done !!!
    [DSP2  ]      5.335326 s:  SYSTEM: CACHE: L1P = 32 KB, L1D = 32 KB, L2 = 32 KB ... after boot !!!
    [DSP2  ]      5.335356 s:  SYSTEM: CACHE: L1P = 32 KB, L1D = 32 KB, L2 = 32 KB ... after update by APP !!!
    [EVE1  ]      4.942566 s:  ***** EVE Firmware build time 13:07:18 Jun 29 2020
    [EVE1  ]      4.944366 s:  *** SYSTEM: CPU Frequency <ORG = 267500000 Hz>, <NEW = 267500000 Hz>
    [EVE1  ]      4.964314 s:  SYSTEM: Notify register to [IPU1-0] line 0, event 15...
    [EVE1  ]      4.965930 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...
    [EVE1  ]      4.967455 s:  SYSTEM: Notify register to [IPU2] line 0, event 15...
    [EVE1  ]      4.968950 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...
    [EVE1  ]      4.970444 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...
    [EVE1  ]      4.971847 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...
    [EVE1  ]      4.973220 s:  SYSTEM: Notify register to [EVE3] line 0, event 15...
    [EVE1  ]      4.974592 s:  SYSTEM: Notify register to [EVE4] line 0, event 15...
    [EVE1  ]      4.975934 s:  SYSTEM: Notify register to [HOST] line 0, event 15...
    [EVE1  ]      4.978130 s:  SYSTEM: System Common Init in progress !!!
    [EVE1  ]      4.980509 s:  UTILS: CIO: Init Done !!!
    [EVE1  ]      4.981455 s:  SYSTEM: IPC init in progress !!!
    [EVE1  ]      4.982797 s:  SYSTEM: Notify init done !!!
    [EVE1  ]      4.984780 s:  SYSTEM: MsgQ init done !!!
    [EVE1  ]      4.985725 s:  SYSTEM: IPC init DONE !!!
    [EVE1  ]      5.001494 s:  SYSTEM: System Common Init Done !!!
    [EVE1  ]      5.002470 s:  SYSTEM: System EVE Init in progress !!!
    [EVE1  ]      5.004026 s:  UTILS: DMA: HWI Create for INT8 !!!
    [EVE1  ]      5.005276 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024
    [EVE1  ]      5.006588 s:  SYSTEM: Heap = LOCAL_L2             @ 0x40020000, Total size = 22528 B (22 KB), Free size = 22528 B (22 KB)
    [EVE1  ]      5.009028 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 262144 B (256 KB), Free size = 252592 B (246 KB)
    [EVE1  ]      5.011285 s:  SYSTEM: Initializing Links !!!
    [EVE1  ]      5.107972 s:  SYSTEM: Initializing Links ... DONE !!!
    [EVE1  ]      5.109009 s:  SYSTEM: System EVE Init Done !!!
    [EVE2  ]      4.920667 s:  ***** EVE Firmware build time 13:07:20 Jun 29 2020
    [EVE2  ]      4.922558 s:  *** SYSTEM: CPU Frequency <ORG = 267500000 Hz>, <NEW = 267500000 Hz>
    [EVE2  ]      4.966571 s:  SYSTEM: Notify register to [IPU1-0] line 0, event 15...
    [EVE2  ]      4.968126 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...
    [EVE2  ]      4.969682 s:  SYSTEM: Notify register to [IPU2] line 0, event 15...
    [EVE2  ]      4.971085 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...
    [EVE2  ]      4.972488 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...
    [EVE2  ]      4.973830 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...
    [EVE2  ]      4.975202 s:  SYSTEM: Notify register to [EVE3] line 0, event 15...
    [EVE2  ]      4.976575 s:  SYSTEM: Notify register to [EVE4] line 0, event 15...
    [EVE2  ]      4.978130 s:  SYSTEM: Notify register to [HOST] line 0, event 15...
    [EVE2  ]      4.980357 s:  SYSTEM: System Common Init in progress !!!
    [EVE2  ]      4.983072 s:  UTILS: CIO: Init Done !!!
    [EVE2  ]      4.984139 s:  SYSTEM: IPC init in progress !!!
    [EVE2  ]      4.985237 s:  SYSTEM: Notify init done !!!
    [EVE2  ]      4.987159 s:  SYSTEM: MsgQ init done !!!
    [EVE2  ]      4.988074 s:  SYSTEM: IPC init DONE !!!
    [EVE2  ]      5.003721 s:  SYSTEM: System Common Init Done !!!
    [EVE2  ]      5.004758 s:  SYSTEM: System EVE Init in progress !!!
    [EVE2  ]      5.006252 s:  UTILS: DMA: HWI Create for INT8 !!!
    [EVE2  ]      5.007411 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024
    [EVE2  ]      5.008784 s:  SYSTEM: Heap = LOCAL_L2             @ 0x40020000, Total size = 22528 B (22 KB), Free size = 22528 B (22 KB)
    [EVE2  ]      5.011163 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 262144 B (256 KB), Free size = 252592 B (246 KB)
    [EVE2  ]      5.013572 s:  SYSTEM: Initializing Links !!!
    [EVE2  ]      5.110168 s:  SYSTEM: Initializing Links ... DONE !!!
    [EVE2  ]      5.111175 s:  SYSTEM: System EVE Init Done !!!
    [EVE3  ]      4.942566 s:  ***** EVE Firmware build time 13:07:19 Jun 29 2020
    [EVE3  ]      4.944366 s:  *** SYSTEM: CPU Frequency <ORG = 267500000 Hz>, <NEW = 267500000 Hz>
    [EVE3  ]      4.968797 s:  SYSTEM: Notify register to [IPU1-0] line 0, event 15...
    [EVE3  ]      4.970292 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...
    [EVE3  ]      4.971695 s:  SYSTEM: Notify register to [IPU2] line 0, event 15...
    [EVE3  ]      4.973098 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...
    [EVE3  ]      4.974440 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...
    [EVE3  ]      4.975812 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...
    [EVE3  ]      4.977185 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...
    [EVE3  ]      4.978740 s:  SYSTEM: Notify register to [EVE4] line 0, event 15...
    [EVE3  ]      4.980296 s:  SYSTEM: Notify register to [HOST] line 0, event 15...
    [EVE3  ]      4.982675 s:  SYSTEM: System Common Init in progress !!!
    [EVE3  ]      4.985207 s:  UTILS: CIO: Init Done !!!
    [EVE3  ]      4.986152 s:  SYSTEM: IPC init in progress !!!
    [EVE3  ]      4.987250 s:  SYSTEM: Notify init done !!!
    [EVE3  ]      4.989385 s:  SYSTEM: MsgQ init done !!!
    [EVE3  ]      4.990331 s:  SYSTEM: IPC init DONE !!!
    [EVE3  ]      5.005673 s:  SYSTEM: System Common Init Done !!!
    [EVE3  ]      5.006679 s:  SYSTEM: System EVE Init in progress !!!
    [EVE3  ]      5.008204 s:  UTILS: DMA: HWI Create for INT8 !!!
    [EVE3  ]      5.009394 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024
    [EVE3  ]      5.010675 s:  SYSTEM: Heap = LOCAL_L2             @ 0x40020000, Total size = 22528 B (22 KB), Free size = 22528 B (22 KB)
    [EVE3  ]      5.013176 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 262144 B (256 KB), Free size = 252592 B (246 KB)
    [EVE3  ]      5.015799 s:  SYSTEM: Initializing Links !!!
    [EVE3  ]      5.111846 s:  SYSTEM: Initializing Links ... DONE !!!
    [EVE3  ]      5.112944 s:  SYSTEM: System EVE Init Done !!!
    [EVE4  ]      4.930763 s:  ***** EVE Firmware build time 13:07:19 Jun 29 2020
    [EVE4  ]      4.932654 s:  *** SYSTEM: CPU Frequency <ORG = 267500000 Hz>, <NEW = 267500000 Hz>
    [EVE4  ]      4.968797 s:  SYSTEM: Notify register to [IPU1-0] line 0, event 15...
    [EVE4  ]      4.970292 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...
    [EVE4  ]      4.971725 s:  SYSTEM: Notify register to [IPU2] line 0, event 15...
    [EVE4  ]      4.973098 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...
    [EVE4  ]      4.974440 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...
    [EVE4  ]      4.975812 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...
    [EVE4  ]      4.977185 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...
    [EVE4  ]      4.978679 s:  SYSTEM: Notify register to [EVE3] line 0, event 15...
    [EVE4  ]      4.980326 s:  SYSTEM: Notify register to [HOST] line 0, event 15...
    [EVE4  ]      4.982736 s:  SYSTEM: System Common Init in progress !!!
    [EVE4  ]      4.985268 s:  UTILS: CIO: Init Done !!!
    [EVE4  ]      4.986213 s:  SYSTEM: IPC init in progress !!!
    [EVE4  ]      4.987372 s:  SYSTEM: Notify init done !!!
    [EVE4  ]      4.989477 s:  SYSTEM: MsgQ init done !!!
    [EVE4  ]      4.990392 s:  SYSTEM: IPC init DONE !!!
    [EVE4  ]      5.005734 s:  SYSTEM: System Common Init Done !!!
    [EVE4  ]      5.006740 s:  SYSTEM: System EVE Init in progress !!!
    [EVE4  ]      5.008265 s:  UTILS: DMA: HWI Create for INT8 !!!
    [EVE4  ]      5.009455 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024
    [EVE4  ]      5.010705 s:  SYSTEM: Heap = LOCAL_L2             @ 0x40020000, Total size = 22528 B (22 KB), Free size = 22528 B (22 KB)
    [EVE4  ]      5.013206 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 262144 B (256 KB), Free size = 252592 B (246 KB)
    [EVE4  ]      5.015768 s:  SYSTEM: Initializing Links !!!
    [EVE4  ]      5.111999 s:  SYSTEM: Initializing Links ... DONE !!!
    [EVE4  ]      5.113097 s:  SYSTEM: System EVE Init Done !!!
    [IPU2  ]      4.150491 s:  ***** IPU2 Firmware build time 13:08:49 Jun 29 2020
    [IPU2  ]      4.150674 s:  *** SYSTEM: CPU Frequency <ORG = 212800000 Hz>, <NEW = 212800000 Hz>
    [IPU2  ]      4.957115 s:  SYSTEM: Notify register to [IPU1-0] line 0, event 15...
    [IPU2  ]      4.957298 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...
    [IPU2  ]      4.957420 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...
    [IPU2  ]      4.957542 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...
    [IPU2  ]      4.957634 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...
    [IPU2  ]      4.957756 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...
    [IPU2  ]      4.957847 s:  SYSTEM: Notify register to [EVE3] line 0, event 15...
    [IPU2  ]      4.957969 s:  SYSTEM: Notify register to [EVE4] line 0, event 15...
    [IPU2  ]      4.958091 s:  SYSTEM: Notify register to [HOST] line 0, event 15...
    [IPU2  ]      4.961141 s:  SYSTEM: System Common Init in progress !!!
    [IPU2  ]      4.962575 s:  UTILS: CIO: Init Done !!!
    [IPU2  ]      4.962697 s:  SYSTEM: IPC init in progress !!!
    [IPU2  ]      4.962788 s:  SYSTEM: Notify init done !!!
    [IPU2  ]      4.964741 s:  SYSTEM: MsgQ init done !!!
    [IPU2  ]      4.964863 s:  SYSTEM: IPC init DONE !!!
    [IPU2  ]      4.970109 s:  SYSTEM: System Common Init Done !!!
    [IPU2  ]      4.970231 s:  SYSTEM: System IPU2 Init in progress !!!
    [IPU2  ]      4.971085 s:  UTILS: DMA: HWI Create for INT25 !!!
    [IPU2  ]      4.971329 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024
    [IPU2  ]      4.971512 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 262144 B (256 KB), Free size = 252424 B (246 KB)
    [IPU2  ]      4.971695 s:  SYSTEM: Initializing Links !!!
    [IPU2  ]      5.081894 s:  UTILS: PRF: ##### Cannot allocate Object for SYNC1 ####
    [IPU2  ]      5.084883 s:  UTILS: PRF: ##### Cannot allocate Object for SYNC2 ####
    [IPU2  ]      5.087750 s:  UTILS: PRF: ##### Cannot allocate Object for SYNC3 ####
    [IPU2  ]      5.090739 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM0 ####
    [IPU2  ]      5.093912 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM1 ####
    [IPU2  ]      5.096962 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM2 ####
    [IPU2  ]      5.100012 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM3 ####
    [IPU2  ]      5.103214 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM4 ####
    [IPU2  ]      5.106295 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM5 ####
    [IPU2  ]      5.109467 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM6 ####
    [IPU2  ]      5.112609 s:  UTILS: PRF: ##### Cannot allocate Object for ALGORITHM7 ####
    [IPU2  ]      5.112761 s:  SYSTEM: Initializing Links ... DONE !!!
    [IPU2  ]      5.112822 s:  SYSTEM: System IPU2 Init Done !!!
    [IPU1-0]      6.472152 s:  UTILS_PRCM_STATS: INA226 Setup Failed. Check if INA226 is connected on I2C3 Lines
    [IPU1-0]      6.476483 s:  QSPI Init Started
    [IPU1-0]      6.476788 s:  MID - 1
    [IPU1-0]      6.476819 s:  DID - 18
    [IPU1-0]      6.476880 s:  QSPI Init Completed Sucessfully
    [IPU1-0]      6.489355 s:
    [IPU1-0]      6.489446 s:  Current System Settings,
    [IPU1-0]      6.489507 s:  ========================
    [IPU1-0]      6.489568 s:  Display Type   : HDMI 1920x1080 @ 60fps
    [IPU1-0]      6.489629 s:  Capture Source : Sensor OV10635 1280x720  @ 30fps - VIP, YUV422
    [IPU1-0]      6.489721 s:  My IP address for interface 1 : 0.0.0.0
    [IPU1-0]      6.489782 s:  My IP address for interface 2 : 0.0.0.0
    [IPU1-0]      6.489843 s:  ISS Settings   : LDC=[OFF] VTNF=[OFF] WDR=[OFF]
    [IPU1-0]      6.489904 s:
    [IPU1-0]      6.489965 s:  ============
    [IPU1-0]      6.489995 s:  Usecase Menu
    [IPU1-0]      6.490026 s:  ============
    [IPU1-0]      6.490087 s:
    [IPU1-0]
    [IPU1-0]  Vision SDK Usecases,
    [IPU1-0]  --------------------
    [IPU1-0]  1: Single Camera Usecases
    [IPU1-0]  2: Multi-Camera LVDS Usecases
    [IPU1-0]  3: AVB RX Usecases, (TDA2x & TDA2Ex ONLY)
    [IPU1-0]  4: Dual Display Usecases, (TDA2x EVM ONLY)
    [IPU1-0]  5: ISS Usecases, (TDA3x ONLY)
    [IPU1-0]  6: TDA2x Stereo Usecases
    [IPU1-0]  7: Network RX/TX Usecases
    [IPU1-0]  9: RADAR Usecases
    [IPU1-0]  a: Miscellaneous test's
    [IPU1-0]  f: TIDL Usecase
    [IPU1-0]  g: Camera Radar Combo Usecases
    [IPU1-0]
    [IPU1-0]  s: System Settings
    [IPU1-0]
    [IPU1-0]  x: Exit
    [IPU1-0]
    [IPU1-0]  Enter Choice:
    [IPU1-0]
    [HOST  ]      9.960714 s:  NETWORK_CTRL: Starting Server (port=5000) !!!
    [HOST  ]      9.960745 s:  NETWORK_CTRL: Starting Server ... DONE (port=5000) !!!
    [IPU1-0]     13.312511 s:
    [IPU1-0]     13.312663 s:
    [IPU1-0]
    [IPU1-0]  TIDL Usecases
    [IPU1-0]  ---------------
    [IPU1-0]  1: TIDL File I/O Usecase
    [IPU1-0]  2: Semantic Segmentation Usecase
    [IPU1-0]  3: TIDL OD Usecase
    [IPU1-0]
    [IPU1-0]  x: Exit
    [IPU1-0]
    [IPU1-0]  Enter Choice:
    [IPU1-0]
    [IPU1-0]     16.023089 s:
    [IPU1-0]     16.076435 s:  TIDL Configuration parameters
    [IPU1-0]     16.076496 s:  -----------------------------
    [IPU1-0]     16.076557 s:  inputWidth         = 1024
    [IPU1-0]     16.076618 s:  inputHeight        = 512
    [IPU1-0]     16.076709 s:  inputFile          = IN.RGB
    [IPU1-0]     16.076770 s:  outputFile         = OUT.BIN
    [IPU1-0]     16.076831 s:  netFileName        = NET.BIN
    [IPU1-0]     16.076892 s:  paramFileName      = PRM.BIN
    [IPU1-0]     16.076953 s:  -----------------------------
    [IPU1-0]     16.077014 s:
    [IPU1-0]
    [IPU1-0]  ====================
    [IPU1-0]  Core Menu
    [IPU1-0]  ====================
    [IPU1-0]
    [IPU1-0]  1: DSP
    [IPU1-0]  2: EVE
    [IPU1-0]
    [IPU1-0]  Enter Choice:
    [IPU1-0]
    [IPU1-0]     17.447172 s:
    [IPU1-0]
    [IPU1-0]  ====================
    [IPU1-0]  Use case Mode
    [IPU1-0]  ====================
    [IPU1-0]
    [IPU1-0]  1: Dump Output Frames to file
    [IPU1-0]  2: Free Run (Output Frames are not dumped)
    [IPU1-0]
    [IPU1-0]  Enter Choice:
    [IPU1-0]
    [IPU1-0]     19.209723 s:  UTILS: DMA: Allocated CH (TCC) = 48 (48)
    [IPU1-0]     19.209906 s:  UTILS: DMA: 0 of 1: Allocated PaRAM = 48 (0x63304800)
    [IPU1-0]     19.397364 s:  Assertion @ Line: 103 in /home/user01/PROCESSOR_SDK_VISION_03_08_00_00/vision_sdk/apps/src/rtos/usecases/common/chains_common_tidl.c: readSize == sizeof(sTIDL_Network_t) : failed !!!
    [IPU1-0]     19.398279 s:  Assertion @ Line: 103 in /home/user01/PROCESSOR_SDK_VISION_03_08_00_00/vision_sdk/apps/src/rtos/usecases/common/chains_common_tidl.c: readSize == sizeof(sTIDL_Network_t) : failed !!!
    
  • Hello again Gaviraju,

    I was able to print to the console and generate you the values you were asking about.

    readSize = 483364
    sizeof(sTIDL_Network_t) = 484384


    Look forward to your help on the next debugging step to see why it is erroring it out.

    Thank you,
    -iFer

  • Hi,

    readSize  should equal to sizeof(sTIDL_Network_t).

     


    From the above print, readSize is correct & other one is not correct. So have you modified the sTIDL_Network_t structure?

    Thanks

    Gaviraju

  • Hello Gaviraju,
    I had not modified the code's functionality. The only time I modified the code was to add the print statements that you had requested.
    Are you able to replicate this or is there something else I may be missing?
    Thank you,
    -iFer
  • Hi,

    Currently I don't have set-up to try out my side, so I will get back next week.

    Thanks

    Gaviraju

  • Hi,

    I tried on my set-up & I'm also got the same error because the files in the below directory are not updated.

    PROCESSOR_SDK_VISION_03_08_00_00\vision_sdk\apps\tools\TIDL_files

     


    So please use the below-updated files.

    TIDL_FILES.zip

  • Great news. Using the new example files you sent, I was able to run it without problems.

    I want to be able to input my own data to run through TIDL, what format does my data need to be? I modified the TIDLCFG.TXT file with the correct resolution for my dataset but had issues.
    I think the format is BGR, but am not sure if that is correct because the output looks off. Does the input need to be a specific resolution? Do I have to train my own net and param files?

    seg_out1.bin.txt
    I have attached a log of the run with Example files. I also attached the output file as well as the TIDLCFG file that I modified to run my dataset.


    I was running 3 images BGR 406*680*3, and seg_out1.bin generated from my dataset was, as I said before, off.

    I can send seg_out1.bin and input dataset if requested by private message.

    Thank you,

    -iFer

  • Hi iFer,

    Yes, the input format is BGR, but you need to import the model using your input to get net and param bin files and use them in the usecase to get the correct output. 

    Thanks,

    Praveen