Part Number: TMS320VC5409A
Tool/software: Code Composer Studio
We have a CCS project, which was developed over 10 years ago to build code running on TMS320VC5409A DSP chip. The project was built using CCS version 3.1.0 running on a Windows XP machine. (The build generated a .out file and we used hex500 to convert it to a .m00 file, if that matters.)
We want to modify the code in this project recently and need to recreate a development environment on Windows 7/10. What version of CCS is my best bet to install on a Windows 7 or 10 machine so tthat I can import this (old) CCS project and build a new execution code? Thanks. I'd also greatly appreciate instructions on what other packages I need to acquire and the steps in installation to recreate an IDE for biold code to run on TMS320C5409A.
The latest CCS I can find on your web site is CCS v3.3. So I downloaded CCS_3.3.83.20_Platinum.zip file. However, it cannot be installed on a Windows 7/10 machine.
Thanks,
Michael Fang