Part Number: TDA4VM
Hello,
I currently have a TDA4VM bundle with Base board + Gateway extension, and I am trying to achieve a stable power-cycle.
The version of U-boot I am using is:
U-Boot 2019.01-g66126341c8 (Dec 11 2019 - 21:52:51 +0000)
Problem:
There are 2 methods of power reset I've tested: One by cutting the power itself (power-cycle) and one using the RESETz button.
When using either of the methods, I see about ~10% of failures, where it will hang in the middle of bootlooder startup (before it gets to U-boot).
Question:
I was wondering if there is a recommended way of resetting/power-cycling this board. (Or is this expected?)
In order for me to automate the validation on this target and really get it ready for development, I need to make sure the reset is working solidly.
Do you have any suggestion on this?