Part Number: TDA4VM
Customer reports the following TDA4 Boot issue on a custom-made board, but one that is modeled directly on the TI SOM from the TDA4 EVM.
The issue is that 10% TDA4 SOM gets hung up on boot and has the error message “Trying to boot from MMC2”.
Of the SOMs that hang up they hang up 80% of the time on boot.
Again, the customer copied the schematic parts and layout that TI did for their EVM SOM.
Here is the log from a SOM failing to boot.
U-Boot SPL 2019.01-g66126341c8 (Oct 24 2019 - 03:52:25 +0000)
SYSFW ABI: 2.6 (firmware rev 0x0013 '19.8.0-v2019.08 (Terrific Llama')
Trying to boot from MMC2
Loading Environment from MMC... *** Warning - No MMC card found, using default environment
Remoteproc 2 started successfully
** File not found /lib/firmware/j7-mcu-r5f0_0-fw **
Starting ATF on ARM64 core...
It was also noted by an TI FAE late last year that the log noted above was also seen in a J7 EVM /SOM. At the time, it was suggested that a couple things can help:
[] Applying power cycle without too much time between turning off and then on
[] Pushing the MCU POR button twice without too much time in between
He went on to further note that "This feels like we have a power rail timing or other sequencing issue, but [he had] not dug deeper on this one yet."