Part Number: AM3505
Background. - We are running up an AM3505AZCN on a new prototype pcb. The design is very much the same to a previous design, with minimal changes.
Problem - to boot from UART3 we assert SYSBOOT5 ("Bootmode") to logic 1 then pulse SYS_NRESPWRON "Pwr_ON_RESET_N).
On release of reset (SYSBOOT 5 still logic1) we see a small burst of data on UART3 - only about 3 bytes. On our previous design we see a large burst of approx 60-70 bytes.
It appears that the ASCI ID begins to transmit then aborts?
Things we have verified are correct:
- The Power supply power-up sequence (although it was initially incorrect - now fixed)
- 26MHZ clock
- 32kHz clock
- SYS_NRESPWRON
- SYSBOOT(8:0) = 001110101 when we assert bit 5 to logic 1
Is there any reason(s) why the ASIC ID transmission would "abort"?
Please advise on what else we should check next.
Thanks in advance.