Sir,
We are using TMS320C6678 DSP (3 nos) in our custom design board, In which DSP 's PCIe, SRIO, Hyperlink, I2C, EMIF, & DDR3 controller Interface are utilized. Board is fully covered with heatsink to dissipate the heat. When the board is booted with all interface, DSP case temperature reaches 98 degree C within 2 hours and going beyond it . Same behavior is observed even the DSP is in idle state.
DSP is running in 1 GHz speed.
Please give your suggestion to reduce the heat.