Tool/software: TI C/C++ Compiler
Hi TI members:
I study the related thread , and try to let our customer board boot u-boot form emmc.
Our SDK use TI Linux 07_00 version.
1. Because our customer board have one SPI flash and one EMMC, so I first confirm our image can boot to kernel successfully by OSPI(bootloader) + EMMC(rootfs) setup, main_uart log as
U-Boot SPL 2020.01-gbb010db1a9 (Oct 12 2020 - 03:47:37 +0000) SYSFW ABI: 3.0 (firmware rev 0x0014 '20.04.1-v2020.04a (Terrific Lla') Reading on-board EEPROM at 0x50 failed 1 Trying to boot from SPI Loading Environment from MMC... *** Warning - No MMC card found, using default environment Loading rproc fw image from device 3 not supported! Loading rproc fw image from device 3 not supported! Starting ATF on ARM64 core... NOTICE: BL31: v2.3():07.00.00.005-dirty NOTICE: BL31: Built : 03:16:46, Oct 12 2020 U-Boot SPL 2020.01-gf9b0d030d3 (Oct 12 2020 - 04:01:58 +0000) SYSFW ABI: 3.0 (firmware rev 0x0014 '20.04.1-v2020.04a (Terrific Lla') Reading on-board EEPROM at 0x50 failed 1 Trying to boot from SPI U-Boot 2020.01-gf9b0d030d3 (Oct 12 2020 - 04:01:58 +0000) SoC: J721E SR1.0 Model: Texas Instruments K3 J721E SoC Reading on-board EEPROM at 0x50 failed 1 Board: J721EX-PM1-SOM rev E2 DRAM: 4 GiB not found for dev hbmc-mux Flash: 0 Bytes MMC: sdhci@4f80000: 0, sdhci@4fb0000: 1 Loading Environment from MMC... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 Reading on-board EEPROM at 0x50 failed 1 Net: Could not get PHY for ethernet@046000000: addr 0 phy_connect() failed No ethernet found. Hit any key to stop autoboot: 2 1 0 switch to partitions #0, OK mmc0(part 0) is current device SD/MMC found on device 0 ** Unrecognized filesystem type ** 16654344 bytes read in 50 ms (317.7 MiB/s) 91121 bytes read in 2 ms (43.4 MiB/s) ## Flattened Device Tree blob at 82000000 Booting using the fdt blob at 0x82000000 Loading Device Tree to 00000000fdda0000, end 00000000fdeb9fff ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080] [ 0.000000] Linux version 5.4.40-gfb1068f4c8 (oe-user@oe-host) (gcc version 9.2.1 20191025 (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10))) #1 SMP PREEMPT Mon Oct 12 01:33:27 UTC 2020 [ 0.000000] Machine model: Texas Instruments K3 J721E SoC [ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '') [ 0.000000] printk: bootconsole [ns16550a0] enabled [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 31 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a3000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a3000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a3100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a3100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a4000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a4100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a5000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a5000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a5100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a5100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a6000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node c66-dma-memory@a6000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a6100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node c66-memory@a6100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a7000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node c66-dma-memory@a7000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a7100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node c66-memory@a7100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a8000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node c71-dma-memory@a8000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a8100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node c71-memory@a8100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000fb000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@fb000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000fb100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@fb100000, compatible id shared-dma-pool [ 0.000000] cma: Reserved 512 MiB at 0x00000000c0000000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.0 [ 0.000000] percpu: Embedded 2 pages/cpu s48408 r8192 d74472 u131072 [ 0.000000] Detected PIPT I-cache on CPU0 [ 0.000000] CPU features: detected: GIC system register CPU interface [ 0.000000] CPU features: detected: EL2 vector hardening [ 0.000000] Built 1 zonelists, mobility grouping off. Total pages: 47825 [ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),128k(ospi.env),128k(ospi.env.backup),1m(ospi.sysfw),-@8m(ospi.rootfs);47034000.hyperbus:512k(hbmc.tiboot3),2m(hbmc.tispl),4m(hbmc.u-boot),256k(hbmc.env),1m(hbmc.sysfw),-@8m(hbmc.rootfs) root=PARTUUID=cf3f74ee-23df-1546-b9c8-38e06600cdde rw rootfstype=ext4 rootwait [ 0.000000] Dentry cache hash table entries: 524288 (order: 6, 4194304 bytes, linear) [ 0.000000] Inode-cache hash table entries: 262144 (order: 5, 2097152 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] software IO TLB: mapped [mem 0xbbff0000-0xbfff0000] (64MB) [ 0.000000] Memory: 3354112K/3063808K available (9534K kernel code, 776K rwdata, 3840K rodata, 1728K init, 695K bss, 18446744073708737024K reserved, 524288K cma-reserved) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2. [ 0.000000] Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000] GICv3: 960 SPIs implemented [ 0.000000] GICv3: 0 Extended SPIs implemented [ 0.000000] GICv3: Distributor has no Range Selector support [ 0.000000] GICv3: 16 PPIs implemented [ 0.000000] GICv3: no VLPI support, no direct LPI support [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001900000 [ 0.000000] ITS [mem 0x01820000-0x0182ffff] [ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS [ 0.000000] ITS@0x0000000001820000: allocated 1048576 Devices @8c0800000 (flat, esz 8, psz 64K, shr 0) [ 0.000000] ITS: using cache flushing for cmd queue [ 0.000000] GICv3: using LPI property table @0x00000008c00c0000 [ 0.000000] GIC: using cache flushing for LPI property table [ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x00000008c00d0000 [ 0.000000] random: get_random_bytes called from start_kernel+0x2b8/0x438 with crng_init=0 [ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns [ 0.000001] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns [ 0.008324] Console: colour dummy device 80x25 [ 0.012879] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000) [ 0.023547] pid_max: default: 32768 minimum: 301 [ 0.028293] LSM: Security Framework initializing [ 0.033035] Mount-cache hash table entries: 8192 (order: 0, 65536 bytes, linear) [ 0.040602] Mountpoint-cache hash table entries: 8192 (order: 0, 65536 bytes, linear) [ 0.072645] ASID allocator initialised with 32768 entries [ 0.086170] rcu: Hierarchical SRCU implementation. [ 0.099114] Platform MSI: gic-its@1820000 domain created [ 0.104631] PCI/MSI: /interconnect@100000/interrupt-controller@1800000/gic-its@1820000 domain created [ 0.122066] smp: Bringing up secondary CPUs ... [ 0.159017] Detected PIPT I-cache on CPU1 [ 0.159033] GICv3: CPU1: found redistributor 1 region 0:0x0000000001920000 [ 0.159042] GICv3: CPU1: using allocated LPI pending table @0x00000008c00e0000 [ 0.159061] CPU1: Booted secondary processor 0x0000000001 [0x411fd080] [ 0.159099] smp: Brought up 1 node, 2 CPUs [ 0.188443] SMP: Total of 2 processors activated. [ 0.193246] CPU features: detected: 32-bit EL0 Support [ 0.198499] CPU features: detected: CRC32 instructions [ 0.209707] CPU: All CPU(s) started at EL2 [ 0.213900] alternatives: patching kernel code [ 0.218820] devtmpfs: initialized [ 0.226221] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.236187] futex hash table entries: 512 (order: -1, 32768 bytes, linear) [ 0.243598] pinctrl core: initialized pinctrl subsystem [ 0.249275] NET: Registered protocol family 16 [ 0.256233] DMA: preallocated 256 KiB pool for atomic allocations [ 0.262729] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.277724] HugeTLB registered 16.0 GiB page size, pre-allocated 0 pages [ 0.284576] HugeTLB registered 512 MiB page size, pre-allocated 0 pages [ 0.291336] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages [ 0.299794] cryptd: max_cpu_qlen set to 1000 [ 0.306778] vsys_3v3: supplied by evm_12v0 [ 0.311053] vsys_5v0: supplied by evm_12v0 [ 0.315559] iommu: Default domain type: Translated [ 0.320752] SCSI subsystem initialized [ 0.324811] mc: Linux media interface: v0.10 [ 0.329180] videodev: Linux video capture interface: v2.00 [ 0.334790] pps_core: LinuxPPS API ver. 1 registered [ 0.339859] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 0.349195] PTP clock support registered [ 0.353205] EDAC MC: Ver: 3.0.0 [ 0.356865] FPGA manager framework [ 0.360374] Advanced Linux Sound Architecture Driver Initialized. [ 0.366879] clocksource: Switched to clocksource arch_sys_counter [ 0.373155] VFS: Disk quotas dquot_6.6.0 [ 0.377200] VFS: Dquot-cache hash table entries: 8192 (order 0, 65536 bytes) [ 0.386411] thermal_sys: Registered thermal governor 'step_wise' [ 0.386412] thermal_sys: Registered thermal governor 'power_allocator' [ 0.392710] NET: Registered protocol family 2 [ 0.404113] tcp_listen_portaddr_hash hash table entries: 4096 (order: 0, 65536 bytes, linear) [ 0.412876] TCP established hash table entries: 32768 (order: 2, 262144 bytes, linear) [ 0.421072] TCP bind hash table entries: 32768 (order: 3, 524288 bytes, linear) [ 0.428748] TCP: Hash tables configured (established 32768 bind 32768) [ 0.435471] UDP hash table entries: 2048 (order: 0, 65536 bytes, linear) [ 0.442359] UDP-Lite hash table entries: 2048 (order: 0, 65536 bytes, linear) [ 0.449739] NET: Registered protocol family 1 [ 0.454423] RPC: Registered named UNIX socket transport module. [ 0.460475] RPC: Registered udp transport module. [ 0.465278] RPC: Registered tcp transport module. [ 0.470081] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.476664] PCI: CLS 0 bytes, default 64 [ 0.480924] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available [ 0.492213] Initialise system trusted keyrings [ 0.496830] workingset: timestamp_bits=46 max_order=16 bucket_order=0 [ 0.505231] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.511462] NFS: Registering the id_resolver key type [ 0.516631] Key type id_resolver registered [ 0.520901] Key type id_legacy registered [ 0.524997] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 0.531950] 9p: Installing v9fs 9p2000 file system support [ 0.544345] Key type asymmetric registered [ 0.548537] Asymmetric key parser 'x509' registered [ 0.553538] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244) [ 0.561100] io scheduler mq-deadline registered [ 0.565727] io scheduler kyber registered [ 0.570817] pinctrl-single 4301c000.pinmux: 94 pins, size 376 [ 0.576875] pinctrl-single 11c000.pinmux: 173 pins, size 692 [ 0.583013] pinctrl-single a40000.timesync_router: 512 pins, size 2048 [ 0.591863] k3-ringacc 2b800000.ringacc: Failed to get MSI domain [ 0.598119] k3-ringacc 3c000000.ringacc: Failed to get MSI domain [ 0.604438] ti-pat 31010000.pat: Found PAT Rev 1.0 with 16384 pages [ 0.610846] debugfs: Directory '31010000.pat' with parent 'regmap' already present! [ 0.618793] ti-pat 31011000.pat: Found PAT Rev 1.0 with 16384 pages [ 0.625204] debugfs: Directory '31011000.pat' with parent 'regmap' already present! [ 0.633146] ti-pat 31012000.pat: Found PAT Rev 1.0 with 16384 pages [ 0.639557] debugfs: Directory '31012000.pat' with parent 'regmap' already present! [ 0.647479] ti-pat 31013000.pat: Found PAT Rev 1.0 with 2048 pages [ 0.653801] debugfs: Directory '31013000.pat' with parent 'regmap' already present! [ 0.661719] ti-pat 31014000.pat: Found PAT Rev 1.0 with 2048 pages [ 0.668040] debugfs: Directory '31014000.pat' with parent 'regmap' already present! [ 0.677303] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled [ 0.688804] brd: module loaded [ 0.694569] loop: module loaded [ 0.699088] libphy: Fixed MDIO Bus: probed [ 0.703421] tun: Universal TUN/TAP device driver, 1.6 [ 0.708795] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k [ 0.716801] igbvf: Copyright (c) 2009 - 2012 Intel Corporation. [ 0.722869] sky2: driver version 1.30 [ 0.727086] VFIO - User Level meta-driver version: 0.3 [ 0.732641] i2c /dev entries driver [ 0.736694] sdhci: Secure Digital Host Controller Interface driver [ 0.743008] sdhci: Copyright(c) Pierre Ossman [ 0.747607] sdhci-pltfm: SDHCI platform and OF driver helper [ 0.753823] ledtrig-cpu: registered to indicate activity on CPUs [ 0.760527] optee: probing for conduit method from DT. [ 0.765785] optee: revision 3.8 (199fca17) [ 0.766075] optee: initialized driver [ 0.774639] NET: Registered protocol family 17 [ 0.779241] 9pnet: Installing 9P2000 support [ 0.783623] Key type dns_resolver registered [ 0.788102] registered taskstats version 1 [ 0.792289] Loading compiled-in X.509 certificates [ 0.800813] k3-ringacc 2b800000.ringacc: Failed to get MSI domain [ 0.807125] k3-ringacc 3c000000.ringacc: Failed to get MSI domain [ 0.814660] ti-sci 44083000.dmsc: ABI: 3.0 (firmware rev 0x0014 '20.04.1-v2020.04a (Terrific Lla') [ 0.839566] random: fast init done [ 0.863002] omap_i2c 40b00000.i2c: bus 0 rev0.12 at 400 kHz [ 0.868968] omap_i2c 40b10000.i2c: bus 1 rev0.12 at 100 kHz [ 0.874957] omap_i2c 42120000.i2c: bus 2 rev0.12 at 400 kHz [ 0.880927] omap_i2c 2000000.i2c: bus 3 rev0.12 at 400 kHz [ 0.886823] omap_i2c 2010000.i2c: bus 4 rev0.12 at 400 kHz [ 0.892698] omap_i2c 2020000.i2c: bus 5 rev0.12 at 400 kHz [ 0.898599] omap_i2c 2030000.i2c: bus 6 rev0.12 at 400 kHz [ 0.904461] omap_i2c 2040000.i2c: bus 7 rev0.12 at 100 kHz [ 0.910356] omap_i2c 2050000.i2c: bus 8 rev0.12 at 100 kHz [ 0.916565] ti-sci-intr interconnect@100000:interconnect@28380000:interrupt-controller2: Interrupt Router 137 domain created [ 0.928134] ti-sci-intr interconnect@100000:interrupt-controller0: Interrupt Router 131 domain created [ 0.937739] ti-sci-intr interconnect@100000:navss@30000000:interrupt-controller1: Interrupt Router 213 domain created [ 0.948745] ti-sci-inta 33d00000.interrupt-controller: Interrupt Aggregator domain 209 created [ 0.965315] cdns-torrent-phy 5050000.serdes: 4 lanes, max bit rate 5.400 Gbps [ 1.970943] j721e-pcie 2910000.pcie: host bridge /interconnect@100000/pcie@2910000 ranges: [ 1.979431] j721e-pcie 2910000.pcie: IO 0x18001000..0x18010fff -> 0x18001000 [ 1.986909] j721e-pcie 2910000.pcie: MEM 0x18011000..0x1fffffff -> 0x18011000 [ 1.994453] j721e-pcie 2910000.pcie: PCI host bridge to bus 0000:00 [ 2.000860] pci_bus 0000:00: root bus resource [bus 00-0f] [ 2.006465] pci_bus 0000:00: root bus resource [io 0x0000-0xffff] (bus address [0x18001000-0x18010fff]) [ 2.016156] pci_bus 0000:00: root bus resource [mem 0x18011000-0x1fffffff] [ 2.023193] pci 0000:00:00.0: [104c:b00d] type 01 class 0x060400 [ 2.029340] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x4 may corrupt adjacent RW1C bits [ 2.039209] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x4 may corrupt adjacent RW1C bits [ 2.049094] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0xe8 may corrupt adjacent RW1C bits [ 2.059052] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x3e may corrupt adjacent RW1C bits [ 2.069018] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x92 may corrupt adjacent RW1C bits [ 2.078980] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0xb2 may corrupt adjacent RW1C bits [ 2.088962] pci 0000:00:00.0: supports D1 [ 2.093056] pci 0000:00:00.0: PME# supported from D0 D1 D3hot [ 2.098927] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x84 may corrupt adjacent RW1C bits [ 2.110282] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring [ 2.118468] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x3e may corrupt adjacent RW1C bits [ 2.128426] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x3e may corrupt adjacent RW1C bits [ 2.138384] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x3e may corrupt adjacent RW1C bits [ 2.149614] pci_bus 0000:01: busn_res: [bus 01-0f] end is updated to 01 [ 2.156381] pci 0000:00:00.0: PCI bridge to [bus 01] [ 2.161598] pcieport 0000:00:00.0: PME: Signaling with IRQ 37 [ 2.167634] pcieport 0000:00:00.0: AER: enabled with IRQ 37 [ 2.174376] k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:235 [ 2.184253] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled [ 2.191013] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66346100, num_proxies:64 [ 2.199819] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:1024, gp-rings[440,150] sci-dev-id:211 [ 2.209959] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled [ 2.216718] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66346100, num_proxies:64 [ 2.224368] omap8250 40a00000.serial: PM domain pd:149 will not be powered off [ 2.231878] 40a00000.serial: ttyS1 at MMIO 0x40a00000 (irq = 7, base_baud = 6000000) is a 8250 [ 2.241014] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 18, base_baud = 3000000) is a 8250 [ 2.249750] printk: console [ttyS2] enabled [ 2.249750] printk: console [ttyS2] enabled [ 2.258186] printk: bootconsole [ns16550a0] disabled [ 2.258186] printk: bootconsole [ns16550a0] disabled [ 2.268521] 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 19, base_baud = 3000000) is a 8250 [ 2.277337] 2840000.serial: ttyS6 at MMIO 0x2840000 (irq = 20, base_baud = 3000000) is a 8250 [ 2.286071] arm-smmu-v3 36600000.smmu: ias 48-bit, oas 48-bit (features 0x00001faf) [ 2.295292] arm-smmu-v3 36600000.smmu: allocated 524288 entries for cmdq [ 2.303879] arm-smmu-v3 36600000.smmu: allocated 524288 entries for evtq [ 3.392268] arm-smmu-v3 36600000.smmu: CMD_SYNC timeout at 0x00000001 [hwprod 0x00000002, hwcons 0x00000001] [ 4.483109] arm-smmu-v3 36600000.smmu: CMD_SYNC timeout at 0x00000004 [hwprod 0x00000005, hwcons 0x00000001] [ 4.492947] arm-smmu-v3 36600000.smmu: msi_domain absent - falling back to wired irqs [ 4.502498] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vdd-hba-supply regulator, assuming enabled [ 4.513012] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vcc-supply regulator, assuming enabled [ 4.523165] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vccq-supply regulator, assuming enabled [ 4.533404] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vccq2-supply regulator, assuming enabled [ 4.544171] scsi host0: ufshcd [ 4.549930] cadence-qspi 47040000.spi: mt35xu512aba_v2 (65536 Kbytes) [ 4.556371] 7 cmdlinepart partitions found on MTD device 47040000.spi.0 [ 4.562968] Creating 7 MTD partitions on "47040000.spi.0": [ 4.568440] 0x000000000000-0x000000080000 : "ospi.tiboot3" [ 4.574339] 0x000000080000-0x000000280000 : "ospi.tispl" [ 4.580002] 0x000000280000-0x000000680000 : "ospi.u-boot" [ 4.585759] 0x000000680000-0x0000006a0000 : "ospi.env" [ 4.591222] 0x0000006a0000-0x0000006c0000 : "ospi.env.backup" [ 4.597319] 0x0000006c0000-0x0000007c0000 : "ospi.sysfw" [ 4.602983] 0x000000800000-0x000004000000 : "ospi.rootfs" [ 4.867082] cadence-qspi 47040000.spi: Cadence QSPI NOR probe failed -517 [ 4.914884] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000 [ 4.922527] libphy: 46000f00.mdio: probed [ 4.926736] mdio_bus 46000f00.mdio: MDIO device at address 0 is missing. [ 4.933439] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00101, cpsw version 0x6BA80100 Ports: 2 [ 4.944876] am65-cpsw-nuss 46000000.ethernet: Failed to request tx dma channel -517 [ 4.953394] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010a, freq:200000000, add_val:4 pps:0 [ 4.961900] mmc0: CQHCI version 5.10 [ 4.962671] cdns-ufshcd 4e84000.ufs: link startup failed 1 [ 4.970979] cdns-ufshcd 4e84000.ufs: UFS Host state=0 [ 4.976022] cdns-ufshcd 4e84000.ufs: lrb in use=0x0, outstanding reqs=0x0 tasks=0x0 [ 4.983661] cdns-ufshcd 4e84000.ufs: saved_err=0x0, saved_uic_err=0x0 [ 4.990086] cdns-ufshcd 4e84000.ufs: Device power mode=1, UIC link state=0 [ 4.996944] cdns-ufshcd 4e84000.ufs: PM in progress=0, sys. suspended=0 [ 5.003542] cdns-ufshcd 4e84000.ufs: Auto BKOPS=0, Host self-block=0 [ 5.005725] mmc0: SDHCI controller on 4f80000.sdhci [4f80000.sdhci] using ADMA 64-bit [ 5.009880] cdns-ufshcd 4e84000.ufs: Clk gate=1 [ 5.009883] cdns-ufshcd 4e84000.ufs: error handling flags=0x0, req. abort count=0 [ 5.018218] davinci_gpio 42110000.gpio: IRQ index 4 not found [ 5.022207] cdns-ufshcd 4e84000.ufs: Host capabilities=0x1587031f, caps=0x0 [ 5.022209] cdns-ufshcd 4e84000.ufs: quirks=0x0, dev. quirks=0x0 [ 5.022213] cdns-ufshcd 4e84000.ufs: ufshcd_print_pwr_info:[RX, TX]: gear=[0, 0], lane[0, 0], pwr[INVALID MODE, INVALID MODE], rate = 0 [ 5.022232] host_regs: 00000000: 1587031f 00000000 00000210 00000000 [ 5.029763] davinci_gpio 42110000.gpio: IRQ not populated, err = -6 [ 5.035407] host_regs: 00000010: 00000000 00000000 00000000 00000000 [ 5.035410] host_regs: 00000020: 00000000 00000470 00000000 00000000 [ 5.035412] host_regs: 00000030: 00000008 00000001 00000000 00000000 [ 5.045672] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fc7100 [ 5.048355] host_regs: 00000040: 00000000 00000000 00000000 00000000 [ 5.060937] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fc7100 [ 5.066835] host_regs: 00000050: 00000000 00000000 00000000 00000000 [ 5.066837] host_regs: 00000060: 00000000 00000000 00000000 00000000 [ 5.066839] host_regs: 00000070: 00000000 00000000 00000000 00000000 [ 5.066841] host_regs: 00000080: 00000000 00000000 00000000 00000000 [ 5.066843] host_regs: 00000090: 00000000 00000000 00000000 00000000 [ 5.073511] omap-mailbox 31f82000.mailbox: omap mailbox rev 0x66fc7100 [ 5.079431] cdns-ufshcd 4e84000.ufs: hba->ufs_version = 0x210, hba->capabilities = 0x1587031f [ 5.079434] cdns-ufshcd 4e84000.ufs: hba->outstanding_reqs = 0x0, hba->outstanding_tasks = 0x0 [ 5.079436] cdns-ufshcd 4e84000.ufs: last_hibern8_exit_tstamp at 0 us, hibern8_exit_cnt = 0 [ 5.086190] omap-mailbox 31f83000.mailbox: omap mailbox rev 0x66fc7100 [ 5.092110] cdns-ufshcd 4e84000.ufs: No record of pa_err errors [ 5.092112] cdns-ufshcd 4e84000.ufs: No record of dl_err errors [ 5.092115] cdns-ufshcd 4e84000.ufs: No record of nl_err errors [ 5.098967] omap-mailbox 31f84000.mailbox: omap mailbox rev 0x66fc7100 [ 5.104959] cdns-ufshcd 4e84000.ufs: No record of tl_err errors [ 5.104961] cdns-ufshcd 4e84000.ufs: No record of dme_err errors [ 5.104962] cdns-ufshcd 4e84000.ufs: No record of auto_hibern8_err errors [ 5.104965] cdns-ufshcd 4e84000.ufs: No record of fatal_err errors [ 5.186996] mmc0: Command Queue Engine enabled [ 5.187489] cdns-ufshcd 4e84000.ufs: link_startup_fail[0] = 0x1 at 4879795 us [ 5.193397] mmc0: new HS400 MMC card at address 0001 [ 5.199292] cdns-ufshcd 4e84000.ufs: No record of resume_fail errors [ 5.210042] mmcblk0: mmc0:0001 S0J58X 59.3 GiB [ 5.211710] cdns-ufshcd 4e84000.ufs: No record of suspend_fail errors [ 5.217805] mmcblk0boot0: mmc0:0001 S0J58X partition 1 31.5 MiB [ 5.224465] cdns-ufshcd 4e84000.ufs: No record of dev_reset errors [ 5.224467] cdns-ufshcd 4e84000.ufs: No record of host_reset errors [ 5.230735] mmcblk0boot1: mmc0:0001 S0J58X partition 2 31.5 MiB [ 5.235059] cdns-ufshcd 4e84000.ufs: No record of task_abort errors [ 5.242232] mmcblk0rpmb: mmc0:0001 S0J58X partition 3 4.00 MiB, chardev (240:0) [ 5.247125] cdns-ufshcd 4e84000.ufs: clk: core_clk, rate: 250000000 [ 5.261035] mmcblk0: p1 [ 5.264401] cdns-ufshcd 4e84000.ufs: clk: phy_clk, rate: 19200000 [ 5.264404] cdns-ufshcd 4e84000.ufs: clk: ref_clk, rate: 19200000 [ 6.100885] j721e-pcie 2900000.pcie: host bridge /interconnect@100000/pcie@2900000 ranges: [ 6.109153] j721e-pcie 2900000.pcie: IO 0x10001000..0x10010fff -> 0x10001000 [ 6.116452] j721e-pcie 2900000.pcie: MEM 0x10011000..0x17ffffff -> 0x10011000 [ 6.123815] j721e-pcie 2900000.pcie: PCI host bridge to bus 0001:00 [ 6.130070] pci_bus 0001:00: root bus resource [bus 00-0f] [ 6.135543] pci_bus 0001:00: root bus resource [io 0x10000-0x1ffff] (bus address [0x10001000-0x10010fff]) [ 6.145175] pci_bus 0001:00: root bus resource [mem 0x10011000-0x17ffffff] [ 6.152047] pci 0001:00:00.0: [104c:b00d] type 01 class 0x060400 [ 6.158105] pci 0001:00:00.0: supports D1 [ 6.162104] pci 0001:00:00.0: PME# supported from D0 D1 D3hot [ 6.169253] pci 0001:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring [ 6.178518] pci_bus 0001:01: busn_res: [bus 01-0f] end is updated to 01 [ 6.185124] pci 0001:00:00.0: PCI bridge to [bus 01] [ 6.190241] pcieport 0001:00:00.0: PME: Signaling with IRQ 396 [ 6.196180] pcieport 0001:00:00.0: AER: enabled with IRQ 396 [ 7.200895] j721e-pcie 2920000.pcie: host bridge /interconnect@100000/pcie@2920000 ranges: [ 7.209158] j721e-pcie 2920000.pcie: IO 0x4400001000..0x4400010fff -> 0x00001000 [ 7.216803] j721e-pcie 2920000.pcie: MEM 0x4400011000..0x4407ffffff -> 0x00011000 [ 7.224498] j721e-pcie 2920000.pcie: PCI host bridge to bus 0002:00 [ 7.230753] pci_bus 0002:00: root bus resource [bus 00-0f] [ 7.236225] pci_bus 0002:00: root bus resource [io 0x20000-0x2ffff] (bus address [0x1000-0x10fff]) [ 7.245250] pci_bus 0002:00: root bus resource [mem 0x4400011000-0x4407ffffff] (bus address [0x00011000-0x07ffffff]) [ 7.255758] pci 0002:00:00.0: [104c:b00d] type 01 class 0x060400 [ 7.261756] pci_generic_config_write32: 50 callbacks suppressed [ 7.261759] pci_bus 0002:00: 2-byte config write to 0002:00:00.0 offset 0x4 may corrupt adjacent RW1C bits [ 7.277293] pci_bus 0002:00: 2-byte config write to 0002:00:00.0 offset 0x4 may corrupt adjacent RW1C bits [ 7.286942] pci_bus 0002:00: 2-byte config write to 0002:00:00.0 offset 0xe8 may corrupt adjacent RW1C bits [ 7.296662] pci_bus 0002:00: 2-byte config write to 0002:00:00.0 offset 0x3e may corrupt adjacent RW1C bits [ 7.306389] pci_bus 0002:00: 2-byte config write to 0002:00:00.0 offset 0x92 may corrupt adjacent RW1C bits [ 7.316113] pci_bus 0002:00: 2-byte config write to 0002:00:00.0 offset 0xb2 may corrupt adjacent RW1C bits [ 7.325856] pci 0002:00:00.0: supports D1 [ 7.329855] pci 0002:00:00.0: PME# supported from D0 D1 D3hot [ 7.335587] pci_bus 0002:00: 2-byte config write to 0002:00:00.0 offset 0x84 may corrupt adjacent RW1C bits [ 7.346647] pci 0002:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring [ 7.354636] pci_bus 0002:00: 2-byte config write to 0002:00:00.0 offset 0x3e may corrupt adjacent RW1C bits [ 7.364356] pci_bus 0002:00: 2-byte config write to 0002:00:00.0 offset 0x3e may corrupt adjacent RW1C bits [ 7.374077] pci_bus 0002:00: 2-byte config write to 0002:00:00.0 offset 0x3e may corrupt adjacent RW1C bits [ 7.385061] pci_bus 0002:01: busn_res: [bus 01-0f] end is updated to 01 [ 7.391665] pci 0002:00:00.0: PCI bridge to [bus 01] [ 7.396750] pcieport 0002:00:00.0: PME: Signaling with IRQ 398 [ 7.402673] pcieport 0002:00:00.0: AER: enabled with IRQ 398 [ 7.409320] ti-udma 285c0000.dma-controller: Channels: 24 (tchan: 12, rchan: 12, gp-rflow: 8) [ 7.419613] ti-udma 31150000.dma-controller: Channels: 84 (tchan: 42, rchan: 42, gp-rflow: 16) [ 7.431492] cadence-qspi 47040000.spi: mt35xu512aba_v2 (65536 Kbytes) [ 7.437924] 7 cmdlinepart partitions found on MTD device 47040000.spi.0 [ 7.444522] Creating 7 MTD partitions on "47040000.spi.0": [ 7.449994] 0x000000000000-0x000000080000 : "ospi.tiboot3" [ 7.455904] 0x000000080000-0x000000280000 : "ospi.tispl" [ 7.461582] 0x000000280000-0x000000680000 : "ospi.u-boot" [ 7.467360] 0x000000680000-0x0000006a0000 : "ospi.env" [ 7.472863] 0x0000006a0000-0x0000006c0000 : "ospi.env.backup" [ 7.479007] 0x0000006c0000-0x0000007c0000 : "ospi.sysfw" [ 7.484649] 0x000000800000-0x000004000000 : "ospi.rootfs" [ 7.530889] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000 [ 7.538532] libphy: 46000f00.mdio: probed [ 7.542743] mdio_bus 46000f00.mdio: MDIO device at address 0 is missing. [ 7.549444] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00101, cpsw version 0x6BA80100 Ports: 2 [ 7.561604] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48 [ 7.568740] pps pps0: new PPS source ptp1 [ 7.572882] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010a, freq:500000000, add_val:1 pps:1 [ 7.581825] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 57.4 [ 7.589116] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64 [ 7.597220] debugfs: Directory 'pd:242' with parent 'pm_genpd' already present! [ 7.604572] debugfs: Directory 'pd:241' with parent 'pm_genpd' already present! [ 7.611877] debugfs: Directory 'pd:240' with parent 'pm_genpd' already present! [ 7.619180] debugfs: Directory 'pd:239' with parent 'pm_genpd' already present! [ 7.627153] hctosys: unable to open rtc device (rtc0) [ 7.644655] ALSA device list: [ 7.647615] No soundcards found. [ 7.660508] EXT4-fs (mmcblk0p1): mounted filesystem with ordered data mode. Opts: (null) [ 7.668609] VFS: Mounted root (ext4 filesystem) on device 179:1. [ 7.675680] devtmpfs: mounted [ 7.679125] Freeing unused kernel memory: 1728K [ 7.683659] Run /sbin/init as init process [ 7.729310] systemd[1]: System time before build time, advancing clock. [ 7.753569] NET: Registered protocol family 10 [ 7.758343] Segment Routing with IPv6 [ 7.769362] systemd[1]: systemd 244.3+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid) [ 7.791061] systemd[1]: Detected architecture arm64. Welcome to Arago 2020.05! [ 7.823228] systemd[1]: Set hostname to <j7-evm>. [ 7.830007] random: systemd: uninitialized urandom read (16 bytes read) [ 7.836624] systemd[1]: Initializing machine ID from random generator. [ 7.952962] systemd[1]: /lib/systemd/system/docker.socket:6: ListenStream= references a path below legacy directory /var/run/, updating /var/run/docker.sock �� /run/docker.sock; please update the unit file accordingly. [ 8.007983] random: systemd: uninitialized urandom read (16 bytes read) [ 8.014675] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling. [ 8.027000] systemd[1]: (This warning is only shown for the first unit using IP firewalling.) [ 8.036689] systemd[1]: Created slice system-getty.slice. [ OK ] Created slice system-getty.slice. [ 8.058941] random: systemd: uninitialized urandom read (16 bytes read) [ 8.066046] systemd[1]: Created slice system-serial\x2dgetty.slice. [ OK ] Created slice system-serial\x2dgetty.slice. [ 8.087369] systemd[1]: Created slice User and Session Slice. [ OK ] Created slice User and Session Slice. [ 8.107008] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. [ OK ] Started Dispatch Password �Kts to Console Directory Watch. [ 8.130971] systemd[1]: Started Forward Password Requests to Wall Directory Watch. [ OK ] Started Forward Password R�Kuests to Wall Directory Watch. [ 8.154967] systemd[1]: Reached target Paths. [ OK ] Reached target Paths. [ 8.170930] systemd[1]: Reached target Remote File Systems. [ OK ] Reached target Remote File Systems. [ 8.190925] systemd[1]: Reached target Slices. [ OK ] Reached target Slices. [ 8.206928] systemd[1]: Reached target Swap. [ OK ] Reached target Swap. [ 8.227355] systemd[1]: Listening on RPCbind Server Activation Socket. [ OK ] Listening on RPCbind Server Activation Socket. [ 8.250937] systemd[1]: Reached target RPC Port Mapper. [ OK ] Reached target RPC Port Mapper. [ 8.272644] systemd[1]: Listening on Process Core Dump Socket. [ OK ] Listening on Process Core Dump Socket. [ 8.295007] systemd[1]: Listening on initctl Compatibility Named Pipe. [ OK ] Listening on initctl Compatibility Named Pipe. [ 8.322150] systemd[1]: Condition check resulted in Journal Audit Socket being skipped. [ 8.330399] systemd[1]: Listening on Journal Socket (/dev/log). [ OK ] Listening on Journal Socket (/dev/log). [ 8.351118] systemd[1]: Listening on Journal Socket. [ OK ] Listening on Journal Socket. [ 8.367128] systemd[1]: Listening on Network Service Netlink Socket. [ OK ] Listening on Network Service Netlink Socket. [ 8.387048] systemd[1]: Listening on udev Control Socket. [ OK ] Listening on udev Control Socket. [ 8.403009] systemd[1]: Listening on udev Kernel Socket. [ OK ] Listening on udev Kernel Socket. [ 8.420918] systemd[1]: Mounting Huge Pages File System... Mounting Huge Pages File System... [ 8.445041] systemd[1]: Mounting POSIX Message Queue File System... Mounting POSIX Message Queue File System... [ 8.468759] systemd[1]: Mounting Kernel Debug File System... Mounting Kernel Debug File System... [ 8.487267] systemd[1]: Mounting Temporary Directory (/tmp)... Mounting Temporary Directory (/tmp)... [ 8.505377] systemd[1]: Starting Create list of static device nodes for the current kernel... Starting Create list of st�Kodes for the current kernel... [ 8.532854] systemd[1]: Starting Start psplash boot splash screen... Starting Start psplash boot splash screen... [ 8.557684] systemd[1]: Started Hardware RNG Entropy Gatherer Daemon. [ OK ] Started Hardware RNG Entropy Gatherer Daemon. [ 8.581072] systemd[1]: Starting RPC Bind... Starting RPC Bind... [ 8.599015] systemd[1]: Condition check resulted in File System Check on Root Device being skipped. [ 8.617250] systemd[1]: Starting Journal Service... Starting Journal Service... [ 8.630058] systemd[1]: Starting Load Kernel Modules... Starting Load Kernel Modules... [ 8.641060] cryptodev: loading out-of-tree module taints kernel. [ 8.656985] systemd[1]: Starting Remount Root and Kernel File Systems... [ 8.667051] cryptodev: driver 1.10 loaded. Starting Remount Root and Kernel File Systems... [ 8.683746] EXT4-fs (mmcblk0p1): re-mounted. Opts: (null) [ 8.691317] systemd[1]: Starting udev Coldplug all Devices... Starting udev Coldplug all Devices... [ 8.713164] systemd[1]: Started RPC Bind. [ OK ] Started RPC Bind. [ 8.731147] systemd[1]: Started Journal Service. [ OK ] Started Journal Service. [ OK ] Mounted Huge Pages File System. [ OK ] Mounted POSIX Message Queue File System. [ OK ] Mounted Kernel Debug File System. [ OK ] Mounted Temporary Directory (/tmp). [ OK ] Started Create list of sta�K nodes for the current kernel. [FAILED] Failed to start Start psplash boot splash screen. See 'systemctl status psplash-start.service' for details. [DEPEND] Dependency failed for Star�Kprogress communication helper. [ OK ] Started Load Kernel Modules. [ OK ] Started Remount Root and Kernel File Systems. Mounting Kernel Configuration File System... Starting Flush Journal to Persistent Storage... [ 8.941118] systemd-journald[218]: Received client request to flush runtime journal. Starting Apply Kernel Variables... Starting Create System Users... [ OK ] Mounted Kernel Configuration File System. [ OK ] Started Flush Journal to Persistent Storage. [ OK ] Started Apply Kernel Variables. [ OK ] Started Create System Users. Starting Create Static Device Nodes in /dev... [ OK ] Started Create Static Device Nodes in /dev. [ OK ] Reached target Local File Systems (Pre). Mounting /media/ram... Mounting /var/volatile... Starting udev Kernel Device Manager... [ OK ] Started udev Coldplug all Devices. [ OK ] Mounted /media/ram. [ OK ] Started udev Kernel Device Manager. [ OK ] Mounted /var/volatile. Starting Load/Save Random Seed... [ OK ] Reached target Local File Systems. Starting Rebuild Dynamic Linker Cache... Starting Create Volatile Files and Directories... [ OK ] Started Create Volatile Files and Directories. Starting Run pending postinsts... Starting Rebuild Journal Catalog... [FAILED] Failed to start Network Time Synchronization. See 'systemctl status systemd-timesyncd.service' for details. [ OK ] Reached target System Time Set. [ OK ] Reached target System Time Synchronized. Starting Update UTMP about System Boot/Shutdown... [ OK ] Started Rebuild Journal Catalog. [ OK ] Stopped Network Time Synchronization. [FAILED] Failed to start Network Time Synchronization. See 'systemctl status systemd-timesyncd.service' for details. [ OK ] Stopped Network Time Synchronization. [FAILED] Failed to start Network Time Synchronization. See 'systemctl status systemd-timesyncd.service' for details. [ OK ] Started Rebuild Dynamic Linker Cache. [ OK ] Started Update UTMP about System Boot/Shutdown. [ OK ] Started Run pending postinsts. [ 9.562952] rti-wdt 2200000.rti: heartbeat 60 sec [ OK ] Stopped Network Time Synchronization. [FAILED] Failed to start Network Time Synchronization. See 'systemctl status systemd-timesyncd.service' for details. Starting Update is Completed... [ OK ] Started Update is Completed. [ OK ] Stopped Network Time Synchronization. [FAILED] Failed to start Network Time Synchronization. See 'systemctl status systemd-timesyncd.service' for details. [ OK ] Reached target System Initialization[ 9.702947] rti-wdt 2210000.rti: heartbeat 60 sec . [ OK ] Started Daily rotation of log files. [ OK ] Started Daily Cleanup of Temporary Directories. [ OK ] Reached target Timers. [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket. [ OK ] Listening on D-Bus System Message Bus Socket. Starting Docker Socket for the API. [ OK ] Listening on Docker Socket for the API. [ OK ] Reached target Sockets. [ OK ] Reached target Basic System. [ OK ] Started Job spooling tools. [ 9.870212] k3-dsp-rproc 4d80800000.dsp: assigned reserved memory node c66-dma-memory@a7000000 [ OK ] Started Periodic Command Scheduler. [ OK ] Started D-Bus System Message Bus. Starting Print notice about GPLv3 packages... Starting IPv6 Packet Filtering Framework... Starting IPv4 Packet Filtering Framework... Starting rc.pvr.service... [FAILED] Failed to start Login Service. See 'systemctl status systemd-logind.service' for details. [ OK ] Stopped Network Time Synchronization. [FAILED] Failed to start Network Time Synchronization. See 'systemctl status systemd-timesyncd.service' for details. [ OK ] Started TEE Supplicant. [ OK ] Started IPv6 Packet Filtering Framework. [ OK ] Started IPv4 Packet Filtering Framework. [ OK ] Reached target Network (Pre). [ OK ] Stopped Login Service. [FAILED] Failed to start Login Service. See 'systemctl status systemd-logind.service' for details. Starting Network Service... [ OK ] Stopped Login Service. [FAILED] Failed to start Login Service. See 'systemctl status systemd-logind.service' for details. [ OK ] Stopped Login Service. [FAILED] Failed to start Login Service[ 10.045351] PVR_K: 341: Read BVNC 22.104.208.318 from HW device registers . See 'systemctl status systemd-logind.service' for details. [ OK ] Stopped Login Service. [ 10.062962] PVR_K: 341: RGX Device initialised with BVNC 22.104.208.318 ;1;31mFAILED] Failed to start Login Service. See 'systemctl status systemd-logind.service' for details. [ OK ] Stopped Login Service. [FAILED] Failed to start Login Service. See 'systemctl status systemd-logind.service' for details. [ OK [ 10.096737] [drm] Initialized pvr 1.10.5371573 20170530 for 4e20000000.gpu on minor 0 ] Started Network Service. Starting Wait for Network to be Configured... [FAILED] Failed to start Network Name Resolution. See 'systemctl status systemd-resolved.service' for details. [ OK ] Reached target Network. [ OK ] Reached target Host and Network Name Lookups. Starting Avahi mDNS/DNS-SD Stack... [ OK ] Started NFS status monitor for NFSv2/3 locking.. Starting Permit User Sessions... [ OK ] Stopped Network Name Resolution. [FAILED] Failed to start Network Name Resolution. See 'systemctl status systemd-resolved.service' for details. [ OK ] Stopped Network Name Resolution. [FAILED] Failed to start Network Name Resolution. See 'systemctl status systemd-resolved.service' for details. [ OK ] Stopped Network Name Resolution. [FAILED] Failed to start Network Name Resolution. See 's[ 10.207174] k3-dsp-rproc 4d80800000.dsp: configured DSP for remoteproc mode ystemctl status systemd-resolved.service' for details. [ OK ] Started Avahi mDNS/DNS-SD Stack. [ OK ] Stopped Network Name Resolution. [FAILED] Failed to start Network Name Resolution. See 'systemctl status systemd-resolved.service' for details. [ OK ] Started Permit User Sessions. [ OK ] Started Getty on tty1. [ OK ] Started Serial Getty on ttyS2. [ OK ] Started Serial Getty on ttyS3. [ OK ] Reached target Login Prompts. Starting Synchronize System and HW clocks... [ OK ] Stopped Network Name Resolution. [FAILED] Failed to start Network Name Resolution. See 'systemctl status systemd-resolved.service' for details. [FAILED] Failed to start Synchronize System and HW clocks. See 'systemctl status sync-clocks.service' for details. [ 10.314581] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013). [ 10.325413] [drm] No driver support for vblank timestamp query. [ 10.335641] [drm] Initialized tidss 1.0.0 20180215 for 4a00000.dss on minor 1 [ 10.556457] Console: switching to colour frame buffer device 240x67 [ 10.586902] tidss 4a00000.dss: fb0: tidssdrmfb frame buffer device *************************************************************** *************************************************************** NOTICE: This file system contains the following GPLv3 packages: bash-dev bash bc binutils cifs-utils cpio dosfstools elfutils gawk gdb gzip less libasm1 libbfd libdw1 libelf1 libgdbm-compat4 libgdbm-dev libgdbm6 libgmp10 libidn2-0 libreadline-dev libreadline8 libunistring2 m4-dev m4 nettle tar which If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove <package> Where <package> is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** *************************************************************** [ 10.842279] k3-dsp-rproc 4d80800000.dsp: local reset is deasserted for device [ OK ] Started Print notice about GPLv3 packages. [ 10.861280] platform 41000000.r5f: configured R5F for remoteproc mode [ 10.908454] remoteproc remoteproc0: 4d80800000.dsp is available [ 10.980563] remoteproc remoteproc0: Direct firmware load for j7-c66_0-fw failed with error -2 [ 10.990562] remoteproc remoteproc0: powering up 4d80800000.dsp [ 10.996424] remoteproc remoteproc0: Direct firmware load for j7-c66_0-fw failed with error -2 [ 11.005735] k3-dsp-rproc 4d81800000.dsp: assigned reserved memory node c66-dma-memory@a6000000 [ 11.014358] remoteproc remoteproc0: request_firmware failed: -2 [ 11.130491] platform 41000000.r5f: assigned reserved memory node r5f-dma-memory@a0000000 [ 11.206703] remoteproc remoteproc1: 41000000.r5f is available [ 11.255033] k3-dsp-rproc 4d81800000.dsp: configured DSP for remoteproc mode [ 11.344954] remoteproc remoteproc1: Direct firmware load for j7-mcu-r5f0_0-fw failed with error -2 [ 11.355483] remoteproc remoteproc1: powering up 41000000.r5f [ 11.361164] remoteproc remoteproc1: Direct firmware load for j7-mcu-r5f0_0-fw failed with error -2 [ 11.374921] platform 5c00000.r5f: configured R5F for remoteproc mode [ 11.377135] remoteproc remoteproc1: request_firmware failed: -2 [ 11.417876] k3-dsp-rproc 4d81800000.dsp: local reset is deasserted for device [ 11.495608] am65-cpsw-nuss 46000000.ethernet: phy /interconnect@100000/interconnect@28380000/ethernet@46000000/mdio@f00/ethernet-phy@0 not found on slave 1 [ 11.562908] random: crng init done [ 11.566302] random: 7 urandom warning(s) missed due to ratelimiting [ 11.582796] platform 5c00000.r5f: assigned reserved memory node r5f-dma-memory@a1000000 [ 11.583086] remoteproc remoteproc2: 4d81800000.dsp is available [ 11.598989] remoteproc remoteproc3: 5c00000.r5f is available [ 11.610940] remoteproc remoteproc3: Direct firmware load for j7-main-r5f0_0-fw failed with error -2 [ 11.622203] remoteproc remoteproc3: powering up 5c00000.r5f [ 11.627815] remoteproc remoteproc3: Direct firmware load for j7-main-r5f0_0-fw failed with error -2 [ 11.644304] remoteproc remoteproc3: request_firmware failed: -2 [ OK ] Started Load/Save Random Seed. [ 11.659417] platform 5d00000.r5f: configured R5F for remoteproc mode [ 11.736476] platform 5d00000.r5f: assigned reserved memory node r5f-dma-memory@a3000000 [ 11.785854] remoteproc remoteproc2: Direct firmware load for j7-c66_1-fw failed with error -2 [ 11.798248] remoteproc remoteproc2: powering up 4d81800000.dsp [ 11.806916] remoteproc remoteproc2: Direct firmware load for j7-c66_1-fw failed with error -2 [ 11.822903] remoteproc remoteproc2: request_firmware failed: -2 [ 11.829821] k3-dsp-rproc 64800000.dsp: assigned reserved memory node c71-dma-memory@a8000000 [ 11.912380] remoteproc remoteproc4: 5d00000.r5f is available [ 12.030893] k3-dsp-rproc 64800000.dsp: configured DSP for remoteproc mode [ 12.048963] remoteproc remoteproc4: Direct firmware load for j7-main-r5f0_1-fw failed with error -2 [ 12.059467] remoteproc remoteproc5: 64800000.dsp is available [ 12.065380] remoteproc remoteproc4: powering up 5d00000.r5f [ 12.070976] remoteproc remoteproc4: Direct firmware load for j7-main-r5f0_1-fw failed with error -2 [ 12.084451] remoteproc remoteproc4: request_firmware failed: -2 [ 12.110918] platform 5e00000.r5f: configured R5F for remoteproc mode [ 12.164357] remoteproc remoteproc5: Direct firmware load for j7-c71_0-fw failed with error -2 [ 12.174678] remoteproc remoteproc5: powering up 64800000.dsp [ 12.187069] remoteproc remoteproc5: Direct firmware load for j7-c71_0-fw failed with error -2 [ 12.198888] remoteproc remoteproc5: request_firmware failed: -2 [ 12.215189] platform 5e00000.r5f: assigned reserved memory node r5f-dma-memory@a4000000 [ 12.392455] remoteproc remoteproc6: 5e00000.r5f is available [ 12.548397] remoteproc remoteproc6: Direct firmware load for j7-main-r5f1_0-fw failed with error -2 [ 12.562890] remoteproc remoteproc6: powering up 5e00000.r5f [ 12.568486] remoteproc remoteproc6: Direct firmware load for j7-main-r5f1_0-fw failed with error -2 [ 12.579676] platform 5f00000.r5f: configured R5F for remoteproc mode [ 12.586061] remoteproc remoteproc6: request_firmware failed: -2 [ 12.736735] platform 5f00000.r5f: assigned reserved memory node r5f-dma-memory@a5000000 [ 12.885020] remoteproc remoteproc7: 5f00000.r5f is available [ 12.966964] remoteproc remoteproc7: Direct firmware load for j7-main-r5f1_1-fw failed with error -2 [ 12.978950] remoteproc remoteproc7: powering up 5f00000.r5f [ 12.986505] remoteproc remoteproc7: Direct firmware load for j7-main-r5f1_1-fw failed with error -2 [ 13.001124] remoteproc remoteproc7: request_firmware failed: -2 [ OK ] Created slice system-weston.slice 13.061280] remoteproc remoteproc8: b034000.pru is available m. [ OK ] Started Weston Wayland Compositor. [FAILED] Failed to start Login Service. See 'systemctl status systemd-logind.service' for details. [ 13.128530] omap_rng 4e10000.trng: Random Number Generator ver. 241b34c [ 13.197898] pru-rproc b034000.pru: PRU rproc node /interconnect@100000/icssg@b000000/pru@34000 probed successfully [ 13.287906] remoteproc remoteproc9: b004000.rtu is available [ 13.312812] pru-rproc b004000.rtu: PRU rproc node /interconnect@100000/icssg@b000000/rtu@4000 probed successfully [ OK ] Started rc.pvr.service. Starting weston.service... [ 13.434980] pru-rproc b00a000.txpru: IRQ vring not found [ 13.468468] pru-rproc b00a000.txpru: IRQ kick not found [ 13.479017] remoteproc remoteproc10: b00a000.txpru is available [ 13.484985] pru-rproc b00a000.txpru: PRU rproc node /interconnect@100000/icssg@b000000/txpru@a000 probed successfully [ 13.507704] remoteproc remoteproc11: b038000.pru is available [ 13.518911] pru-rproc b038000.pru: PRU rproc node /interconnect@100000/icssg@b000000/pru@38000 probed successfully [ 13.535309] remoteproc remoteproc12: b006000.rtu is available [ 13.542916] pru-rproc b006000.rtu: PRU rproc node /interconnect@100000/icssg@b000000/rtu@6000 probed successfully [ 13.563161] pru-rproc b00c000.txpru: IRQ vring not found [ 13.568477] pru-rproc b00c000.txpru: IRQ kick not found [ 13.582988] remoteproc remoteproc13: b00c000.txpru is available [ 13.588932] pru-rproc b00c000.txpru: PRU rproc node /interconnect@100000/icssg@b000000/txpru@c000 probed successfully [ 13.611312] remoteproc remoteproc14: b134000.pru is available [ 13.617083] pru-rproc b134000.pru: PRU rproc node /interconnect@100000/icssg@b100000/pru@34000 probed successfully [ 13.635274] remoteproc remoteproc15: b104000.rtu is available [ 13.641039] pru-rproc b104000.rtu: PRU rproc node /interconnect@100000/icssg@b100000/rtu@4000 probed successfully [ 13.663170] pru-rproc b10a000.txpru: IRQ vring not found [ 13.668484] pru-rproc b10a000.txpru: IRQ kick not found [ 13.678982] remoteproc remoteproc16: b10a000.txpru is available [ 13.684962] pru-rproc b10a000.txpru: PRU rproc node /interconnect@100000/icssg@b100000/txpru@a000 probed successfully [ 13.703281] remoteproc remoteproc17: b138000.pru is available [ 13.709052] pru-rproc b138000.pru: PRU rproc node /interconnect@100000/icssg@b100000/pru@38000 probed successfully [ 13.727281] remoteproc remoteproc18: b106000.rtu is available [ 13.733044] pru-rproc b106000.rtu: PRU rproc node /interconnect@100000/icssg@b100000/rtu@6000 probed successfully [ 13.751094] pru-rproc b10c000.txpru: IRQ vring not found [ 13.751943] cdns-usb3 6000000.usb: DRD version v1 (ID: 0004024e, rev: 00000200) [ 13.756921] pru-rproc b10c000.txpru: IRQ kick not found [ 13.780895] remoteproc remoteproc19: b10c000.txpru is available [ 13.793173] pru-rproc b10c000.txpru: PRU rproc node /interconnect@100000/icssg@b100000/txpru@c000 probed successfully [ 14.578916] cdns-usb3 6000000.usb: Initialized ep0 support: [ 14.584753] cdns-usb3 6000000.usb: Initialized ep1out support: BULK, INT ISO [ 14.598884] cdns-usb3 6000000.usb: Initialized ep2out support: BULK, INT ISO [ 14.606018] cdns-usb3 6000000.usb: Initialized ep3out support: BULK, INT ISO [ 14.614898] cdns-usb3 6000000.usb: Initialized ep4out support: BULK, INT ISO [ 14.624154] cdns-usb3 6000000.usb: Initialized ep5out support: BULK, INT ISO [ 14.634891] cdns-usb3 6000000.usb: Initialized ep6out support: BULK, INT ISO [ 14.646881] cdns-usb3 6000000.usb: Initialized ep7out support: BULK, INT ISO [ 14.654013] cdns-usb3 6000000.usb: Initialized ep8out support: BULK, INT ISO [ 14.666881] cdns-usb3 6000000.usb: Initialized ep9out support: BULK, INT ISO [ 14.674011] cdns-usb3 6000000.usb: Initialized ep10out support: BULK, INT ISO [ 14.686881] cdns-usb3 6000000.usb: Initialized ep11out support: BULK, INT ISO [ 14.694091] cdns-usb3 6000000.usb: Initialized ep12out support: BULK, INT ISO [ 14.706881] cdns-usb3 6000000.usb: Initialized ep13out support: BULK, INT ISO [ 14.714092] cdns-usb3 6000000.usb: Initialized ep14out support: BULK, INT ISO [ 14.726881] cdns-usb3 6000000.usb: Initialized ep15out support: BULK, INT ISO [ 14.734097] cdns-usb3 6000000.usb: Initialized ep1in support: BULK, INT ISO [ 14.742895] cdns-usb3 6000000.usb: Initialized ep2in support: BULK, INT ISO [ 14.752049] cdns-usb3 6000000.usb: Initialized ep3in support: BULK, INT ISO [ 14.763493] cdns-usb3 6000000.usb: Initialized ep4in support: BULK, INT ISO [ 14.775076] cdns-usb3 6000000.usb: Initialized ep5in support: BULK, INT ISO [ 14.787071] cdns-usb3 6000000.usb: Initialized ep6in support: BULK, INT ISO [ 14.797821] cdns-usb3 6000000.usb: Initialized ep7in support: BULK, INT ISO [ 14.806887] cdns-usb3 6000000.usb: Initialized ep8in support: BULK, INT ISO [ 14.813924] cdns-usb3 6000000.usb: Initialized ep9in support: BULK, INT ISO [ 14.826882] cdns-usb3 6000000.usb: Initialized ep10in support: BULK, INT ISO [ 14.834013] cdns-usb3 6000000.usb: Initialized ep11in support: BULK, INT ISO [ 14.846880] cdns-usb3 6000000.usb: Initialized ep12in support: BULK, INT ISO [ 14.854010] cdns-usb3 6000000.usb: Initialized ep13in support: BULK, INT ISO [ 14.866880] cdns-usb3 6000000.usb: Initialized ep14in support: BULK, INT ISO [ 14.874012] cdns-usb3 6000000.usb: Initialized ep15in support: BULK, INT ISO [ 14.891387] cdns-usb3 6400000.usb: DRD version v1 (ID: 0004024e, rev: 00000200) [ 14.936826] usbcore: registered new interface driver usbfs [ 14.947247] usbcore: registered new interface driver hub [ 14.959641] usbcore: registered new device driver usb [ 14.971168] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller [ 14.976660] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 1 [ 14.999041] xhci-hcd xhci-hcd.2.auto: hcc params 0x200073c9 hci version 0x100 quirks 0x0000000000010010 [ 15.008737] xhci-hcd xhci-hcd.2.auto: irq 512, io mem 0x06410000 [ 15.023018] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.04 [ 15.034894] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 15.042107] usb usb1: Product: xHCI Host Controller [ 15.054881] usb usb1: Manufacturer: Linux 5.4.40-gfb1068f4c8 xhci-hcd [ 15.061312] usb usb1: SerialNumber: xhci-hcd.2.auto [ 15.071539] hub 1-0:1.0: USB hub found [ 15.075302] hub 1-0:1.0: 1 port detected [ 15.083512] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller [ 15.089004] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 2 [ 15.098907] xhci-hcd xhci-hcd.2.auto: Host supports USB 3.0 SuperSpeed [ 15.110918] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM. [ 15.121257] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 5.04 [ 15.121261] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 15.121264] usb usb2: Product: xHCI Host Controller [ 15.121266] usb usb2: Manufacturer: Linux 5.4.40-gfb1068f4c8 xhci-hcd [ 15.121267] usb usb2: SerialNumber: xhci-hcd.2.auto [ 15.124164] hub 2-0:1.0: USB hub found [ 15.124181] hub 2-0:1.0: 1 port detected _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org j7-evm ttyS2 Arago 2020.05 j7-evm ttyS2 j7-evm login:
2. then I try to flash boot bootloader & rootds into EMMC by dfu_util, the flash's main_uart log as
U-Boot SPL 2020.01-gbb010db1a9 (Oct 12 2020 - 03:47:37 +0000) SYSFW ABI: 3.0 (firmware rev 0x0014 '20.04.1-v2020.04a (Terrific Lla') Reading on-board EEPROM at 0x50 failed 1 Trying to boot from SPI Loading Environment from MMC... *** Warning - No MMC card found, using default environment Loading rproc fw image from device 3 not supported! Loading rproc fw image from device 3 not supported! Starting ATF on ARM64 core... NOTICE: BL31: v2.3():07.00.00.005-dirty NOTICE: BL31: Built : 03:16:46, Oct 12 2020 U-Boot SPL 2020.01-gf9b0d030d3 (Oct 12 2020 - 04:01:58 +0000) SYSFW ABI: 3.0 (firmware rev 0x0014 '20.04.1-v2020.04a (Terrific Lla') Reading on-board EEPROM at 0x50 failed 1 Trying to boot from SPI U-Boot 2020.01-gf9b0d030d3 (Oct 12 2020 - 04:01:58 +0000) SoC: J721E SR1.0 Model: Texas Instruments K3 J721E SoC Reading on-board EEPROM at 0x50 failed 1 Board: J721EX-PM1-SOM rev E2 DRAM: 4 GiB not found for dev hbmc-mux Flash: 0 Bytes MMC: sdhci@4f80000: 0, sdhci@4fb0000: 1 Loading Environment from MMC... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 Reading on-board EEPROM at 0x50 failed 1 Net: Could not get PHY for ethernet@046000000: addr 0 phy_connect() failed No ethernet found. Hit any key to stop autoboot: 2 0 => => setenv dfu_alt_info ${dfu_alt_info_emmc} => gpt gpt wi rite mmc 0 ${partitions} Writing GPT: success! => print partitions partitions=name=rootfs,start=0,size=-,uuid=${uuid_gpt_rootfs} => dfu 0 mmc 0 ##DOWNLOAD ... OK Ctrl+C to exit ... ######DOWNLOAD ... OK Ctrl+C to exit ... ########DOWNLOAD ... OK Ctrl+C to exit ... ###DOWNLOAD ... OK Ctrl+C to exit ... ################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################DOWNLOAD ... OK Ctrl+C to exit ... => => =>
and PC side command as
D:\Virtualbox\Sharefolder\V3GA\Sandro\windows>dfu-util.exe -l dfu-util 0.9 Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc. Copyright 2010-2016 Tormod Volden and Stefan Schmidt This program is Free Software and has ABSOLUTELY NO WARRANTY Please report bugs to http://sourceforge.net/p/dfu-util/tickets/ Found DFU: [0451:6163] ver=0224, devnum=13, cfg=1, intf=0, path="1-2.1.3", alt=6, name="sysfw.itb.raw", serial="0000000000000000" Found DFU: [0451:6163] ver=0224, devnum=13, cfg=1, intf=0, path="1-2.1.3", alt=5, name="u-env.raw", serial="0000000000000000" Found DFU: [0451:6163] ver=0224, devnum=13, cfg=1, intf=0, path="1-2.1.3", alt=4, name="u-boot.img.raw", serial="0000000000000000" Found DFU: [0451:6163] ver=0224, devnum=13, cfg=1, intf=0, path="1-2.1.3", alt=3, name="tispl.bin.raw", serial="0000000000000000" Found DFU: [0451:6163] ver=0224, devnum=13, cfg=1, intf=0, path="1-2.1.3", alt=2, name="tiboot3.bin.raw", serial="0000000000000000" Found DFU: [0451:6163] ver=0224, devnum=13, cfg=1, intf=0, path="1-2.1.3", alt=1, name="rootfs", serial="0000000000000000" Found DFU: [0451:6163] ver=0224, devnum=13, cfg=1, intf=0, path="1-2.1.3", alt=0, name="rawemmc", serial="0000000000000000" D:\Virtualbox\Sharefolder\V3GA\Sandro\windows>dfu-util.exe -c 1 -i 0 -a 2 -D D:\Virtualbox\Sharefolder\V3GA\Localbuild\tisdk-base-image\1012\tiboot3.bin dfu-util 0.9 Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc. Copyright 2010-2016 Tormod Volden and Stefan Schmidt This program is Free Software and has ABSOLUTELY NO WARRANTY Please report bugs to http://sourceforge.net/p/dfu-util/tickets/ Invalid DFU suffix signature A valid DFU suffix will be required in a future dfu-util release!!! Opening DFU capable USB device... ID 0451:6163 Run-time device DFU version 0110 Claiming USB DFU Interface... Setting Alternate Setting #2 ... Determining device status: state = dfuIDLE, status = 0 dfuIDLE, continuing DFU mode device DFU version 0110 Device returned transfer size 4096 Copying data from PC to DFU device Download [=========================] 100% 230579 bytes Download done. state(7) = dfuMANIFEST, status(0) = No error condition is present state(2) = dfuIDLE, status(0) = No error condition is present Done! D:\Virtualbox\Sharefolder\V3GA\Sandro\windows>dfu-util.exe -c 1 -i 0 -a 3 -D D:\Virtualbox\Sharefolder\V3GA\Localbuild\tisdk-base-image\1012\tispl.bin dfu-util 0.9 Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc. Copyright 2010-2016 Tormod Volden and Stefan Schmidt This program is Free Software and has ABSOLUTELY NO WARRANTY Please report bugs to http://sourceforge.net/p/dfu-util/tickets/ Invalid DFU suffix signature A valid DFU suffix will be required in a future dfu-util release!!! Opening DFU capable USB device... ID 0451:6163 Run-time device DFU version 0110 Claiming USB DFU Interface... Setting Alternate Setting #3 ... Determining device status: state = dfuIDLE, status = 0 dfuIDLE, continuing DFU mode device DFU version 0110 Device returned transfer size 4096 Copying data from PC to DFU device Download [=========================] 100% 687104 bytes Download done. state(7) = dfuMANIFEST, status(0) = No error condition is present state(2) = dfuIDLE, status(0) = No error condition is present Done! D:\Virtualbox\Sharefolder\V3GA\Sandro\windows>dfu-util.exe -c 1 -i 0 -a 4 -D D:\Virtualbox\Sharefolder\V3GA\Localbuild\tisdk-base-image\1012\u-boot.img dfu-util 0.9 Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc. Copyright 2010-2016 Tormod Volden and Stefan Schmidt This program is Free Software and has ABSOLUTELY NO WARRANTY Please report bugs to http://sourceforge.net/p/dfu-util/tickets/ Invalid DFU suffix signature A valid DFU suffix will be required in a future dfu-util release!!! Opening DFU capable USB device... ID 0451:6163 Run-time device DFU version 0110 Claiming USB DFU Interface... Setting Alternate Setting #4 ... Determining device status: state = dfuIDLE, status = 0 dfuIDLE, continuing DFU mode device DFU version 0110 Device returned transfer size 4096 Copying data from PC to DFU device Download [=========================] 100% 1025800 bytes Download done. state(7) = dfuMANIFEST, status(0) = No error condition is present state(2) = dfuIDLE, status(0) = No error condition is present Done! D:\Virtualbox\Sharefolder\V3GA\Sandro\windows>dfu-util.exe -c 1 -i 0 -a 6 -D D:\Virtualbox\Sharefolder\V3GA\Localbuild\tisdk-base-image\1012\sysfw.itb dfu-util 0.9 Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc. Copyright 2010-2016 Tormod Volden and Stefan Schmidt This program is Free Software and has ABSOLUTELY NO WARRANTY Please report bugs to http://sourceforge.net/p/dfu-util/tickets/ Invalid DFU suffix signature A valid DFU suffix will be required in a future dfu-util release!!! Opening DFU capable USB device... ID 0451:6163 Run-time device DFU version 0110 Claiming USB DFU Interface... Setting Alternate Setting #6 ... Determining device status: state = dfuIDLE, status = 0 dfuIDLE, continuing DFU mode device DFU version 0110 Device returned transfer size 4096 Copying data from PC to DFU device Download [=========================] 100% 268410 bytes Download done. state(7) = dfuMANIFEST, status(0) = No error condition is present state(2) = dfuIDLE, status(0) = No error condition is present Done! D:\Virtualbox\Sharefolder\V3GA\Sandro\windows>dfu-util.exe -c 1 -i 0 -a 1 -D D:\Virtualbox\Sharefolder\V3GA\Localbuild\tisdk-base-image\small_rootfs.img dfu-util 0.9 Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc. Copyright 2010-2016 Tormod Volden and Stefan Schmidt This program is Free Software and has ABSOLUTELY NO WARRANTY Please report bugs to http://sourceforge.net/p/dfu-util/tickets/ Invalid DFU suffix signature A valid DFU suffix will be required in a future dfu-util release!!! Opening DFU capable USB device... ID 0451:6163 Run-time device DFU version 0110 Claiming USB DFU Interface... Setting Alternate Setting #1 ... Determining device status: state = dfuIDLE, status = 0 dfuIDLE, continuing DFU mode device DFU version 0110 Device returned transfer size 4096 Copying data from PC to DFU device Download [=========================] 100% 1073741824 bytes Download done. state(7) = dfuMANIFEST, status(0) = No error condition is present state(2) = dfuIDLE, status(0) = No error condition is present Done! D:\Virtualbox\Sharefolder\V3GA\Sandro\windows>
every command seem work successfully.
after that I change the dip switch settings to eMMC mode and power-on customer board again.
SW 8: 1 2 3 4 5 6 7 8 On Off Off Off Off Off Off Off SW 9: 1 2 3 4 5 6 7 8 Off On Off Off Off Off Off Off
Because Our customer board boot mode pins are no different with TI TDA4 EVM board,
I guess I can get some log like "Trying to boot from MMC",
But in fact, there is nothing pup-out form main-uart.
So I can't figure-out what status our board was.
Is there any way can help us to debug what happened?
BR
Sentinen Chen