This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320DM642: Continuous discussion for 925140

Part Number: TMS320DM642

I had a technical support at your site:

https://e2e.ti.com/support/processors/f/791/t/925140

And my customer has just answered the question for the support engineer.

(Q)

could you confirm the application is similar to a HDMI->Svideo converter? and it is only for standard SDTV resolutions?

The processor device may be an overkill, yet still need an external HDMI receiver.

once you confirm we can direct you to the right department.

(A)

This is a converter from TMDS(HDMI) to S-video. I hope "only for standard SDTV resolutions" type if available. If such IC is not available, I accept another video IC that includes this feature (as possible as simple).
I switch the input of NTSC-M / PAL-B and output to same S-Video port.

Could you please suggest the video codec IC?