I am not able to load a new program to the board (for example: tested programs, demo-codes from TI).
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am not able to load a new program to the board (for example: tested programs, demo-codes from TI).
Hello Martin,
Since you put all on-chip memory to disable mode, they are basically non-functional. Can you reprogram your bootloader?
Regards.
Hello Steve,
no, I'm not able to reprogram the bootloader. It's not possible to load a new program to the board, for a new bootloader I have to load the programmer.out file.
Is there a possibility to power up the board without bootloader-mode (maybe reset, etc.)?
Or is it possible to reporgram the board with an other programmer?
Regards
Martin
Martin,
You have JTAG and can bring up CCS, right? Before you "Connect" or "Alt-C", remove the GEL, then "Connect". Once connected, edit the I/O location "0x1c28" via View->Memory->I/O->0x1c28. Re-enable the on-chip memory here. Then load the programmer.out and add back the GEL file.
Please try this.
Regards.