Other Parts Discussed in Thread: TFP410
Hi all,
We use TDA4 CSITX port(picture1) output mipi signal to the GMSL1 Serializer, transfer to the other board by coaxial cable, and the other board use the GMSL1 Deserializer to receive the signal, but we can't detect the HS signal from the Deserializer, we only detect the PCLK, VS, DE(picture2), so we want to know, could the TDA4 CSITX port produce the HS signal transfer by mipi? or we only produce it by the Serializer or Deserializer?
On the other hand, we use TDA2XX output(picture3) the HSYNC, VSYNC, CLK and DATA, to the GMSL1 Serializer, and transfer to the other board by coaxial cable as the same like before, then the other board use the GMSL1 Deserializer to receive the signal, we can detect the HS signal from the Deserializer, it is normal.
Regards,