Hello
I am working on OMAPL138EVM board and my primary requirement is i want to transfer data between FPGA and OMAPL138 using Universal parallel Port
Did anyone transfer data from FPGA to OMAP-L138 EVM via uPP ? The omap-l138 (http://www.ti.com/product/omap-l138) has a Universal Parallel Port (uPP) which offers a high-speed parallel data bus with several important features.
If yes then please provide me the driver functionality
Thanks in advance
Regards
Shubham