Hi,
Firstly, I run command as documented:
root@j7-evm:/opt/vision_apps# ./vx_app_srv_fileio --cfg app_srv.cfg -sh: ./vx_app_srv_fileio: No such file or directory
And then I run vx_app_srv_fileio.out instead of vx_app_srv_fileio
root@j7-evm:/opt/vision_apps# ./vx_app_srv_fileio.out --cfg app_srv.cfg APP: Init ... !!! MEM: Init ... !!! MEM: Initialized DMA HEAP (fd=4) !!! MEM: Init ... Done !!! IPC: Init ... !!! IPC: Init ... Done !!! REMOTE_SERVICE: Init ... !!! REMOTE_SERVICE: Init ... Done !!! APP: Init ... Done !!! 126.781435 s: VX_ZONE_INIT:Enabled 126.781451 s: VX_ZONE_ERROR:Enabled 126.781456 s: VX_ZONE_WARNING:Enabled 126.787201 s: VX_ZONE_INIT:[tivxInit:71] Initialization Done !!! 126.787460 s: VX_ZONE_INIT:[tivxHostInit:48] Initialization Done for HOST !!! Reading calmat file file read completed obj->num_views = 10 app_srv_fileio: Verifying graph 1 ... . app_srv_fileio: Verifying graph 1... Done EGL: version 1.4 EGL: GL Version = (null) EGL: GL Vendor = (null) EGL: GL Renderer = (null) EGL: GL Extensions = (null) app_srv_fileio: Verifying graph 2 ... . app_srv_fileio: Verifying graph 2... Done app_srv_fileio: Running graph 1 ... app_srv_fileio: Running graph 1 ... Done app_srv_fileio: Running graph 2 ... app_srv_fileio: Running graph 2 ... Done 127.692453 s: VX_ZONE_INIT:[tivxHostDeInit:56] De-Initialization Done for HOST !!! 127.696844 s: VX_ZONE_INIT:[tivxDeInit:111] De-Initialization Done !!! APP: Deinit ... !!! REMOTE_SERVICE: Deinit ... !!! REMOTE_SERVICE: Deinit ... Done !!! IPC: Deinit ... !!! IPC: DeInit ... Done !!! MEM: Deinit ... !!! MEM: Alloc's: 34 alloc's of 26845076 bytes MEM: Free's : 34 free's of 26845076 bytes MEM: Open's : 0 allocs of 0 bytes MEM: Deinit ... Done !!! APP: Deinit ... Done !!! root@j7-evm:/opt/vision_apps# ls *.bin app_tidl_avp4.bin
No file named srv_output_file.bin in current directory
But I got an warning, and it's related to this test app?
[MCU2_0] 187.726284 s: DHCP client timed out. Retrying.....
Thanks!