Hi,
I'm working on a custom board with a TDA4 SoC, using Processor SDK 7.0.
I'm trying to bring up the serdes3 in PCIe mode. There's a NVMe SSD connected to serdes3, both lanes of the serdes3 are used by the SSD.
On the TDA4 EVM the first lane of serdes3 is used by USB. I removed that from the device tree.
The Linux kernel PCIe driver times out trying to bring up PCIe3:
[ 4.853657] j721e-pcie 2930000.pcie: Timed out while waiting for link [ 4.860088] j721e-pcie 2930000.pcie: PCIe link never came up [ 4.865737] j721e-pcie 2930000.pcie: host bridge /interconnect@100000/pcie@2930000 ranges: [ 4.873987] j721e-pcie 2930000.pcie: Parsing ranges property... [ 4.874005] j721e-pcie 2930000.pcie: IO 0x4410001000..0x4410010fff -> 0x00001000 [ 4.881650] j721e-pcie 2930000.pcie: MEM 0x4410011000..0x4417ffffff -> 0x00011000 [ 4.925080] j721e-pcie 2930000.pcie: PCI host bridge to bus 0001:00
Do you have a device tree example that uses serdes3 in PCIe mode?
Here's the part of the device tree that is related to this subject:
&usb_serdes_mux { idle-states = <1>, <0>; /* USB0 to SERDES3, USB1 to SERDES1 */ mux-reg-masks = <0x4000 0x0000000>, /* USB0 to SERDES0 mux */ <0x4010 0x0000000>; /* USB1 to SERDES1 mux */ }; &serdes_ln_ctrl { mux-reg-masks = <0x4080 0x3>, <0x4084 0x3>, /* SERDES0 lanes not used */ <0x4090 0x3>, <0x4094 0x3>, /* SERDES1 lanes not used */ <0x40a0 0x3>, <0x40a4 0x3>, /* SERDES2 lanes not used */ <0x40b0 0x3>, <0x40b4 0x3>, /* SERDES3 lanes PCIE3 */ <0x40c0 0x3>, <0x40c4 0x3>, <0x40c8 0x3>, <0x40cc 0x3>; /* SERDES4 lane0/1/2/3 select */ idle-states = <SERDES0_LANE0_PCIE0_LANE0>, <SERDES0_LANE1_PCIE0_LANE1>, <SERDES1_LANE0_PCIE1_LANE0>, <SERDES1_LANE1_PCIE1_LANE1>, <SERDES2_LANE0_PCIE2_LANE0>, <SERDES2_LANE1_PCIE2_LANE1>, <SERDES3_LANE0_PCIE3_LANE0>, <SERDES3_LANE1_PCIE3_LANE1>, <SERDES4_LANE0_QSGMII_LANE5>, <SERDES4_LANE1_QSGMII_LANE6>, <SERDES4_LANE2_QSGMII_LANE7>, <SERDES4_LANE3_QSGMII_LANE8>; }; &serdes_wiz3 { lane0-mode = <PHY_TYPE_PCIE>; lane1-mode = <PHY_TYPE_PCIE>; }; &serdes3 { serdes3_pcie_link: link@0 { reg = <0>; cdns,num-lanes = <2>; #phy-cells = <0>; cdns,phy-type = <PHY_TYPE_PCIE>; resets = <&serdes_wiz3 1>, <&serdes_wiz3 2>; }; }; &pcie3_rc { status = "okay"; pinctrl-names = "default"; pinctrl-0 = <&pcie3_pins_default>; reset-gpios = <&main_gpio0 40 GPIO_ACTIVE_LOW>; phys = <&serdes3_pcie_link>; phy-names = "pcie_phy"; num-lanes = <2>; };
Thank you.