Hi all!
I want to use the 5515EVM to test some algorithms using both the AIC3204 and the C5515. I modified the loopback routine that came with the board, but with little success. When I try to change the Sampling Rate from 48kHz to 20kHz by changing the PLL register values, it stops working. I found literally no documentation concerning the connection and Clocks involved. Maybe someone can point me in the right direction.
Many Thanks in Advance,
Best,
Axel