This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2HG: VSDK3.07

Part Number: TDA2HG

Hi,

When I referTIDeepLearningLibrary_UserGuide.pdf,

3.3.4

5) The above step creates executable files, “dsp_test_dl_algo.out” and “eve_test_dl_algo.out” in the modules\ti_dl\test\out sub-directory.
6) Open CCS with TDA2x platform selected configuration file. Select Target > Load Program on C66x DSP/EVE, browse to the modules\ti_dl\test\out sub-directory, select the executable created in step 5, and load it into Code Composer Studio in preparation for execution.
7) Select Target > Run on C66x DSP/EVE window to execute the sample test application.

 

CCS cannt run,

the error is as follws

[C66xx_DSP1]
Processing config file ..\..\test\testvecs\config\infer\tidl_config_jseg21.txt !
Could Not Open Files ..\..\test\testvecs\config\tidl_models\tidl_net_jsegnet21v2.bin
Could not open ..\..\test\testvecs\config\tidl_models\tidl_param_jsegnet21v2.bin
file for reading
Could not open ..\..\test\testvecs\input\000100_1024x512_bgr.y
file for reading

Processing Frame Number : 0

TSC Mega Cycles = 0.01 End of config list found !