This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: DDR 64bit address range

Part Number: TDA4VM


Is there anyway to access all ddr as a sequential physical address space. Looks like first 2gby is always at 0x8000_0000 and next address is 0x8_0000_0000 but "The first 2 GB of this region are inaccessible." so it is really 0x8_8000_0000.  I don't want to use the a72 MMU since peripherals and other cores would need a virt to phy conversion.

On am6 I could use CTRLMMR0_MCU_MSMC_CFG to map that first 2gby up to 0x8_0000_0000 but I don't see that option on j7.