This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: AM-5728 Board Tester Software

Part Number: AM5728

Hello,

I have AM-5728 evaluation module and I am trying to test my board interfaces, following the below link.

https://software-dl.ti.com/processor-sdk-rtos/esd/docs/06_03_00_106/rtos/Board_EVM_Abstration.html ( Section 3.2 Diagnostics )

According to this link, there are two ways to test the board interfaces 

1. Using SD Card 

2. Using SPI flash

I am able to create SD loadable files and run the diagnostics through them successfully. However, when I try the SPI flash method (refer to Section 3.2.3.2),

it asks to load and run the pre-built SPI flash writer binary, which must be available at path <PDK>/packages/ti/starterware/tools/flash_writerspi_flash_writer_AMXXXX.out

I could not find this file and path in my RTOS SDK.

Folders present in RTOS SDK at path <pdk_am57xx_1_0_17/packages/ti> are

binary, board, boot, build, csl, drv, fs, osal, transport, utils

Regards

Sahil Kalra