Hi
I have a question related to
We are planning to use at 85℃.
To increase the refresh rale at high temp, we believe that ASR or SRT should be enabled.
Therefore, we would like to confirm if we can enable it appropriately.
> Setting either bit will trigger an initialization, which would only be noticeable if you probe the DDR signals.
I understand that we can see if we can enable it appropriately by monitoring the DDR signals.
Which signal should be observed at what timing?
In addition to set ASR or SRT, is there any points which we have to take care to use the device at high temp environment?
Thanks and Best regards,
HaTa