This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5746: SDRAM connections on EMIFx

Part Number: AM5746


Working with a customer on this device. They used the AM5726BABCXA in an older design with 2 SDRAMs on the board but only wired one of them. Now they are using the dual core AM5746ABZXA instead of AM5726BABCXA and want to use both SDRAMs. Do they need to wire up both channels EMIF1 and EMIF2 for the two SDRAMs?